Single-Board Computers
  • Products
  • Dev Tools
  • Single-Board Computers
  • More
  • Cancel
Single-Board Computers
Forum Re: TGIF - share your weekend plans for the BeagleBone Black!
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Single-Board Computers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 7 replies
  • Subscribers 60 subscribers
  • Views 852 views
  • Users 0 members are here
Related

Re: TGIF - share your weekend plans for the BeagleBone Black!

morgaine
morgaine over 13 years ago

Brian Welsby wrote:

 

I have been tinkering with high speed ADCs and FPGAs running currently at 60Mhz and transferring data to my PC over USB.  Then along came BBB and it's PRUs  image so my thinking is more along the lines of a multi function device, basic scope, logic analyser, frequency counter..... 

 

I have the Open Bench Logic Sniffer (OBLS), and always appreciate good instrumentation with open hardware just making it even better.  It did occur to me that the BBB could be used as the basis of a really powerful engineering instrument, possibly by interfacing the PRUs directly with the OBLS's Spartan 3E.  And the sky's the limit when one is willing to reprogram the instrument's FPGA!

 

Indeed, even the very low hanging fruit of attaching OBLS via USB as normal and running the OBLS client on the BBB provides a feature of a kind, since it turns the LA into a detached networked LA with all the benefits of galvanic isolation from your desktop computer that you get for free with Ethernet.  Even that small thing can be a bonus.

 

And I occasionally use my Bus Pirate as a stupid little extra ultra-slow PirateScope when my real scope's two channels are tied up, so I can't resist the feeling that there is a supreme additional instrument just begging to be made here by combining some of these bits of hardware together with BBB. image

 

If this awesome possibility is going to be pursued further, either through an instrumentation cape or by riding on the shoulders of giants by harnessing existing open hardware instruments or their designs, please let's split it out into a separate thread before it gets submerged inside this kitchen sink topic!!!

 

Drew's done this splitting service for us before, we just have to ask nicely. image

 

Morgaine.

  • Sign in to reply
  • Cancel
Parents
  • fustini
    fustini over 13 years ago

    I can branch the discussion with my admin account... would this be the logical point?

     

    http://www.element14.com/community/message/78090#78045

     

    thanks,

    drew

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • fustini
    fustini over 13 years ago

    I can branch the discussion with my admin account... would this be the logical point?

     

    http://www.element14.com/community/message/78090#78045

     

    thanks,

    drew

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • interested1
    interested1 over 13 years ago in reply to fustini

    Well, my first to-do is wait by the mailbox for the LCD7 Cape. 

     

    As far as interaction with the BBB, I am going to be learning more about embedded Linux, Yocto, and device tree stuff since my experience with Linux is grounded in the '90s --a bit of a different animal it seems.  I hope soon to be taking Boris for a walk, and if I can get a portable power setup working (the batter cape is on backorder image) then I will definately go for a walk with the Beagle!

     

    Another thing on my to-do list is to make a Boneyard for the Beagles that I currently have in my pound.  I haven't decided if I am going to do some laser cutting or just do a cheap wood mock-up so the boards don't run away because of cable pull (beagles do like to bolt, the dogs anyway!).

     

    Have a great weekend everyone!

     

    David

    P.S.

    Drew, it might be nice to have a weekly thread, since the site makes it look like someone merely used "touch" on an old thread.  Actually, I would have posted my previous weeks BBB adventure, but thought the thread then was old... I guess it pays to investigate more on my part.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • bwelsby
    bwelsby over 13 years ago in reply to fustini

    Drew Fustini wrote:

     

    I can branch the discussion with my admin account... would this be the logical point?

     

    http://www.element14.com/community/message/78090#78045

     

    thanks,

    drew

     

    Yes Drew that would be great, the primary focus will be a discussion an the development of a multifunction instrument based on the BBB

    Cheers,

    Brian

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • fustiniadmin
    fustiniadmin over 13 years ago in reply to bwelsby

    I've branched the thread from thread http://www.element14.com/community/thread/23802?tstart=0

     

    (Please note the existing replies in this thread retain the old subject.  This turns out to be intentional functionality after talking to our platform vendor.  The reasoning is that the meaning of one's reply could be altered by the name of the new branch.)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • bwelsby
    bwelsby over 13 years ago in reply to fustiniadmin

    Thank you Drew.