Single-Board Computers
  • Products & Partners
  • Dev Tools
  • Single-Board Computers
  • More
  • Cancel
Single-Board Computers
Forum Intel to give away 50,000 Arduino-friendly computers based on 400MHz Quark SoC
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Single-Board Computers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 23 replies
  • Subscribers 63 subscribers
  • Views 4745 views
  • Users 0 members are here
Related

Intel to give away 50,000 Arduino-friendly computers based on 400MHz Quark SoC

e14 Contributor
e14 Contributor over 13 years ago

http://www.theregister.co.uk/2013/10/03/intel_seeks_slice_of_pi_with_arduinofriendly_galileo_board_computer/

http://www.intel.com/content/www/us/en/do-it-yourself/galileo-maker-quark-board.html

http://download.intel.com/support/galileo/Galileo_Datasheet_329681.pdf

https://communities.intel.com/docs/DOC-21828

http://www.anandtech.com/show/7387/intel-announces-galileo-quark-based-arduino-compatible-developer-board

 

ISA: 32-bit x86

RAM:  256MB  (SoC can support up to 2GB)

DImensions:  4.2 inches long by 2.8 inches wide.

fab: 32nm

SoC package: Flip-Chip Ball Grid Array (FCBGA) package with 393 solder

                       balls with 0.593 mm ball pitch. The package dimensions are 15mm x 15mm.

L1 cache: 16Kbyte shared I/D

 

Power supply:  3A at 5V

Price:  Under $60

Availability: December, 2013

 

Development OS Support (see Note below):

  • Linux Ubuntu 12.04* (32-bit & 64-bit)
  • Mac OS X version 10.8.5* (also tested on Mac OS X 10.6.8, 10.7.5, and 10.9* developer preview)
  • Windows 7* (32-bit & 64-bit) and Windows 8*

 

I/O:

  • A full sized mini-PCI Express slot,
  • 100Mb Ethernet port,
  • Micro-SD slot,
  • RS-232 serial port,
  • USB Host port,
  • USB Client port,
  • 8MByte NOR flash.

 

NOTE:  don't understand how 32-bit ISA claims to support 64-bit OSs.

added:  Maybe these OS's aren't actually running on the board itself, but are

intended to run on a connected host computer. 

  • Sign in to reply
  • Cancel

Top Replies

  • DAB
    DAB over 13 years ago in reply to morgaine +1
    I have some special research tools that I build that are still at work on my MS DOS computers. Yes I still have some up and running for data collection purposes. If the new board supports the 8086 instruction…
  • morgaine
    morgaine over 13 years ago in reply to DAB +1
    DAB wrote: Plus I was never into this throw away society. My German roots run deep and we try to keep everything running as long as they can still do the job. +1. I like the philosophy you express above…
  • morgaine
    morgaine over 13 years ago in reply to e14 Contributor +1
    Although true, most upgrades aren't made because the user will benefit from improved efficiency, but because the old gear is no longer compatible with new product or else is portrayed by marketing as no…
Parents
  • DAB
    DAB over 13 years ago

    Very interesting.

     

    I wonder if Element 14 could snag a few for us to test. image

     

    If it is truely 86 compatible, I can see a lot of interesting uses for this new system.

     

    I would definately pay 60 USD for one just to see what I could do with it and to see what legacy software I could run.  I have a few old MS DOS tools that would just scream if I could run them on this fast of a processor set.

     

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 13 years ago in reply to DAB

    DAB wrote:

     

    If it is truely 86 compatible, I can see a lot of interesting uses for this new system.

     

    Could you enumerate some for us please?  I can see the "warm fuzzy feeling of being on familiar territory" that selsinork mentioned (great phrase) as indeed being a very strong selling point, but I don't see any significant engineering reasons that aren't extremely niche.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to morgaine

    Morgaine Dinova wrote:

     

    I can see the "warm fuzzy feeling of being on familiar territory" that selsinork mentioned (great phrase) as indeed being a very strong selling point, but I don't see any significant engineering reasons that aren't extremely niche.

    Engineering reasons don't tend to get a look in when there's an emotional factor overriding the rational decision image

     

    How many times have we seen the question asked around whether the RPi can run windows ?  As the answer here will likely be that you can, it'll keep some people happy.  I'd still question the rationale behind even trying on a device with no display and various other limitations, but none of that will matter to them..

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • DAB
    DAB over 13 years ago in reply to morgaine

    I have some special research tools that I build that are still at work on my MS DOS computers.  Yes I still have some up and running for data collection purposes.

     

    If the new board supports the 8086 instruction set, it might be possible to set up a cut down version of MS DOS to drive the some of the tools.

    Most of them just need a way to access data ports, memory and disk I/O.  So if I can get it to access the configuration files, run the code and generate the output data I need, I could do some interesting data collection.

     

    MS DOS is soooo much simpler than windows that you can run some very simple programs at very fast speeds.

     

    Like I said, it would be an interesting side project, assuming I can find the time to do the port.  Meanwhile my old computers are still just plugging along.

    One nice thing about the older machines, some of these last nearly forever.

     

    Plus I was never into this throw away society.  My German roots run deep and we try to keep everything running as long as they can still do the job.

     

    DAB

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 13 years ago in reply to DAB

    DAB wrote:

     

    Plus I was never into this throw away society.  My German roots run deep and we try to keep everything running as long as they can still do the job.

     

    +1.

     

    I like the philosophy you express above, and it's tragic that engineers are coaxed into developing throwaway junk for the sake of profit and occasionally even defend that market norm as if it were good.  It's never good to create junk designed to last only until the next upgrade:   1) it's not good for the planet and 2) it's not good for our self-esteem as engineering professionals.  "Engineering for obsolence" is a corruption of responsible engineering practice.

     

    Somehow both of those reasons have got lost in most of today's manufacturing circles.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • morgaine
    morgaine over 13 years ago in reply to DAB

    DAB wrote:

     

    Plus I was never into this throw away society.  My German roots run deep and we try to keep everything running as long as they can still do the job.

     

    +1.

     

    I like the philosophy you express above, and it's tragic that engineers are coaxed into developing throwaway junk for the sake of profit and occasionally even defend that market norm as if it were good.  It's never good to create junk designed to last only until the next upgrade:   1) it's not good for the planet and 2) it's not good for our self-esteem as engineering professionals.  "Engineering for obsolence" is a corruption of responsible engineering practice.

     

    Somehow both of those reasons have got lost in most of today's manufacturing circles.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Children
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to morgaine

    There is a flip side to this philosopy.  If the product is fixed-function and

    fully satisfies its purpose, then there is no point replacing it just because

    something newer/better/cheaper comes along.  But if the newer product

    has new functionality that can be taken advantage of, then it can be a

    mistake to hold on to the old product even if it still works.

    I think it is referred to as economic life vs. useful life.

     

    For example if a new solar panel comes along with significantly better

    efficiency, it might be economic to replace an existing panel before the

    end of its useful life.  Getting the timing right is tricky if it's likely that an

    even better panel will come along in the near future.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 13 years ago in reply to e14 Contributor

    Although true, most upgrades aren't made because the user will benefit from improved efficiency, but because the old gear is no longer compatible with new product or else is portrayed by marketing as no longer being adequate or cool.  An example is Intel and AMD changing the CPU socket for the 500th time and so requiring everyone either to upgrade their motherboards (rare) if they want the new CPU or else have to buy a whole new computer.  It's inexcusable.