Single-Board Computers
  • Products
  • Dev Tools
  • Single-Board Computers
  • More
  • Cancel
Single-Board Computers
Forum Angstrom
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Single-Board Computers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 26 replies
  • Subscribers 59 subscribers
  • Views 3528 views
  • Users 0 members are here
Related

Angstrom

e14 Contributor
e14 Contributor over 12 years ago

Interesting discussion over on the beagleboard google group https://groups.google.com/forum/#!category-topic/beagleboard/kz3M-It3U5Y

 

Reading between the lines, you get the impression that angstrom was a one man show and that the CircuitCo employee who was that one man has now left for another company.

Exactly what that means for any boards currently using angstrom is as yet unclear.

 

However, if true that angstrom was effectively one person it may explain a lot of the issues people here have seen with it.  Unfortunately the risk is that if angstrom ends up effectively unmaintained, any boards using it as the default pre-installed distro could well get stuck in a dead-end.

 

The beagleboard folks have so far steadfastly stuck with angstrom in spite of the obvious problems, I think it'll be interesting to see what happens next.

  • Sign in to reply
  • Cancel

Top Replies

  • morgaine
    morgaine over 12 years ago +2
    selsinork wrote: Reading between the lines, you get the impression that angstrom was a one man show and that the CircuitCo employee who was that one man has now left for another company. You're…
  • e14 Contributor
    e14 Contributor over 12 years ago +2
    Probably about as close as an official response you're likely to get from Jason in this thread: https://groups.google.com/forum/#!category-topic/beagleboard/GK8Chte-4Xs I don't think there's any huge surprise…
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to shabaz +1
    There's been a couple of off-hand comments over there about angstrom being dead or in the process of being replaced, but I could never find out where those people were getting their rumours from. Someone…
Parents
  • e14 Contributor
    e14 Contributor over 12 years ago

    Probably about as close as an official response you're likely to get from Jason in this thread:

    https://groups.google.com/forum/#!category-topic/beagleboard/GK8Chte-4Xs

     

    I don't think there's any huge surprise that his requirements seem to come down to bonescript, capemgr and dtbo's for known capes on top of <insert OS here>.

    What I find interesting is that they're prepared to discuss a move, have sensible requirements before doing so, and have obviously been doing some work around getting a version of Debian to that point already. I'd not seen anything suggesting it would even be open for discussion previously.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • johnbeetem
    johnbeetem over 12 years ago in reply to e14 Contributor

    selsinork wrote:

     

    Probably about as close as an official response you're likely to get from Jason in this thread:

    https://groups.google.com/forum/#!category-topic/beagleboard/GK8Chte-4Xs

     

    I don't think there's any huge surprise that his requirements seem to come down to bonescript, capemgr and dtbo's for known capes on top of <insert OS here>.

    What I find interesting is that they're prepared to discuss a move, have sensible requirements before doing so, and have obviously been doing some work around getting a version of Debian to that point already. I'd not seen anything suggesting it would even be open for discussion previously.

    That's good news on Debian.  I'll be looking forward to it -- I wonder if it can run decently on a 128MB BeagleBoard B4?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to johnbeetem

    John Beetem wrote:

     

    I wonder if it can run decently on a 128MB BeagleBoard B4?

    I wouldn't like to guess.  In the end, base requirements will continue to rise, pushed ever upwards by x86 systems that will reasonably have terabyte drives and 8-16Gb ram. Trying to push an OS designed with easy availability of resources onto an Arm board that more closely resembles where x86 was a decade or more ago can't be the easiest of things to do.

    I'm not convinced Debian is the best choice for an embedded board, but then I don't really have a better idea. Debian does have the advantage of having a much bigger pool of active developers than we could hope for on a beagle* only distro. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 12 years ago in reply to johnbeetem

    John Beetem wrote:

     

    That's good news on Debian.  I'll be looking forward to it -- I wonder if it can run decently on a 128MB BeagleBoard B4?

     

    I've run Linux in 16MB of RAM and it's known to run in a lot less than that, so the answer is undoubtedly "yes" as far as the kernel is concerned.  Although the kernel codebase has grown massively over the years, it's so modular that tiny kernels can still be configured.

     

    On the user-space side, to make a distro fit a small embedded board just requires disabling superfluous subsystems, of which there are typically vast numbers in any modern distro.  I doubt that 128MB represents a serious constraint at all for an embedded environment.  This even applies to desktops, but there it's subject to personal expectations of what needs to be present.  Some people require not only the kitchen sink to be running, but 5 of them simultaneously.

     

    Morgaine.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • johnbeetem
    johnbeetem over 12 years ago in reply to morgaine

    Morgaine Dinova wrote:

     

    I've run Linux in 16MB of RAM and it's known to run in a lot less than that, so the answer is undoubtedly "yes" as far as the kernel is concerned.  Although the kernel codebase has grown massively over the years, it's so modular that tiny kernels can still be configured.

    I first used Unix on a 256KB PDP-11/45, with multiple users.  If two people compiled at the same time it would slow down a bit, but normally people were editing (using ed, natürlich) so the PDP-11/45 could support quite a few users.

     

    While a 128MB BeagleBone is physically small, I like to think of it as a small mainframe and bloat-free software runs quite well.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 12 years ago in reply to johnbeetem

    John Beetem wrote:

     

    I first used Unix on a 256KB PDP-11/45, with multiple users.

    ...

    While a 128MB BeagleBone is physically small, I like to think of it as a small mainframe

    Ah, the reminiscing. image

     

    Well a PDP-11/45 almost was a mainframe, compared to its younger sibling PDP-11/34 on which I first ran Unix V6 and V7 (and something called "mini-Unix" prior to V6).  Unfortunately I can't remember how much RAM it had, but the likelihood is less than your 11/45.  We didn't have a lot of money ...

     

    I never had a chance to bring up Unix on our 11/20, as it got upgraded to the 11/34 at the same time as I was discovering the joys of "ls -l" and "cc -c" on another department's larger PDPs, but it probably had even less memory and was still known to run Unix.

     

    Anyway, back in Linux time, I think we can safely say that the Linux kernel is happy with any amount that one is likely to find on an ARM applications processor board.

     

    Morgaine.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • morgaine
    morgaine over 12 years ago in reply to johnbeetem

    John Beetem wrote:

     

    I first used Unix on a 256KB PDP-11/45, with multiple users.

    ...

    While a 128MB BeagleBone is physically small, I like to think of it as a small mainframe

    Ah, the reminiscing. image

     

    Well a PDP-11/45 almost was a mainframe, compared to its younger sibling PDP-11/34 on which I first ran Unix V6 and V7 (and something called "mini-Unix" prior to V6).  Unfortunately I can't remember how much RAM it had, but the likelihood is less than your 11/45.  We didn't have a lot of money ...

     

    I never had a chance to bring up Unix on our 11/20, as it got upgraded to the 11/34 at the same time as I was discovering the joys of "ls -l" and "cc -c" on another department's larger PDPs, but it probably had even less memory and was still known to run Unix.

     

    Anyway, back in Linux time, I think we can safely say that the Linux kernel is happy with any amount that one is likely to find on an ARM applications processor board.

     

    Morgaine.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to morgaine

    Morgaine Dinova wrote:

    Anyway, back in Linux time, I think we can safely say that the Linux kernel is happy with any amount that one is likely to find on an ARM applications processor board.

    the kernel itself will run with very little, lots of those cheap wifi and adsl routers run linux and have as little as 8MB, of course the userspace component is hugely cut down and specialised compared to any regular distro.