Single-Board Computers
  • Products
  • Dev Tools
  • Single-Board Computers
  • More
  • Cancel
Single-Board Computers
Forum Wandboard Quad vs CubieTruck
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Single-Board Computers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 7 replies
  • Subscribers 59 subscribers
  • Views 1166 views
  • Users 0 members are here
  • cubieboard
  • wandboard
  • cubietruck
Related

Wandboard Quad vs CubieTruck

e14 Contributor
e14 Contributor over 12 years ago

Title says it all.. What do people thing of the $129 Wandboard Quad (http://wandboard.org/)  vs the approx $90-$120 CubieTruck (https://www.miniand.com/products/Cubietruck%20A20%20Dev%20Board Cubietruck CUBIEBOARD3 Cortex A7 Dual Core 2GB RAM 8GB Flash with WiFi BT | eBay)

 

CubieTruck:

912MHz Dual core Cortex-A7 (Allwinner A20)

2GB ram

Gigabit Network

SATA

Onboard WiFi+BT

micro SD

HDMI

Optical S/PDIF

 

WBQuad:

996MHz Quad Core Cortex-A9 (Freescale i.MX6)

2GB ram

Gigabit network

SATA

Onboard WiFI+BT (broadcom?)

micro SD x2

HDMI

Optical S/PDIF

USB 3

 

The WBDual lacks SATA and only has 1GB ram for $99 so may be less attractive compared to a 2GB CT.

 

Neither are available from e14, so we have to look elsewhere.

Here in the UK, the CT is approx 95 GBP + shipping http://www.coolcomponents.co.uk/cubietruck-kit-dual-core-single-board-computer.html

Compared to WBQuad from Future Electronics and shipped from the US since there don't appear to be any UK stockists at 91.85 GBP + shipping WBQUAD | i.MX6 Quad Core@1GHz Multimedia Processor Development Board w/WiFi and Bluetooth | WANDBOARD.ORG - Future E… (76.54 + 20% UK VAT to get to 91.85)

 

So very similar specs, and mostly identical cost, yet dual core vs quad core.  The A7 is potentially better as it's feature compatible with the A15 which could offer a smoother upgrade path later. The A7 therefore offers hardware virtualisation while the A9 doesn't. The A7 is still basically an A8 class cpu at heart though, so will be somewhat slower than the A9.

Does anyone care though ?  It seems that the Linux Kernel Virtual Machine isn't yet quite ready to do virtualisation on these and Debian/Ubuntu/Fedora etc are targetting armv7l (or A8 upwards) which means the additional features like vfpv4 are unlikley to be used. Yet.. By the time they are, it seems likely there'll be something better, faster and likely cheaper and people will move on.

 

So what do we think today, is the WBQuad a better buy, or the CubieTruck ?

  • Sign in to reply
  • Cancel

Top Replies

  • e14 Contributor
    e14 Contributor over 12 years ago in reply to johnbeetem +1
    John Beetem wrote: Thank you for the specs. From the specs alone, it's kind of a toss-up, though I personally like the i.MX6 better because of superior documentation. The last time I looked the AllWinner…
  • morgaine
    morgaine over 12 years ago in reply to e14 Contributor +1
    selsinork wrote: I've experienced websites that cause the cpu fans to speed up on a quad core Intel i7, so these javascript heavy sites are still likely to be problematic. At this time of year, those…
Parents
  • morgaine
    morgaine over 12 years ago

    It's a draw, so the best answer is "Both"! image

     

    I deferred a purchase as I didn't expect to have time to work with it in December anyway, but I'll probably be ordering one of them shortly.  I might relent on foreign ordering as I find the i.MX6 quad more tempting and we're about to get invaded with A20 product from Olimex anyway ...

     

    Oh, and Happy New Year 2014 to all! image

     

    Morgaine.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • morgaine
    morgaine over 12 years ago

    It's a draw, so the best answer is "Both"! image

     

    I deferred a purchase as I didn't expect to have time to work with it in December anyway, but I'll probably be ordering one of them shortly.  I might relent on foreign ordering as I find the i.MX6 quad more tempting and we're about to get invaded with A20 product from Olimex anyway ...

     

    Oh, and Happy New Year 2014 to all! image

     

    Morgaine.