Single-Board Computers
  • Products & Partners
  • Dev Tools
  • Single-Board Computers
  • More
  • Cancel
Single-Board Computers
Forum EOMA-68 finally ?
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Single-Board Computers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 9 replies
  • Subscribers 59 subscribers
  • Views 1499 views
  • Users 0 members are here
  • allwinner-a20
  • eoma
  • sbc
  • eoma-68
Related

EOMA-68 finally ?

e14 Contributor
e14 Contributor over 12 years ago

http://liliputing.com/2013/11/improv-is-a-75-modular-arm-based-computer-core-eoma-68.html

 

Could this be the first actual EOMA-68 turned into a product that you can (almost) buy ?  Have rhombus tech been beaten to the finish line ?

 

It'll be interesting to see where it leads, now that there's an actual product (almost) available, not sure on the $75 though, it seems that there's probably better value boards available today, and that there's only going to be more of those in the next year.  We've seen mention of an OLinuXino-LIME2 with almost identical specs plus gigabit ethernet, which could possibly be below this price point.

 

Interesting times for SBC's indeed..  Although I'm not really sure that things like Improv or Wandboard where you have two boards really qualify as Single Board Computers.

  • Sign in to reply
  • Cancel
Parents
  • morgaine
    morgaine over 12 years ago

    selsinork wrote:

     

    Interesting times for SBC's indeed..  Although I'm not really sure that things like Improv or Wandboard where you have two boards really qualify as Single Board Computers.

     

    Haha, good point.  Maybe the phrase Modular Board Computers should be coined for these multi-board assembles?  (The 'M' could also refer to "multi".)  "Modular" certainly reflects the intent behind EOMA-68 and EDM.

     

    What's missing in all these cases though are third-party baseboards or motherboards.  There's still no general buy-in for these modular concepts by third parties.  When the baseboards are available only from the same manufacturer as the CPU module, that creates strong lock-in.

     

    Morgaine.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to morgaine

    From reading the Wandboard forums and google group, it sounds like there are some other base boards in the process of being designed/manufactured by third parties. Although until they're available to buy it's mostly irrelevant.  As part of the bigger Technexion range there are other EDM cpu boards and carrier boards available, so there is some choice there even if it is all from the same vendor. Wandboard/Technexion do seem to encourage third party take up by making cpu boards and connector kits available, albeit in 10 packs.

     

    As for EOMA.. well there's been lots of talk over the last two years or so, and so far the Improv appears to be the only product. There was mention of a tablet that's going to use it, but again from the same people selling the Improv.  Potentially there's Rhombus and Improv as two distinct vendors of EOMA - assuming Rhombus ever actually manage to cross the finish line and get a product on sale..

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 12 years ago in reply to e14 Contributor

    Maybe this is where the open source hardware community could step in and design a modular computer without the hard parts --- because those are inside the plugin-in modules.

     

    There's no shortage of dab-hands with Eagle here, and in many other places.  It just needs the itch. image

     

    Morgaine.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • morgaine
    morgaine over 12 years ago in reply to e14 Contributor

    Maybe this is where the open source hardware community could step in and design a modular computer without the hard parts --- because those are inside the plugin-in modules.

     

    There's no shortage of dab-hands with Eagle here, and in many other places.  It just needs the itch. image

     

    Morgaine.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to morgaine

    Morgaine Dinova wrote:

     

    Maybe this is where the open source hardware community could step in and design a modular computer without the hard parts --- because those are inside the plugin-in modules.

     

    There's no shortage of dab-hands with Eagle here, and in many other places.  It just needs the itch.

     

    Morgaine.

     

    now you're getting it, morgaine image  and unlike other modular computing units (such as the engineering board style ones mentioned earlier, as well as Q-Seven and so on) the idea is that EOMA68 units will be *mass-volume* and therefore a) lower cost b) easy to get hold of.  my vision is that EOMA68 CPU Cards would be available literally as off-the-shelf units in supermarkets.

     

    if you look at the interfaces on EOMA68, you have all the high-speed signals as differential pairs.  a good engineer can do differential-pairs with KiCAD by creating a temporary part that has the exact width of the two tracks needed to be laid out and then dragging that around (this was a tip from an experienced KiCAD user).  the RGB/TTL interface on the current EOMA68 specification maxes out at 1280x800 so the data rate is going to be somewhere around 60mhz for a 60hz refresh rate.  SD/MMC goes up to what... 50mhz at the moment?  you only really have to worry about R.F. emissions at above 400 to 500mhz.

     

    so yes, you're exactly on the right track (so to speak).  the whole point of the exercise is that a *really* good computing module is available as a future-proof off-the-shelf upgradeable unit, leaving engineers with the much easier task of creating a simple 2 or 4 layer PCB, confident that they really don't have to do that work again just because processors get faster.

     

    which is kinda cool.