Single-Board Computers
  • Products & Partners
  • Dev Tools
  • Single-Board Computers
  • More
  • Cancel
Single-Board Computers
Forum EOMA-68 finally ?
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Single-Board Computers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 9 replies
  • Subscribers 59 subscribers
  • Views 1497 views
  • Users 0 members are here
  • allwinner-a20
  • eoma
  • sbc
  • eoma-68
Related

EOMA-68 finally ?

e14 Contributor
e14 Contributor over 12 years ago

http://liliputing.com/2013/11/improv-is-a-75-modular-arm-based-computer-core-eoma-68.html

 

Could this be the first actual EOMA-68 turned into a product that you can (almost) buy ?  Have rhombus tech been beaten to the finish line ?

 

It'll be interesting to see where it leads, now that there's an actual product (almost) available, not sure on the $75 though, it seems that there's probably better value boards available today, and that there's only going to be more of those in the next year.  We've seen mention of an OLinuXino-LIME2 with almost identical specs plus gigabit ethernet, which could possibly be below this price point.

 

Interesting times for SBC's indeed..  Although I'm not really sure that things like Improv or Wandboard where you have two boards really qualify as Single Board Computers.

  • Sign in to reply
  • Cancel
Parents
  • morgaine
    morgaine over 12 years ago

    selsinork wrote:

     

    Interesting times for SBC's indeed..  Although I'm not really sure that things like Improv or Wandboard where you have two boards really qualify as Single Board Computers.

     

    Haha, good point.  Maybe the phrase Modular Board Computers should be coined for these multi-board assembles?  (The 'M' could also refer to "multi".)  "Modular" certainly reflects the intent behind EOMA-68 and EDM.

     

    What's missing in all these cases though are third-party baseboards or motherboards.  There's still no general buy-in for these modular concepts by third parties.  When the baseboards are available only from the same manufacturer as the CPU module, that creates strong lock-in.

     

    Morgaine.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to morgaine

    Morgaine Dinova wrote:

     

    What's missing in all these cases though are third-party baseboards or motherboards.  There's still no general buy-in for these modular concepts by third parties.  When the baseboards are available only from the same manufacturer as the CPU module, that creates strong lock-in.

     

    Morgaine.

     

    the source code in KiCAD CAD/CAM format for various EOMA68 hardware PCB projects is available publicly under the GPL software license if you look for it on the rhombus-tech.net web site.  unfortunately there was no take-up (no assistance offered by open hardware engineers) when those projects were begun, as it takes quite a lot of committment and no such committment was given.

     

    so i was forced, in order to complete the project, to begin using proprietary CAD/CAM tools and to pay professional engineering teams quite large sums of money to get the boards completed.

     

    obviously, i want that investment of funds back.

     

    you have to bear in mind that i am primarily a software libre advocate (with an incredibly ambitious goal).  it is going to be necessary to kick-start this project with a number of different CPU Cards and different base units before people start to "Get It (tm)".  once there are several examples (on each side of the EOMA68 interface) to play with, people will stop thinking of this as a) vapourware b) yet another SBC project c) will find the KiCAD examples that i began 3 years ago, and will consider completing them or creating their own.

     

    if that doesn't happen as quickly as i would like it to, i will (once the project is financially self-sustaining and the personal funds invested have been recouped) release a number of products as full GPL'd Open Hardware PCB designs.

     

    so i foresee a future in which there will be plenty of open hardware third party EOMA68 designs out there.  in fact, there is one third party team who has stuck with the project throughout: they are creating a hand-held games console.  http://rhombus-tech.net/community_ideas/games_console/

     

    does that help address the point that you raise?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to morgaine

    Morgaine Dinova wrote:

     

    What's missing in all these cases though are third-party baseboards or motherboards.  There's still no general buy-in for these modular concepts by third parties.  When the baseboards are available only from the same manufacturer as the CPU module, that creates strong lock-in.

     

    Morgaine.

     

    the source code in KiCAD CAD/CAM format for various EOMA68 hardware PCB projects is available publicly under the GPL software license if you look for it on the rhombus-tech.net web site.  unfortunately there was no take-up (no assistance offered by open hardware engineers) when those projects were begun, as it takes quite a lot of committment and no such committment was given.

     

    so i was forced, in order to complete the project, to begin using proprietary CAD/CAM tools and to pay professional engineering teams quite large sums of money to get the boards completed.

     

    obviously, i want that investment of funds back.

     

    you have to bear in mind that i am primarily a software libre advocate (with an incredibly ambitious goal).  it is going to be necessary to kick-start this project with a number of different CPU Cards and different base units before people start to "Get It (tm)".  once there are several examples (on each side of the EOMA68 interface) to play with, people will stop thinking of this as a) vapourware b) yet another SBC project c) will find the KiCAD examples that i began 3 years ago, and will consider completing them or creating their own.

     

    if that doesn't happen as quickly as i would like it to, i will (once the project is financially self-sustaining and the personal funds invested have been recouped) release a number of products as full GPL'd Open Hardware PCB designs.

     

    so i foresee a future in which there will be plenty of open hardware third party EOMA68 designs out there.  in fact, there is one third party team who has stuck with the project throughout: they are creating a hand-held games console.  http://rhombus-tech.net/community_ideas/games_console/

     

    does that help address the point that you raise?