Single-Board Computers
  • Products
  • Dev Tools
  • Single-Board Computers
  • More
  • Cancel
Single-Board Computers
Forum Wanted: sub-$10 *networked* boards
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Single-Board Computers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 25 replies
  • Subscribers 60 subscribers
  • Views 2703 views
  • Users 0 members are here
  • discovery
  • freescale
  • $10
  • networking
  • iot
  • st
  • launchpad
  • freedom
  • ti
Related

Wanted: sub-$10 *networked* boards

morgaine
morgaine over 12 years ago

The early part of this decade witnessed the rise of a new commercial phenomenon, the bringing to market of many sub-$10 evaluation, prototyping and hobbyist boards.  Although the terminology and market positioning has varied depending on the company, they're really all the same thing --- boards for enthusiasts, which serve the purposes of industrial evaluation equally well and also play a valuable company PR and device promotion role.  It's all one category really, and it's very sensible to roll these diverse purposes into one because of economies of scale, inventory reduction, and audience synergy.

 

Probably the greatest mindshare in this $10 (ballpark) area has been obtained by three companies so far:

 

  • Freescale with its Freedom boards FRDM-KL25Z and FRDM-KL46Z, featuring low-power Cortex-M0+.
  • ST with its STM32Fx-Discovery range, often given away free, featuring high performance Cortex-M4.
  • TI with its LaunchPad ranges, covering MSP430 (low power), C2000 (DSP), and Tiva/Hercules (ARM).

 

These devices are all, to summarize the $10 scene in a word, awesome. image  And that's probably understating it.

 

However, there is something missing from this excellent picture.  It's a very important thing, and it's very bad that it is missing:  networking.  This new millennium was built on a solid foundation of networking created in the latter part of the preceding one.  IP networking has so permeated our civilization today that its absence is as inconceivable as life without the telephone would have been in the preceding decades.  And yet despite this, the above three pillars of awesomeness live on isolated islands of non-communication.

 

Yes I know, it's quite easy to integrate them into an IP network, either through USB-based NICs or wifi adapters or using a small I2C-connected Ethernet or wifi board, or even Bluetooth or NFC, or even using SLIP over RS232 from days gone by.  But that's not the point.  The point is that they are not inherently connected, and so they have to be brought in from the cold.  This is more regrettable than it appears at first glance for several reasons.  It's a barrier to instant networking, it costs a lot more (there's a dollar penalty owing to unnecessary overheads), networking is not directly supported in the otherwise-awesome board's software, the add-ons dilute the manufacturer's own device promotion, and to be blunt, it's just annoying and not forward-looking.

 

I would recommend to manufacturers in this $10 (ballpark) space that 2014 be their year for networking everything in sight.  There's even a marketing angle for it --- the Internet of Things has acquired quite a lot of meme-space recently, and it's always a better idea to ride a wave rather than to stand in its way.  Sub-$10 networked boards would be extraordinarily synergistic to the IoT concept --- it shouldn't surprise anyone if hundreds of millions of a single board are sold, because $10 falls wells under the price-worry radar in the West at least.  I suspect the main limitation on sales would be effectiveness of promotion/advertising producing awareness, and not the price.

 

Come on Freescale, ST and TI (strictly in alphabetical order), add networking into this extremely cost-constrained niche, even if it's only 10Mbps.  You can do it.  And the rest of you manufacturers, don't worry about the incumbents ruling the roost.  Word of mouth and reblogging is the primary form of advertising today (I'm even doing it right here), and if you provide the goods, we'll spread the interest.

 

Morgaine.

  • Sign in to reply
  • Cancel

Top Replies

  • morgaine
    morgaine over 12 years ago in reply to johnbeetem +1
    John Beetem wrote: Morgaine Dinova wrote: Yes you do! Oh no, I don't Touche'! < Rest of infinite-length cultural exchange elided through Run-Length Encoding. > There are two kinds of…
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to morgaine +1
    Morgaine Dinova wrote: Your TV and TV usage would benefit enormously from full-capability IP networking. Actually it would be highly detrimental. As it would require owning a TV to begin with …
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to morgaine +1
    Morgaine Dinova wrote: There are in the universe these beings called "engineers", and they're not all stupid. In fact, many of them can focus on issues very clearly and ensure that certain requirements…
Parents
  • johnbeetem
    johnbeetem over 12 years ago

    USB hardware is very cheap (no magnetics, low power) and usually present all but the cheapest SoCs, so why not do IP over USB directly without messing around with Ethernet?  With 10baseT and higher you need an Ethernet hub or switch anyway, and you could fairly easily make an IPoUSB bridge/router that has a bunch of USB host ports to connect to your devices plus an Ethernet up-link.  The b/router would perform the polling needed to see if devices have upstream IP packets.

     

    I thought something like this might be a nice way to network a classroom filled with RasPi Model A boards.

     

    I've heard lots of talk about the Internet of Digital Things (IDioT), but I haven't seen standards or chips for handling the 'torking (my first neologism for 2014, an abbreviation of "networking" based on its common Internet mis-spelling "newtorking").

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 12 years ago in reply to johnbeetem

    John Beetem wrote:

     

    why not do IP over USB directly

    That sentence carries its own answer, by proposing an impossibility. image

     

    The serious answer though is that I dealt with (and eliminated) adding external USB-based NICs and Wifi adapters in my opening post.  My reason first and foremost is that if you have to add networking (over USB or through any other interface) then by definition it's no longer integrated, always present, running out of the box, expected by on-board software, and so on --- in other words, the board is not a networked device by design intent.  It's this design intent and matter of principle that I'm seeking --- that everything that isn't by design intent meant to be isolated should be networked, and networking in 2014 means IP.

     

    Specifically, a board with USB is not a networked board.  You can turn it into one, but that's a different kettle of fish.  Pi Model B is networked, but Pi Model A is not --- it's merely networkable.  Note also that this thread is about microcontroller boards because application processor boards are nowhere close to $10 at this stage of development.  We need to walk before we can run so I'm focusing on $10 networked microcontrollers initially as a baby step.

     

    There's an important secondary problem too:  when they have no integrated networking, microcontroller boards typically do not contain networking software built in either, so even if one accepted a not-out-of-the-box approach and added an external USB NIC, that would get you nowhere by itself.  It becomes a project in its own right to get them networked, instead of it being a default and well supported function.

     

    Note that I haven't eliminated integrated Ethernet or Wifi NICs sitting on a board's USB, in the manner employed on Pi Model B.  Although I agree that it's an option, I don't like that approach because of its high power consumption and poor performance (on Pi at least).  Worst of all though, and really the kiss of death for it, is that it requires quite a costly component.  Since this thread is about the sub-$10 market niche, integrating a USB-NIC or USB-Wifi device is going to be seriously difficult to achieve on cost grounds.  Even external PHY chips are problematic owing to cost, so a SoC providing both Ethernet MAC and PHY (like the old Stellaris Cortex-M3 and others) is really the way to go in this bottom-end niche.

     

    And a Happy New Year 2014 to you and all !!! image

     

    Morgaine.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • morgaine
    morgaine over 12 years ago in reply to johnbeetem

    John Beetem wrote:

     

    why not do IP over USB directly

    That sentence carries its own answer, by proposing an impossibility. image

     

    The serious answer though is that I dealt with (and eliminated) adding external USB-based NICs and Wifi adapters in my opening post.  My reason first and foremost is that if you have to add networking (over USB or through any other interface) then by definition it's no longer integrated, always present, running out of the box, expected by on-board software, and so on --- in other words, the board is not a networked device by design intent.  It's this design intent and matter of principle that I'm seeking --- that everything that isn't by design intent meant to be isolated should be networked, and networking in 2014 means IP.

     

    Specifically, a board with USB is not a networked board.  You can turn it into one, but that's a different kettle of fish.  Pi Model B is networked, but Pi Model A is not --- it's merely networkable.  Note also that this thread is about microcontroller boards because application processor boards are nowhere close to $10 at this stage of development.  We need to walk before we can run so I'm focusing on $10 networked microcontrollers initially as a baby step.

     

    There's an important secondary problem too:  when they have no integrated networking, microcontroller boards typically do not contain networking software built in either, so even if one accepted a not-out-of-the-box approach and added an external USB NIC, that would get you nowhere by itself.  It becomes a project in its own right to get them networked, instead of it being a default and well supported function.

     

    Note that I haven't eliminated integrated Ethernet or Wifi NICs sitting on a board's USB, in the manner employed on Pi Model B.  Although I agree that it's an option, I don't like that approach because of its high power consumption and poor performance (on Pi at least).  Worst of all though, and really the kiss of death for it, is that it requires quite a costly component.  Since this thread is about the sub-$10 market niche, integrating a USB-NIC or USB-Wifi device is going to be seriously difficult to achieve on cost grounds.  Even external PHY chips are problematic owing to cost, so a SoC providing both Ethernet MAC and PHY (like the old Stellaris Cortex-M3 and others) is really the way to go in this bottom-end niche.

     

    And a Happy New Year 2014 to you and all !!! image

     

    Morgaine.