Single-Board Computers
  • Products
  • Dev Tools
  • Single-Board Computers
  • More
  • Cancel
Single-Board Computers
Forum Intel Edison: Single Card Computer?
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Single-Board Computers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 42 replies
  • Subscribers 66 subscribers
  • Views 4592 views
  • Users 0 members are here
  • intel
  • soc
  • sbc
  • single_board_computer
  • quark
  • ces
  • iot
Related

Intel Edison: Single Card Computer?

fustini
fustini over 12 years ago

or should I say "Secure Digital Computer" image

image

Intel announced a new Quark dev board in the form factor of a SD card at CES.  Matt Richardson of Make reports:

 

Intel Edison: A Computer in an SD Card | MAKE

Intel’s new single board computer, Edison, takes on a familiar form factor. Jammed into an SD card, the 400MHz Quark processor on board has two cores, flash memory, and includes Wi-Fi and Bluetooth Low Energy for communication. It runs Linux on one core and a real time operating system on the other. You can program Edison by inserting the board into the SD card reader of your computer. The pins on the bottom of the board are capable of GPIO, UART, I2C, SPI, and PWM.

What do folks think?  My interest would depend on the price but the form factor is quite interesting.

 

 

Cheers from the Polar Vortex,

Drew

http://twitter.com/pdp7

  • Sign in to reply
  • Cancel

Top Replies

  • e14 Contributor
    e14 Contributor over 12 years ago +3
    Drew Fustini wrote: What do folks think? My interest would depend on the price but the form factor is quite interesting. Your interest should be tempered by the simple fact that it's x86. Looking at…
  • vsluiter
    vsluiter over 12 years ago +1
    Do they also make it in micro-sd ? Looks really cool though.
  • michaelkellett
    michaelkellett over 12 years ago in reply to vsluiter +1
    ARM had better look out - just compare the full-on power of the Intel marketing machine launching this board with the launch of the BBB. So far no detail on power or price but if they are competitive I…
Parents
  • GeorgeIoak
    GeorgeIoak over 12 years ago

    I just got back from CES and although there was big press about this board I was really expecting more of the booth to be dedicated to this and the Galileo. There was always a crowd around the board and the baby and coffee cup application examples. For those asking about uSD format, there's just no way to put everything into that small a format with everything has. I'm not sure I like the choice of using the SD format but I guess they were going for a known low cost form factor.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to GeorgeIoak

    George Ioakimedes wrote:

     

    I'm not sure I like the choice of using the SD format but I guess they were going for a known low cost form factor.

    Me neither, however as long as it behaves like a standard SD or SDIO card then there may be method behind the madness as it would save inventing some new interface and then trying to get others to buy into that idea.  Others have observed that getting embedded folks to agree on a common form factor is virtually impossible.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to GeorgeIoak

    George Ioakimedes wrote:

     

    I'm not sure I like the choice of using the SD format but I guess they were going for a known low cost form factor.

    Me neither, however as long as it behaves like a standard SD or SDIO card then there may be method behind the madness as it would save inventing some new interface and then trying to get others to buy into that idea.  Others have observed that getting embedded folks to agree on a common form factor is virtually impossible.