Single-Board Computers
  • Products
  • Dev Tools
  • Single-Board Computers
  • More
  • Cancel
Single-Board Computers
Forum PhoenixA20
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Single-Board Computers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 1 reply
  • Subscribers 57 subscribers
  • Views 258 views
  • Users 0 members are here
  • allwinner
  • allwinner_technology
Related

PhoenixA20

e14 Contributor
e14 Contributor over 12 years ago

No obvious end in sight, here's another Allwinner A20 board http://www.swiftboard.org/wiki/index.php?title=%E9%A6%96%E9%A1%B5

 

From: http://www.swiftboard.org/wiki/index.php?title=PhoenixA20_Over_View

  • ARM Cortex-A7 Dule-core(1 GHz)
  • 1G Bytes DDR3,4G Bytes On board Nand Flash,32G Bytes Micro SD card (extern)
  • UHD 2160P video decoding 3D video decoding;Support various video decoding formats, including VP8, AVS, H. 264 MVC, VC-1,MPEG-1,2,4, etc  ;H.264 HP video encoding up to 1080p@30 fps or dual-channel 720p@30 fps
  • HDMI,VGA,LVDS(extern),RGB(extern),CVBS(extern)
  • SATA 2.0 interface support 2.5’ HDD (for 3.5’ HDD, only need another 12V power input)
  • Camera interface,CSI
  • WIFI,Bluetooth 4.0,100M Ethernet
  • Extended pins including 3×UART,2×IIC,1×IIS,1×CVBS,4×TVIN,2×Line IN,1×SPDIF,2×PWM,2×LRADC,2×FMIN,1×Headphone,4×TVOUT、MIC、IR、TP
  • Support Android4.2.2+ and Linux3.4+

 

1GB may be on the low side now that we're seeing several boards with 2GB, but nice none the less.

PhoenixA20_main.jpg

  • Sign in to reply
  • Cancel
Parents
  • morgaine
    morgaine over 12 years ago

    Excellent, the more the merrier, and I'm very glad to see more boards move up from just 512MB of RAM to the new baseline of 1GB DDR3.

     

    Morgaine.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • morgaine
    morgaine over 12 years ago

    Excellent, the more the merrier, and I'm very glad to see more boards move up from just 512MB of RAM to the new baseline of 1GB DDR3.

     

    Morgaine.