Single-Board Computers
  • Products
  • Dev Tools
  • Single-Board Computers
  • More
  • Cancel
Single-Board Computers
Forum Pocket Ethernet and Network Tester
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Single-Board Computers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 15 replies
  • Subscribers 57 subscribers
  • Views 3278 views
  • Users 0 members are here
  • ethernet
  • test_and_measurement_equipment
  • networks
  • network
  • networking
  • test_and_measurement
Related

Pocket Ethernet and Network Tester

shabaz
shabaz over 12 years ago

Someone just showed me this link - I contributed straight away, it seems a great time-saver, and it has future software expansion capabilities. I wonder what others think about this product. There are still some 'early bird' offerings for those interested.

  • Sign in to reply
  • Cancel

Top Replies

  • e14 Contributor
    e14 Contributor over 12 years ago in reply to shabaz +1
    If it can work over usb, perhaps to a laptop rather than a phone that's all good. The reason the one you have is like that is that it works and has all the backup Michael mentioned, will survive all sorts…
  • shabaz
    shabaz over 12 years ago in reply to mcb1 +1
    Hi Mark, I think you're right, good as a general tool, not for commercial installers. I've been in some awful locations where people have been stepping on cables, wires are strung across racks etc. (so…
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to shabaz +1
    they usually start off like the first photo, but it takes discipline to keep them that way. I have a colleague whos purpose in life is to make the second photo seem neat
  • e14 Contributor
    e14 Contributor over 12 years ago

    Nice idea, shame about the reliance on bluetooth and a smartphone.

    Having been in a fair number of datacenters with my job, a good proportion don't allow phones, and an increasing number have installed shielding or suppression devices that render phones/bluetooth/wifi inoperational.  This might be the best bit of kit available, but what do you do with it when your phone is sitting in a box in the security station ?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 12 years ago in reply to e14 Contributor

    Very good points. The strength of using the smartphone for controlling it and analyzing the data is also it's weakness if it cannot be used : ( I suppose a tablet with no mobile connectivity could be used, but then that destroys much of the convenience if you have to carry that around too.

    I wonder if we can talk to them about including a USB capability for direct connectivity to a smartphone, to at least eliminate bluetooth issues. I'll e-mail them, see what they say and report back.

    Most equipment racks I've worked on have been open-frame (in development labs), but then I've not been in many datacenters and caged/shielded racks would be a problem : (

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • michaelkellett
    michaelkellett over 12 years ago in reply to shabaz

    Like so many crowdfunded launches there just isn't enough technical data published to feel convinced. If you buy a network tester from a normal supplier you can expect a spec with things like the battery size, operating temperature range etc etc all quoted. This thingy might be OK but it isn't being presented in a professional way. I suspect that if it were, and by the time all the backup and support you get from one of the established suppliers is added, it wouldn't be much cheaper.

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 12 years ago in reply to michaelkellett

    Hi Michael,

    I think you're right. A few have some interesting price-features mix where alternatives are vastly expensive but the points are valid. Someone should write a product launch book for projects - actually I'm sure that exists I may have one. I'm going to try to get more data out of them. I got a fairly positive response back about USB will post later tonight (on mobile, hard to type image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 12 years ago in reply to e14 Contributor

    Hi Selsinork,

     

    The response back concerning USB is that the connector is physically there, currently used for charging, and that over USB they also ran the same protocol that they are using over Bluetooth during h/w development, so this use-case may work out. They are trying to stay focussed on the main features, because they are getting new use-cases every day.

    So, it could work out positively. They appreciated the suggestions.

    I currently have a very old 'luggable' test tool at work (can't recall the manufacturer, but it is huge, blue, the size of a brick x 2 halves image but this new pocket tester will far exceed that tool functionality, assuming it functions well.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to shabaz

    If it can work over usb, perhaps to a laptop rather than a phone that's all good.

     

    The reason the one you have is like that is that it works and has all the backup Michael mentioned, will survive all sorts of rough handling etc. There's a certain if it's not broke thing going on there. Even so, new technology comes along and makes things smaller, faster, more accurate, more feature packed.. which is a good thing.

     

    For something that should be a serious engineering tool I agree with Michael, concentrate more on the professional, less on the shiny.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 12 years ago

    There have been some updates, I'm just getting up-to-speed on them now.

    A type of remote terminator device will be included, and some IOS support for those with iPhones (prior it was Android-only) - apparently IOS needs Bluetooth v4.

    They have a short physical/electrical spec (not much there):

    90x65x25 mm | 200 g | Micro-USB charge | 8 hours operating time on battery
    Voltage measurement up to 110V | Input protection | TDR range up to 400m

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to shabaz

    Ok, so I'll ask the obvious.  This is an Ethernet cable tester ?  Ethernet cable installed to spec shouldn't be over 100m, 90m fixed and two 5m patch cables.  So why a 400m TDR ?  Wouldn't 150m be a better range, especially if you can be more accurate that way.  If the TDR can't find the end/fault then you know what's wrong - your installation is out of spec!

     

    I realise it's never quite so black and white, and that ethernet may work on longer cable - but you should not be planning on installing something like that.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 12 years ago in reply to e14 Contributor

    I wondered why too : ) Probably a technical limitation of the tool rather than a practically experienced one. I've been in situations where the building is huge but where 100m should be ok, but since it traverses to patchrooms and back the 100m is exceeded and it's often not known with existing cabling without invoking the built-in TDR in switches. So an idea on length is good, but 400m does seem excessive : ) I suppose it may be possible to figure out the length of cable on a huge drum (don't know if that's a likely or unlikely use-case for installers or not - personally I'd measure out an amount of cable if it was going to be long, and hence know what's left).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to shabaz

    Typically 305m / 1000ft on a reel, so that's possible. Having to terminate the cable would seem to make it less likely.

     

    If it's a decent TDR, it should really be able to tell you where it sees 'features' in the cable. That ought to get you to things like where the discontinuities at patch panels are, or to things like a cable being cable tied to a metal tray tightly enough that some sharp bit of metal has pierced the cable and is shorted to just one conductor of the pair - but no actual break.

    Not being able to do stuff like that means your cable fault finder just isn't very good, no matter the manufacturer...

     

    Of course it's also possible that the TDR device they're using has good accuracy out to some silly distance just because of general improvements in the technology, but we'd need to know more than just range to even guess if that's the case.  Would you rather have 400m range, +-4m accuracy, or, 100m +-1m ?  Yes, of course, 400m +-10cm would be even better image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
>