Single-Board Computers
  • Products
  • Dev Tools
  • Single-Board Computers
  • More
  • Cancel
Single-Board Computers
Forum pcDuino v3
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Single-Board Computers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 2 replies
  • Subscribers 57 subscribers
  • Views 854 views
  • Users 0 members are here
  • allwinner
  • a20
  • pcduino
Related

pcDuino v3

e14 Contributor
e14 Contributor over 12 years ago

I just noticed that a new pcDuino with an A20 SoC will be released soon. I have a pcDuino v1 and an A20-Olinuxino-Micro, so this board may be of interest to me.  I'd be curious to know if anyone is working on a board with an A31 or A80 SoC.  I know Allwinner has an A80 board that they provide to tablet developers, but I don't think just anyone can buy one.

 

pcDuino V3 » pcDuino

  • Sign in to reply
  • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago

    The PCDuino v3 seems like it could be interesting as it now has SATA and gigabit ethernet. Thanks for pointing it out.

     

    From what I've read over on the linux-sunxi mailing list it seems that neither A31 or A80 will have SATA and as such they are much less interesting. There are however patches being submitted for A31 which suggest there are boards available somewhere.

    The only A80 one that appears to be around is the Optimus http://liliputing.com/2013/12/allwinner-a80-optimus-board.html but I've no idea if they're available to buy anywhere as yet.

    A80 also seems to use a PowerVR GPU, that likely means Android will be the only useful choice of OS unless you don't want a display image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to e14 Contributor

    I have already got the board, but they call it pcDuino3 not pcDuino v3.

    It is available at sainsmart and LinkSprite for $77.99, a little expensive than raspberrypi.

    Anyway, if you take it as a pc, then it is totally worth the price.

    tumblr_n3g9zj51Cg1sqiwwyo4_500.jpg

    tumblr_n3g9zj51Cg1sqiwwyo2_500.jpg