Single-Board Computers
  • Products
  • Dev Tools
  • Single-Board Computers
  • More
  • Cancel
Single-Board Computers
Forum Meet MinnowBoard MAX
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Single-Board Computers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 14 replies
  • Subscribers 60 subscribers
  • Views 2336 views
  • Users 0 members are here
  • minnowboard
Related

Meet MinnowBoard MAX

e14 Contributor
e14 Contributor over 12 years ago

Meet MinnowBoard MAX | minnowboard.org

 

Maybe they've realised the original MinnowBoard was too little, too late, too expensive..  $99 for the base Max looks mildly more interesting, but it needs to be a lot faster and much less power hungry if it's to get close to the current Arm boards.

  • Sign in to reply
  • Cancel

Top Replies

  • johnbeetem
    johnbeetem over 12 years ago +1
    There's a good write-up of MinnowBoard Max at LinuxGizmos: http://linuxgizmos.com/intel-unveils-tiny-x86-minnowboard-max-open-sbc/ It sounds like MB Max has much better software support than the original…
  • prpplague
    prpplague over 12 years ago +1
    The original MinnowBoard was nothing more than a learning exercise for both Intel and Circuitco. Intel needed to learn a few things about open hardware, and circuitco needed to learn about x86 hardware…
  • prpplague
    prpplague over 12 years ago in reply to johnbeetem +1
    john, yes indeed the plains on the original minnow were swiss cheese..... you can download the gerbers for a view if you'd like, hehe the Max indeed supports more standard distributions such as ubuntu…
Parents
  • johnbeetem
    johnbeetem over 12 years ago

    There's a good write-up of MinnowBoard Max at LinuxGizmos: http://linuxgizmos.com/intel-unveils-tiny-x86-minnowboard-max-open-sbc/

     

    It sounds like MB Max has much better software support than the original Minnow.  It also has SATA: one dedicated connector and a second off the high-speed connector, which also provides PCIe.  [Update #2: You also get SATA and PCIe with original Minnow, but not with RasPi or Beagle.]  MBMax can have dual core for US$129.  The MB Max cores are 64-bit, if that's of importance.

     

    Update #1: They've also cut way back on the number of passives that they had on the original.  IMO the original board must have had inner layers that looked like Swiss Cheese, or else so many blind vias that the PC board itself was a major product cost.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • prpplague
    prpplague over 12 years ago in reply to johnbeetem

    john,

     

    yes indeed the plains on the original minnow were swiss cheese..... you can download the gerbers for a view if you'd like, hehe

     

    the Max indeed supports more standard distributions such as ubuntu and fedora as compared to the original minnow which was somewhat specific to the angstrom builds...

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to prpplague

    David Anders wrote

    the Max indeed supports more standard distributions such as ubuntu and fedora as compared to the original minnow which was somewhat specific to the angstrom builds...

    Not sure I understand that comment, I booted angstrom on my original minnow for all of about a minute - just long enough to prove that it booted, before switching to a sensible distro. Other than UEFI there's nothing much unusual about the original. Whatever way you look at it, x86 is just x86.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to prpplague

    David Anders wrote

    the Max indeed supports more standard distributions such as ubuntu and fedora as compared to the original minnow which was somewhat specific to the angstrom builds...

    Not sure I understand that comment, I booted angstrom on my original minnow for all of about a minute - just long enough to prove that it booted, before switching to a sensible distro. Other than UEFI there's nothing much unusual about the original. Whatever way you look at it, x86 is just x86.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • prpplague
    prpplague over 12 years ago in reply to e14 Contributor

    selsinork,

     

    there were a lot of special kernel aspects to the original minnowboard, but the biggest issue is the stock distributions that do support UEFI only support 64-bit UEFI which made it much more difficult to install stock distros. we've specifically made sure that stock distros will work out of the box for minnowboardmax..

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to prpplague

    David Anders wrote:

     

    there were a lot of special kernel aspects to the original minnowboard, but the biggest issue is the stock distributions that do support UEFI only support 64-bit UEFI

    Not entirely sure I agree, sure there are things on the Minnow you don't tend to find on more 'normal' x86 boards, so the distros don't tend to include them. So you need to be prepared to do a bit of work yourself.

    UEFI being 32bit is only really a problem if you're the sort of person who just wants to install from CD and have everything handed to them on a plate and I suspect very few people who bought one were in the "I have an RPi and can't work out Win32DiskImager" category.

     

    You might have guessed that I'm fairly self sufficient in these sorts of things image