Single-Board Computers
  • Products
  • Dev Tools
  • Single-Board Computers
  • More
  • Cancel
Single-Board Computers
Forum Cloud9
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Single-Board Computers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 6 replies
  • Subscribers 59 subscribers
  • Views 812 views
  • Users 0 members are here
Related

Cloud9

e14 Contributor
e14 Contributor over 12 years ago

In the new Debian release is there documentation anywhere of the changes made to the Cloud9 environment?  Or maybe an update to "Getting started with Beaglebone"?

  • Sign in to reply
  • Cancel

Top Replies

  • jkridner
    jkridner over 12 years ago +1
    Yes, it can handle running all the PWMs at once. You need to be careful that you aren't using the same PMW on two different pins. Using two different signals out of the same PWM requires you to use the…
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to jkridner +1
    I did get it to work after commenting out 2 of the three in the code and bringing them one at a time. I'm using EHRPWM0. EHRPWM1 and EHRPWM2, it looks like each one can feed two output pins, but it seems…
Parents
  • jkridner
    jkridner over 12 years ago

    Yes, it can handle running all the PWMs at once. You need to be careful that you aren't using the same PMW on two different pins. Using two different signals out of the same PWM requires you to use the same frequency.

     

    Please paste your problematic code.

     

    I don't think there is a way to bring back the disk icon. File --> Save provides a guide saying where it will save, but you have to be paying attention to it. Agree it would be nice to update the book.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • jkridner
    jkridner over 12 years ago

    Yes, it can handle running all the PWMs at once. You need to be careful that you aren't using the same PMW on two different pins. Using two different signals out of the same PWM requires you to use the same frequency.

     

    Please paste your problematic code.

     

    I don't think there is a way to bring back the disk icon. File --> Save provides a guide saying where it will save, but you have to be paying attention to it. Agree it would be nice to update the book.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Children
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to jkridner

    I did get it to work after commenting out 2 of the three in the code and bringing them one at a time. I'm using EHRPWM0. EHRPWM1 and EHRPWM2, it looks like each one can feed two output pins, but it seems to be fussy which one you pick and that's even related to which other PWMs you're using.  I did get it going after a lot of trial and error with the pin assignment.

    Tom