Single-Board Computers
  • Products
  • Dev Tools
  • Single-Board Computers
  • More
  • Cancel
Single-Board Computers
Forum Unmanned Submarine
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Single-Board Computers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 10 replies
  • Subscribers 59 subscribers
  • Views 1219 views
  • Users 0 members are here
  • aurdino
  • raspberry-pi
  • beaglebone-black
Related

Unmanned Submarine

e14 Contributor
e14 Contributor over 11 years ago

I'm new to the single board processor hobby but I am working on an idea of an unmanned exploratory submarine.  Requirements would be GPS, Camera with small LED light for underwater pics, capability of location transmitting and solar cell for self recharging.  Would like to be able to launch to a coordinate and have it return days later, taking  pics along the way and self surfacing to recharge as well.  Any ideas or suggestions?

  • Sign in to reply
  • Cancel
  • Robert Peter Oakes
    Robert Peter Oakes over 11 years ago

    Not sure how well the GPS will work underwater. H2O is a great attenuator, that's why subs have to send things up to the surface to establish communications etc.

     

    There was a documentary I watched a couple of years ago where a group created an autonomous sub and sent it across the Atlantic on its own none stop. Cant remember the name of it but Im sure a Google search would soon find it for you

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to Robert Peter Oakes

    I looked at their project and yes the gps signal would have to be transmitted once it surfaces.  Probably have to program some dead reckoning type logic for the subsurface course.  So I guess it would also require a compass and a way to measure drift/current/speed.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Robert Peter Oakes
    Robert Peter Oakes over 11 years ago in reply to e14 Contributor

    Quad Copters have all the sensors you may need

     

    Accelerometers to detect drift and turns to help with direction and inclination, barometer for depth sensing or other model pressure transducer

     

    GPS for when surfaced to re-set the dead reconing system

     

    How deep are you planning on going with this

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to Robert Peter Oakes

    Yes I also found a trial test of the glide type AUV's (like the one Rutgers launched) which listed the manufacturer of the electronics they used.  Checked their website and waiting on some pricing.  Only plan on going as deep as needed to avoid boats and shipping, so prob 50'.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • jw0752
    jw0752 over 11 years ago

    Hi Tom, It might make sense to plan for surface travel except when it gets to areas of interest. On the surface you could use GPS for navigation and a satellite phone for communications as well as solar for energy. Under the water you would have difficulty even detecting if you were in a current or not. I am sure that there is mapping of major ocean currents that could be used for estimating drift. How big are you planning on making this submarine? Size is a consideration as scaling smaller reduces volume needed for battery capacity and infrastructure. This is illustrated by the reduction in range of small drones as compared to the large ones.

    Good luck, ideas like this are fun to think about.

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to e14 Contributor

    Actually depth will have to be variable due to reefs and shallows here in South Florida until out in open water.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to jw0752

    Wanted to stay sub surface as much as possible only surfacing for solar recharging and position checks.  Wanted to keep it small as possible. No more than 1 meter in length hopefully.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Robert Peter Oakes
    Robert Peter Oakes over 11 years ago in reply to e14 Contributor

    50' is a lot of pressure, meaning thick walls and less room for kit

     

    Waterproofing will be a big challenge as many parts will require external mounting with holes for wiring to get through to main part of sub

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to Robert Peter Oakes

    Made a propulsion type system once for diving using PVC and lexan.  It was able to stand more pressure then I will need at 50' little less than 44 psi.  Yes it will be challenging to maintain water tight integrity with any penetrations so the fewer the better.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • jw0752
    jw0752 over 11 years ago

    Here is a link to a book about the technology on AUVs that might be of interest.  http://www.amazon.com/dp/0415301548/ref=asc_df_04153015483180506?smid=ATVPDKIKX0DER&tag=pg-1583-86-20&linkCode=df0&creative=395097&creativeASIN=0415301548    . The specification of 1 meter in length coupled with the need to keep the shape hydrodynamic will limit your space for batteries. You might get an hour between needing charges. You will also have to have a high pressure air supply on board to control depth with ballast. This will be a consumable resource and will limit the number of times you can go up and down unless you have room for a high pressure compressor and related support mechanisms. Your other option is to have the sub slightly positively buoyant so that it will naturally float to the surface. The disadvantage to this is that it will have to use its planes to pull itself underwater and this will increase the resistance in the water and shorten the distance between recharges. When one starts to think about all the complications it makes you really appreciate the advantage of a biological organism like a fish that can swim and dive for years, pull its fuel from the environment, and probably know exactly where it is all the while.

    John