Single-Board Computers
  • Products & Partners
  • Dev Tools
  • Single-Board Computers
  • More
  • Cancel
Single-Board Computers
Forum What do you know about km2m806-02 Kontron IoT Platform ?
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Single-Board Computers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 5 replies
  • Subscribers 59 subscribers
  • Views 1912 views
  • Users 0 members are here
  • km2m806
  • intel
  • kontron
  • atom
  • iot
  • km2m806-02
Related

What do you know about km2m806-02 Kontron IoT Platform ?

rzr
rzr over 11 years ago

I've just got one and plan to review it ... so any questions are welcome. Also I havent found much manuals , but as Linux hacker I will figure it out


http://www.kontron.jp/downloads/datasheet/datasheet_m2m.pdf Keep in touch : https://twitter.com/RzrFreeFr

 

 

Specifications : http://www.kontron.jp/downloads/datasheet/datasheet_m2m.pdf

M2M Smart Services Developer Kit

 

Simply connected

 

- Ready-to-run M2M platform

- Broad connectivity for efficient enterprise solutions

- Ample performance for a wide range of application tests

- Qualified by multiple carriers

 

M2M Smart Services Developer Kit

The Kontron M2M Smart Services Developer Kit offers efficient enterprise

solutions by enabling faster time-to-market with quick development and

deployment of M2M applications.

 

The Kontron Developer Kit was especially designed for deployment in

laboratories and for test installations in office and home environments.

Due to its fl exible chassis concept, adaptation is simplified, which

translates into faster time-to-market. Using the Intel Atom E600 series

processor provides high performance for a wide range of application

tests.

 

Kontron's M2M Smart Services Developer Kit is designed for developers

who need a simple development platform for quick solutions. After

unpacking, the device is immediately ready to go and can be used for

developing numerous applications.

 

The pre-installed Operating System ensures drivers are installed and available, no more searching for drivers!

 

Its 0-50c temperature range makes it adaptable to almost all application

areas. 802.11a/b/g/n WLAN and 802.15.4 WPAN support is standard in

 

Kontron's M2M Smart Services Developer Kit.

Further, the modules are also equipped with an accelerometer, 2x microHDMI, Audio, 1x Gigabit

Ethernet, and USB 2.0.

 

Product Kontron M2M Smart Services Developer Kit

 

Chassis Dimensions (H x W x D) 67 x 100 x 27mm (92 x 100 x 62mm with mounting brackets)

 

Interfaces Top SIM slot

Interfaces Left USB 2.0 (Type A), MicroUSB 2.0 (Type B), Power, RJ-45 Ethernet, 2x antenna connectors

Interfaces Right Microphone, Headphone/Line Out, 2x MicroHDMI, MicroSD slot, MicroUSB 2.0, 2x antenna connectors

 

Controls on top Reset button, user input button/software enabled, LED status indicators

Internal Data Storage capacity 4 GB via internal MicroSD card

External Power Supply 12 VDC, 2A operating input/rating

Processor/Chipset IntelRegistered AtomTM processor E620 600MHz

Cache 32 KB instruction cache + 24 KB L1 cache, 512 KB L2 cache

Memory 1 GB DDR2

Wi-Fi WLAN (802.11b/g/n) IntelRegistered CentrinoRegistered Advanced N 6205 Wi-Fi module installed

WPAN (802.15.4) TI CC2531 SOC; ready for ZigBeeRegistered certifi cation or for 6LoPAN or Wireless HART WPAN use

3G/4G WWAN Ericsson 3G module installed or other PCI Express 3G/4G broadband module on request

Expansion (for non-3G option SKU) 1 PCIe MiniCard slot for WWAN 3G/4G broadband module (certifi cation/drivers needed) or solid state disk addition

Accelerometer Ultra low-power high performance three axis linear accelerometer

 

Weight 0.8 lb/0.36 kg system; 2.35 lb/1.1 kg packaged kit

Temperature Operating: -0°C to +50°C, Storage: -25°C to +70°C (-13°F to 158°F)

Humidity Operating: 5 to 95 % RH @ 25-35°C non condensing

Shock Operating: 2G 11ms duration, 6 directions (half-sine), Non-operating: 25G 11ms duration, 6 directions (half-sine)

Vibration Packaged: 2G 5-40 Hz: sloping to 0.00015 g2/Hz@ 500 Hz; Unpackaged system: 5-500 Hz: 0.5G sine / 3 axis

Approvals Nemko NRTL 60950-1, FCC Class B, CE, PTCRB certifi ed

 

OS Wind River Intelligent Device Platform 1.0 1.6 – 90 day trial; 2x 3G antennas (on request)

 

Also in the Box 2x 3G antennas (including cabling), 2x 802.11/802.15.4 antennas, 16 GB USB Memory stick with Wind

River Linux LiveUSB and USB adapter, 90-240VAC PSU

 

For additional information www.kontron/M2M

Ordering Information

Article Description

KM2M806-01 Kontron M2M Smart Services Developer Kit (WiFi only)

KM2M806-02 Kontron M2M Smart Services Developer Kit (3G HSPA)

KM2M806-08 Kontron M2M Smart Services Developer Kit (3G CDMA)

KM2M806-09 Kontron M2M Smart Services Developer Kit (4G LTE)

CORPORATE OFFICES

Europe, Middle East & Africa North America Asia Pacifi c

Lise-Meitner-Str. 3-5

86156 Augsburg

Germany 14118 Stowe Drive

Poway, CA 92064-7147

USA 17 Building,Block #1, ABP.

188 Southern West 4th Ring Road

Beijing 100070, P.R.China

Tel.: + 49 (0) 821 4086-0

Fax: + 49 (0) 821 4086 111

sales@kontron.com Tel.: + 1 888 294 4558

Fax: + 1 858 677 0898

info@us.kontron.com Tel.: + 86 10 63751188

Fax: + 86 10 83682438

info@kontron.cn

2

www.kontron.com

purposes.

inaccurancies.

Technical Information

http://www.windriver.com/products/intelligent-device-platform/

  • Sign in to reply
  • Cancel

Top Replies

  • e14 Contributor
    e14 Contributor over 10 years ago in reply to rzr +1
    I didnt recieve the USB dongle with the linux distro either.. I assumed because it was free it wasnt going to include that.. Have you guys figured out a distro that will have most of the driver support…
  • e14 Contributor
    e14 Contributor over 10 years ago +1
    Is this thread dead?? A bunch of people got theese today in the mail, they are discussing on reddit. has anyone been able to load another distro? does anyone have a link to a clean image to restore unit…
Parents
  • Pavel.Simon
    0 Pavel.Simon over 11 years ago

    Hi, any news on it?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • rzr
    0 rzr over 11 years ago in reply to Pavel.Simon

    Not much I have it and can share some info


    CPU : E620 32bit    http://ark.intel.com/products/52491/Intel-Atom-Processor-E620-512K-Cache-600-MHz http://ark.intel.com/products/codename/37567/Tunnel-Creek


    grep proc  /proc/cpuinfo processor      : 0 processor      : 1 model name      : Intel(R) Atom(TM) CPU E620  @  600MHz


    On mine I have an Old Fedora on MMC


    cat /proc/version Linux version 3.2.22-5.M2M.recovery.fc14.i686 (mockbuild@server) (gcc version 4.5.1 20100924 (Red Hat 4.5.1-4) (GCC) ) #1 SMP Mon Nov 19 17:46:20 MSK 2012



    I dont have Windriver Linux Eval usbkey supposed to be along, do you ?


    I'll be curious to know about it


    https://marketplace.windriver.com/index.php?bsp&on=list&type=architecture&value=x86/Pentium/IA-32/IA-64

    https://marketplace.windriver.com/index.php?bsp&on=details&bsp=11787

    Feel free to comment if you own it

    Resources : https://embedded.communities.intel.com/docs/DOC-7501#comment-1375

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • rzr
    0 rzr over 11 years ago in reply to Pavel.Simon

    Not much I have it and can share some info


    CPU : E620 32bit    http://ark.intel.com/products/52491/Intel-Atom-Processor-E620-512K-Cache-600-MHz http://ark.intel.com/products/codename/37567/Tunnel-Creek


    grep proc  /proc/cpuinfo processor      : 0 processor      : 1 model name      : Intel(R) Atom(TM) CPU E620  @  600MHz


    On mine I have an Old Fedora on MMC


    cat /proc/version Linux version 3.2.22-5.M2M.recovery.fc14.i686 (mockbuild@server) (gcc version 4.5.1 20100924 (Red Hat 4.5.1-4) (GCC) ) #1 SMP Mon Nov 19 17:46:20 MSK 2012



    I dont have Windriver Linux Eval usbkey supposed to be along, do you ?


    I'll be curious to know about it


    https://marketplace.windriver.com/index.php?bsp&on=list&type=architecture&value=x86/Pentium/IA-32/IA-64

    https://marketplace.windriver.com/index.php?bsp&on=details&bsp=11787

    Feel free to comment if you own it

    Resources : https://embedded.communities.intel.com/docs/DOC-7501#comment-1375

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to rzr

    I didnt recieve the USB dongle with the linux distro either..

     

    I assumed because it was free it wasnt going to include that..

     

    Have you guys figured out a distro that will have most of the driver support built in?

     

    -Doug