Single-Board Computers
  • Products
  • Dev Tools
  • Single-Board Computers
  • More
  • Cancel
Single-Board Computers
Forum beaglebone metal detector
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Single-Board Computers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 5 replies
  • Subscribers 58 subscribers
  • Views 1010 views
  • Users 0 members are here
Related

beaglebone metal detector

e14 Contributor
e14 Contributor over 10 years ago

hi i am trying to build a special type of metal detector called a constant current metal detector. i need to use 7 gpio's to and turn some on transistors and some off in a repeating pattern. i will show a table at the bottom to make things more easier understand what iam trying to do each of the 7 gpio's are responsible for turning on transistor or turning it off switch  s57,s58,s59,s60,s61,s62,s63 to s64 are each equivalent to one gpio all the logic states are repeated after the whole cycle has finished. as i see it i can look at it this way if i chose s57 which was gpio60 i would have to put a if statement so   it would not just turn the gpio60 on again before the first iteration had finished

S57 S58 S59 S60 S61 S62 S63 S64
onoffoffonn/aonn/aoff
onoffoffonn/aoffn/aon
offononoffonn/aoffn/a
offononoffoffn/aonn/a.
offoffononononoffoff
offoffonononoffoffon
offoffononoffononoff

 

  • Sign in to reply
  • Cancel
Parents
  • shabaz
    shabaz over 10 years ago

    Hi Anthony,

     

    I didn't try to follow the pattern (hint: it would have been easier to follow with colored squares!) however surely any microcontroller or processor can be used for this?

    If you're asking how to implement it, you could create an array and step through it using a for loop perhaps, and repeat forever.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • shabaz
    shabaz over 10 years ago

    Hi Anthony,

     

    I didn't try to follow the pattern (hint: it would have been easier to follow with colored squares!) however surely any microcontroller or processor can be used for this?

    If you're asking how to implement it, you could create an array and step through it using a for loop perhaps, and repeat forever.