Single-Board Computers
  • Products
  • Dev Tools
  • Single-Board Computers
  • More
  • Cancel
Single-Board Computers
Forum Is it possible to get a POWER-based SBC?
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Single-Board Computers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 11 replies
  • Answers 6 answers
  • Subscribers 60 subscribers
  • Views 6465 views
  • Users 0 members are here
  • solidrun
  • sbc
  • nxp
  • power
  • ibm
Related

Is it possible to get a POWER-based SBC?

ullbeking
ullbeking over 6 years ago

Hello,

 

I am interested in the POWER ISA, and I know about projects such as Talos II (https://raptorcs.com/content/TL2WK2/intro.html) and Microwatt (https://github.com/antonblanchard/microwatt), and so on.

 

I would like to experiment with POWER-based SBC's.  They don't have to be POWER9 because I've already got that particular CPU covered in the form of my Talos II (although still a work in progress to get it provisioned properly).

 

I would like to purchase a few POWER-based SBC's and build a small, quiet cluster.  The intended use cases are as follows:

  • general purpose computing
  • digital signal processing
  • self-education about:
    • POWER ISA
    • clusters and distributed computing, including HA
    • formal reasoning about the state of a distributed system

 

So far I have found

  • NXP is producing interesting POWER SoC's (https://www.nxp.com/products/processors-and-microcontrollers/power-architecture:POWER-ARCHITECTURE)
  • Solid Run is producting SBC's of the "NXP family" but none of these include POWER CPU's (https://shop.solid-run.com/product-category/embedded-computers/nxp-family/)

 

I am continuing to researcg, but if you know of anybody who is producing POWER-based SBC's then I would be greatly appreciative if you could please, please let me know.  Thank you!!

 

Kind regards,

 

Andrew

  • Sign in to reply
  • Cancel

Top Replies

  • gdstew
    gdstew over 6 years ago in reply to clem57 +2 suggested
    I'm just replying to the original post. I just happened to know about this one and after verifying that it was still available, passed it on to Andrew. I would imagine that there is some interest in Power…
  • e14 Contributor
    e14 Contributor over 6 years ago +1
    Something that might amuse Power fans: https://itsfoss.com/linux-powerpc-notebook-project/ It's still active: https://gitlab.com/oshw-powerpc-notebook/powerpc-laptop-mobo
  • ullbeking
    ullbeking over 6 years ago in reply to gdstew +1 suggested
    Thank you gdstew , this information is very helpful. In fact, I think that looking at PPC32-based SBC's would be most fruitful, and these are some excellent starting points. Re: Raptor's Talos II, I actually…
Parents
  • gdstew
    0 gdstew over 6 years ago

    I'm not sure what the difference between Power and Power PC is however you can get a relatively inexpensive Power PC SBC here:

    https://www.directron.com/efika.html

     

    Here are a couple more links to useful information:

    https://genesi.company/products/efika/5200b

    https://genesi.company/support/efika

     

    They have some interesting features including a PCI slot and a ATA/IDE hard drive interface however they lack any GPIO. You could find a PCI bus parallel

    printer card to provide some GPIO and the last generation of parallel printer interfaces came with EPP and EPC modes that include much more powerful

    interface  capabilities. I have no idea if there are usable Linux drivers for these interfaces anymore but at one time they were used for zip drives and other

    peripherals so there might be, There should be drivers for the standard and bi-directional modes for the printer interface (these are usually supported on

    cards with the advanced modes too) which would give some GPIO capabilities. Finally It does have 2 - USB 1 interfaces which can also be used with other

    interface boards for GPIO.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • clem57
    0 clem57 over 6 years ago in reply to gdstew

    gdstew good to know. But this is a reseller only market. I wonder how large is the interest in this architecture.

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • gdstew
    0 gdstew over 6 years ago in reply to clem57

    I'm just replying to the original post. I just happened to know about this one and after verifying that it was still available, passed it on to Andrew. I would

    imagine that there is some interest in Power (more likely PowerPC) based SBC's but have no idea if there is enough to sustain a market for them at prices

    that are fairly close to ARM offerings. I'm sure there are some out there that would be willing to pay something extra for the PowerPC just to work with it.

     

    Just FYI

     

    There is a Power9 based PC called the Raptor Talos II Lite (there is also a dual CPU socket server version) that was recently released. Base price is

    $1399 USD without a CPU (motherboard + PSU + case + heatsink). The CPU costs (all USD) are for 4-core POWER9 CPU - $375, 8-core CPU - $595,

    18-core CPU - $1375, and 22-core CPU - $2575. Although these prices are on the high side if I had a spare few thousand dollars laying around I would

    be very tempted to buy one.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • ullbeking
    0 ullbeking over 6 years ago in reply to gdstew

    Thank you gdstew, this information is very helpful.  In fact, I think that looking at PPC32-based SBC's would be most fruitful, and these are some excellent starting points.

     

    Re: Raptor's Talos II, I actually have one of these (https://www.raptorcs.com/content/TL2WK2/intro.html) and there have been a few teething issues but finally it's getting sorted.  I intend for this to be my primary workstation+server, and once I get some issues with PSU's sorted out, (touch wood) I hope that I will be ready to put it into production.  It's an amazing machine, but you have to really care about what it offers you for it to be a good investment.

     

    And because the Talos II is so large, I would like a smaller, SBC-sized machine or cluster of SBC-sized machines to learn the fundamentals of working with this architecture and ISA.  The Blackbird would be a great machine for a quiet workstation.  I intend to get one of those too but not until the Talos II is working 100%.

     

    It's very late here now (London, UK) and I'd better get to bed.  Thank you all for your answers.  I'll be coming back to this thread tomorrow.  Good night all!!

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 6 years ago in reply to ullbeking

    I do not know your motivation for investing in Power technology as a "primary workstation+server" nor am I challenging it.  I was also a Unix PPC developer in years long past and found them to be just as good as DEC VAX or Intel-based systems.  But, as you can see on the Internet, manufacturers interested in small products are abandoning Power technologies (or never considered them) in favor of ARM, Intel, or AMD.  Its all about money and momentum.

     

    Regarding the Genesi company (https://genesi.company/aboutus ), they seems focused on (freescale today) ARM-based hardware.  For example, https://genesi.company/products/efika/5200b (discontinued), they state: "The 5200B-based version of the EfikaPPC mainboard has been discontinued and was replaced with the EFIKA MX. While the EfikaPPC is no longer in stock at Genesi, it is still available with resellers."  EFIKA MX (also discontinued) is ARM-based.  Actually, a lot of their products and "Projects" have been discontinued.  That is a bit worrying to me.

     

    Power architecture-based products may see a resurgence in the future but that is speculation on my part.  I suspect that IBM is trying to salvage their investment in the i-Series. 

    Keep an eye on https://openpowerfoundation.org/the-next-step-in-the-openpower-foundation-journey/

     

    In the UK:   https://www.broadberry.co.uk/tyan-rackmount-servers   You might investigate Broadberry for leads.

    Tyan has been manufacturing Power-based products using Broadberry and others as distributors.

    It looks like all of the new and continuing Power-based development is focused on rack and server.

     

    Whatever you decide to do, I suggest avoiding discontinued, ebbing, or inactive products so as to continue getting consumer support in terms of documentation, user forums, and product updates.

    Good luck.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • gdstew
    0 gdstew over 6 years ago in reply to ullbeking

    Hi Andrew,

     

    In case you are not aware of it this web site https://www.phoronix.com/scan.php?page=home  has been covering the Talos workstations for over a year now.

    There are quite a few articles about both versions that may have useful information about the problems you are having. The owner and pretty much only

    contributor of the web site articles has run a series of in depth benchmarks on the server version which indicates a fully working system. I do remember him

    having some teething problems too but I do not remember any of the specifics.

     

    What a coincidence, I have actually owned an Efika SBC for a couple of years now. I am more than a little embarrassed  to admit that other than get it up and

    running with Linux and testing the I/O available (I have a video card in the PCI slot) that I have done little else with it. I'm afraid that I have just spread myself

    way too thin with way too many projects and too many interesting SBCs. I do at least think about getting back to it often but have not done so yet.

     

    One final note, there used to be a nice metal case for the Efika SBC at Directron, I don't know if they are still available.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • gdstew
    0 gdstew over 6 years ago in reply to ullbeking

    Hi Andrew,

     

    In case you are not aware of it this web site https://www.phoronix.com/scan.php?page=home  has been covering the Talos workstations for over a year now.

    There are quite a few articles about both versions that may have useful information about the problems you are having. The owner and pretty much only

    contributor of the web site articles has run a series of in depth benchmarks on the server version which indicates a fully working system. I do remember him

    having some teething problems too but I do not remember any of the specifics.

     

    What a coincidence, I have actually owned an Efika SBC for a couple of years now. I am more than a little embarrassed  to admit that other than get it up and

    running with Linux and testing the I/O available (I have a video card in the PCI slot) that I have done little else with it. I'm afraid that I have just spread myself

    way too thin with way too many projects and too many interesting SBCs. I do at least think about getting back to it often but have not done so yet.

     

    One final note, there used to be a nice metal case for the Efika SBC at Directron, I don't know if they are still available.