Single-Board Computers
  • Products & Partners
  • Dev Tools
  • Single-Board Computers
  • More
  • Cancel
Single-Board Computers
Forum NEON/VFPV3 for the OOB Debian image
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Single-Board Computers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 3 replies
  • Answers 1 answer
  • Subscribers 59 subscribers
  • Views 903 views
  • Users 0 members are here
  • maaxboard
  • oob_debian
Related

NEON/VFPV3 for the OOB Debian image

filippin
filippin over 6 years ago

Hi,

I wanted to compile opencv 4.2.0 from source code but when I did the config I noticed that the Debian image does not expose NEON/VFPV3 instructions.

I did check with "lscpu" and what I see is:

 

==============================================

(cv) root@maaxboard:~/opencv_installs/opencv/build# lscpu
  Architecture:        aarch64
  Byte Order:          Little Endian
  CPU(s):              4
  On-line CPU(s) list: 0-3
  Thread(s) per core:  1
  Core(s) per socket:  4
  Socket(s):           1
  NUMA node(s):        1
  Vendor ID:           ARM
  Model:               4
  Model name:          Cortex-A53
  Stepping:            r0p4
  CPU max MHz:         1300.0000
  CPU min MHz:         800.0000
  BogoMIPS:            16.66
  L1d cache:           unknown size
  L1i cache:           unknown size
  L2 cache:            unknown size
  NUMA node0 CPU(s):   0-3
  Flags:               fp asimd evtstrm aes pmull sha1 sha2 crc32 cpuid

==============================================

 

 

is this correct? the maaxboard ARM A-53 does support neon, right?

 

is this an issue of the debian build only ?

 

 

thanks

  • Sign in to reply
  • Cancel

Top Replies

  • jafoste4
    jafoste4 over 6 years ago +1 suggested
    Hi, Apologies for the delay, yes it supports NEON. I am talking to the SW team in charge of the Debian release and seeing about adding it to the next quarterly release. If you find its missing any additional…
Parents
  • filippin
    0 filippin over 6 years ago

    Thanks Anton, I agree with you, I think it is because it is mandatory. I also think that OpenCV logic is a little buggy for neon detect.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • filippin
    0 filippin over 6 years ago

    Thanks Anton, I agree with you, I think it is because it is mandatory. I also think that OpenCV logic is a little buggy for neon detect.