Single-Board Computers
  • Products & Partners
  • Dev Tools
  • Single-Board Computers
  • More
  • Cancel
Single-Board Computers
Forum Using the GPIOs.
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Single-Board Computers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 1 reply
  • Subscribers 57 subscribers
  • Views 969 views
  • Users 0 members are here
  • gpio
  • maaxboard
Related

Using the GPIOs.

labi
labi over 6 years ago

Hello All,

 

I use the official Debian image (Image V1.1.1.r10)

 

Is there any PIN based GPIO access library what is written in C/C++? Or how can I write/read to/from GPIO?

 

ty

Labi

  • Sign in to reply
  • Cancel
Parents
  • jafoste4
    0 jafoste4 over 6 years ago

    Hi Labi,

     

     

    I take it you are looking to access the GPIOs using somthing similar to Wiring Pi, but for the MaaXBoard?

    https://www.ics.com/blog/how-control-gpio-hardware-c-or-c

     

    Unfortunatly I am unaware of any similar access library available for i.mx 8m. I'd reccomend taking the sysfs approach for GPIO control.

     

    To find the GPIO address for each GPIO you must do the following

     

    The GPIO pins number is from 1 to calculate for the CPU,and it is from 0 to mapped for the sysfs in Linux.

      The address of GPIOx_IOy  in sysfs is (x-1) * 32 + y,  so the address of these gpio are as follows:

    Pin Number Address
    GPIO1_IO03           3
    GPIO1_IO15           15
    GPIO3_IO11           75
    GPIO3_IO15           79

     

    Does this make sense?

     

    -Josh

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Reply
  • jafoste4
    0 jafoste4 over 6 years ago

    Hi Labi,

     

     

    I take it you are looking to access the GPIOs using somthing similar to Wiring Pi, but for the MaaXBoard?

    https://www.ics.com/blog/how-control-gpio-hardware-c-or-c

     

    Unfortunatly I am unaware of any similar access library available for i.mx 8m. I'd reccomend taking the sysfs approach for GPIO control.

     

    To find the GPIO address for each GPIO you must do the following

     

    The GPIO pins number is from 1 to calculate for the CPU,and it is from 0 to mapped for the sysfs in Linux.

      The address of GPIOx_IOy  in sysfs is (x-1) * 32 + y,  so the address of these gpio are as follows:

    Pin Number Address
    GPIO1_IO03           3
    GPIO1_IO15           15
    GPIO3_IO11           75
    GPIO3_IO15           79

     

    Does this make sense?

     

    -Josh

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer