Single-Board Computers
  • Products & Partners
  • Dev Tools
  • Single-Board Computers
  • More
  • Cancel
Single-Board Computers
Forum Maaxboard overheating/ sensitive to ESD?
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Single-Board Computers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 2 replies
  • Subscribers 58 subscribers
  • Views 783 views
  • Users 0 members are here
  • maaxboard
  • esd
Related

Maaxboard overheating/ sensitive to ESD?

pphilippos
pphilippos over 6 years ago

Hello, I have received the board for Roadtest and it is a nice little computer, However, has anyone noticed it being sensitive to Electrostatic discharge? I once touched it while running and the USB ports cut the power off and the display showed a strange pattern on the screen. It could be a coincidence, as there are other concerns as well, such as overheating. It idles at 70 C. Do I have to make any adjustments to the heatsink first? (peel any thermal pad film?)  

 

UPDATE: I took new measurements and it idles at 57-60 C, so something must have been running in the background before. The ESD issue hasn't happened again. It must be rare. Still, having a small fan is recommended (or Joshua Foster's workaround etc.), just like with other new well-performing SBCs such as RPi4 . 

 

image

 

Message was edited by: Philippos Papaphilippou

  • Sign in to reply
  • Cancel
  • jafoste4
    0 jafoste4 over 6 years ago

    Hi,

     

    I haven't experienced ESD issues thus far. Is it replicable?

     

    In regards to the thermal concerns, yes the board gets quite hot when in use. In particular I personally notice a quite a bit of heat when running an HDMI display. I'd reccomend if possible to add some rubber standoffs to the bottom of your board to provide some air gap under neath the board. This seems to help quite a bit. In regards to a thermal pad film. I don't recall. Was the heatsink pre installed when you received your MaaXBoard? If you installed it yourself i'd probably verify there isn't a film you missed. If it was installed by factory it should be good.


    Thx,

    Josh

     

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • pphilippos
    0 pphilippos over 6 years ago in reply to jafoste4

    Thanks,

     

    > I haven't experienced ESD issues thus far. Is it replicable?

     

    I hasn't happened since. I am not sure if it is replicable (e.g. if I started zapping it on purpose).

     

    However, without the fan, it crashed twice unde ordinary workload (trying to install 0.5GB worth of new software through apt-get). (crash confirmed by the hearbeat led stop flashing).

    I will monitor the temperature ranges better and see. The crashes could relate to the sd card (also being close to the heat source)

     

    > Was the heatsink pre installed when you received your MaaXBoard?

     

    Yes, I now removed the screws and it remains firmly attatched, so it must be correctly installed.