Single-Board Computers
  • Products & Partners
  • Dev Tools
  • Single-Board Computers
  • More
  • Cancel
Single-Board Computers
Forum MaaxBoard HDMI not working
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Single-Board Computers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 6 replies
  • Answers 1 answer
  • Subscribers 58 subscribers
  • Views 2275 views
  • Users 0 members are here
  • imx8
  • hdmi
Related

MaaxBoard HDMI not working

jxa0
jxa0 over 5 years ago

Hello,

I just received my MaaxBoard and flashed the SD card with multiple different oob images I found on your sites and none have worked long enough for me to modify my display or network settings

Is there a specific image that i should be using?

 

Issues:

  1. the display initially works; however, as soon as I attempt to open a terminal or set up a network connection the screen blanks
  2. The LG nvidia/G-sync display states that the resolution is 3840x2160, yet recommends 1920x1080



Images I've tried a few, including the two below and

  1. MaaXBoard-LinuxShipmentImage-Debian-V1.1.1r10.img
  2. MaaXBoard-LinuxShipmentImage-Yocto-V1.0.6r07

Thank you,
John

  • Sign in to reply
  • Cancel

Top Replies

  • jxa0
    jxa0 over 5 years ago in reply to jafoste4 +1
    Thank you Joshua, I was able to borrow a 1080 monitor and everything is functional. I was able to configure a static IP so I can ssh into it for future modifications. Please ask the SW engineering team…
  • jxa0
    jxa0 over 5 years ago in reply to jafoste4 +1
    Thank you Joshua, This is the same answer I found from another of your replies here: https://www.element14.com/community/message/290407/l/re-how-to-change-hdmi-output-resolution#290407 I am able to rectify…
Parents
  • jafoste4
    0 jafoste4 over 5 years ago

    Hi John,

     

    What are you using for a power supply? We reccomend a 5V 3A supply such as this https://www.avnet.com/shop/us/products/avnet-engineering-services/aes-acc-maax-pwrul-3074457345642357173/

     

    It appears it is initially working, then perhaps when you try to interact with it, you are experiencing an Over Current moment for your current supply?

     

    Can you also try to manually set the resolution to 1920x1080 to see if that helps? Also are you getting any error messages? Also do you have an additional HDMI display you could try the MaaXBoard with?

     

     

    Thx,

    Josh

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • jxa0
    0 jxa0 over 5 years ago in reply to jafoste4

    I have tried both a 5.1V 3.5A & a 5V 3.0A supplies.

    The same thing happens with both supplies.




    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • jxa0
    0 jxa0 over 5 years ago in reply to jafoste4

    I have tried both a 5.1V 3.5A & a 5V 3.0A supplies.

    The same thing happens with both supplies.




    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • jafoste4
    0 jafoste4 over 5 years ago in reply to jxa0

    Hi John,

     

    The supply you are using should be ok.

     

    Are you able to try a different display? There may be a compatibility issue. Do you have a 3.3V UART TTL debugger you can use to monitor the console output during failure? If so please connect it to the UART on the 40pin gpio header and use a terminal application to see what is happening.

     

    I'll reach out to the SW engineering team responsible for this board and get reccomendations. Should have an answer for you come tomorrow.

     

    -Josh

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jxa0
    0 jxa0 over 5 years ago in reply to jafoste4

    Thank you Joshua,

    I was able to borrow a 1080 monitor and everything is functional.
    I was able to configure a static IP so I can ssh into it for future modifications.

     

     

    Please ask the SW engineering team the following:
    What file can I modify to force the resolution to 1080 or lower on startup? This allows me to use my monitor instead of the borrowed one.

     

     

    This build info via uname -a may help them:
         Linux maaxboard 4.14.78 #1 SMP PREEMPT Tue Jan 14 02:48:31 UTC 2020 aarch64 GNU/Linux

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jafoste4
    0 jafoste4 over 5 years ago in reply to jxa0

    Hi John,

     

    Here is what I received back from my SW support team.

     

     

    Customers could modify the Weston config file to change the resolution.

     

    ```bash

    nano /etc/xdg/weston/weston.ini

    ```

     

    ```ini

    #[output]

    #name=HDMI-A-1

    #mode=1920x1080@60

    #transform=90

    ```

     

    Then, restart the Weston service

     

    ```bash

    systemctl restart weston@root

    ```

     

     

    Thx,

    Josh

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • jxa0
    0 jxa0 over 5 years ago in reply to jafoste4

    Thank you Joshua,

    This is the same answer I found from another of your replies here: https://www.element14.com/community/message/290407/l/re-how-to-change-hdmi-output-resolution#290407

     

    I am able to rectify it when I ssh and manually modify the file and restart the system.