Single-Board Computers
  • Products
  • Dev Tools
  • Single-Board Computers
  • More
  • Cancel
Single-Board Computers
Forum Need a 4 channel multiplexer with a loooot of inputs...
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Single-Board Computers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 6 replies
  • Subscribers 56 subscribers
  • Views 734 views
  • Users 0 members are here
Related

Need a 4 channel multiplexer with a loooot of inputs...

Former Member
Former Member over 12 years ago

I'm designing a cape for a BeagleBone and I'd like them to be stackable. For this reason, I need to be able to put a cape into a particular "mode" such that the I/O goes to a different set of pins on the beaglebone for each cape. I plan to do this with a 4 channel multiplexer (I plan to stack up to three shields), but I have a total of 10 signals (possibly more later) that need to be switched concurrently. So far I've found a dual 4 channel multiplexer, but I need something that can handle 10 signals at once, not just two. Anyone know if such a chip exists?

  • Sign in to reply
  • Cancel
Parents
  • element14jamie
    0 element14jamie over 12 years ago

    Hello Riley,

    Apologize for the delay, I am moving this to the Single Board Computers area of the Community,

     

     

     

    Thank you,

     

    Jamie

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 12 years ago in reply to element14jamie

    Hi Riley,

     

    Assuming I've interpreted it correctly (I may have misread), I'm not sure this would be feasible, because if you want 10 pins per cape to go to different pins on the BBB, then that is 40 pins you're consuming on the BBB for four stacked capes. That is a lot of pins to configure, and your design will be very complex since you'll need an IC (or multiple) on each cape connected to 40 pins on the headers so you can perform the switching operation. Better to maybe address each cape on the same 10 pins (much like a computer data bus and a few address lines) assuming your circuitry can go tri-state.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • shabaz
    0 shabaz over 12 years ago in reply to element14jamie

    Hi Riley,

     

    Assuming I've interpreted it correctly (I may have misread), I'm not sure this would be feasible, because if you want 10 pins per cape to go to different pins on the BBB, then that is 40 pins you're consuming on the BBB for four stacked capes. That is a lot of pins to configure, and your design will be very complex since you'll need an IC (or multiple) on each cape connected to 40 pins on the headers so you can perform the switching operation. Better to maybe address each cape on the same 10 pins (much like a computer data bus and a few address lines) assuming your circuitry can go tri-state.