Single-Board Computers
  • Products
  • Dev Tools
  • Single-Board Computers
  • More
  • Cancel
Single-Board Computers
Forum What boards should element14 carry besides the Raspberry Pi?
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Single-Board Computers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 21 replies
  • Subscribers 59 subscribers
  • Views 2569 views
  • Users 0 members are here
  • industrial
  • sbc
  • sabre
  • sabrelite
  • saber
  • embedded
  • raspberry_pi
  • cabeatwell
  • development
  • prototyping
  • innovation
  • sabre_lite
  • communication
Related

What boards should element14 carry besides the Raspberry Pi?

Catwell
Catwell over 13 years ago

Take a look at the blogs... and report back here.

 

I would like to see the ODROID and UDOO board here.

 

C

  • Sign in to reply
  • Cancel

Top Replies

  • e14 Contributor
    e14 Contributor over 13 years ago +1
    I like the Odroid-U2 for it's faster cpu and 2Gb ram, but not for the interesting looking heatsink 'case' and usb ethernet. The UDOO with it's iMX6 SoC is interesting, but I'd like more gpio via the iMX6…
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to morgaine +1
    Morgaine Dinova wrote: It's worth noting that in the time this thread was inactive, the Wandboard Quad was added to the family and features not only a populated SATA connector but also 2 gigs of RAM. And…
  • morgaine
    morgaine over 13 years ago in reply to e14 Contributor +1
    selsinork wrote: With 2GB ram, a couple of these just got added to my list.. just a pity we can't get them from e14 ! I certainly agree with that, and I'll add a couple here! E14, you have at least 4 guaranteed…
Parents
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    I like the Odroid-U2 for it's faster cpu and 2Gb ram, but not for the interesting looking heatsink 'case' and usb ethernet.

     

    The UDOO with it's iMX6 SoC is interesting, but I'd like more gpio via the iMX6 rather than the double indirection via the onboard arduino. I see they have a goal to do this if they get funded to $500K.  I struggle with the hybrid approach - a standalone arduino due is going to be cheaper and I can use it with an existing pc.

     

    I'd like to see the CubieBoard as it's reasonably cheap while offering some different options from R-Pi & BeagleBone.

     

    While I can understand that e14 wouldn't want to carry every available board, we already see Olimex, R-Pi, Beagleboard, Sabre-Lite etc. and it's noticeable that the various Alwinner or exynos boards appearing out of china are under represented in e14's lineup.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    I like the Odroid-U2 for it's faster cpu and 2Gb ram, but not for the interesting looking heatsink 'case' and usb ethernet.

     

    The UDOO with it's iMX6 SoC is interesting, but I'd like more gpio via the iMX6 rather than the double indirection via the onboard arduino. I see they have a goal to do this if they get funded to $500K.  I struggle with the hybrid approach - a standalone arduino due is going to be cheaper and I can use it with an existing pc.

     

    I'd like to see the CubieBoard as it's reasonably cheap while offering some different options from R-Pi & BeagleBone.

     

    While I can understand that e14 wouldn't want to carry every available board, we already see Olimex, R-Pi, Beagleboard, Sabre-Lite etc. and it's noticeable that the various Alwinner or exynos boards appearing out of china are under represented in e14's lineup.