Single-Board Computers
  • Products
  • Dev Tools
  • Single-Board Computers
  • More
  • Cancel
Single-Board Computers
Forum What boards should element14 carry besides the Raspberry Pi?
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Single-Board Computers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 21 replies
  • Subscribers 59 subscribers
  • Views 2592 views
  • Users 0 members are here
  • industrial
  • sbc
  • sabre
  • sabrelite
  • saber
  • embedded
  • raspberry_pi
  • cabeatwell
  • development
  • prototyping
  • innovation
  • sabre_lite
  • communication
Related

What boards should element14 carry besides the Raspberry Pi?

Catwell
Catwell over 13 years ago

Take a look at the blogs... and report back here.

 

I would like to see the ODROID and UDOO board here.

 

C

  • Sign in to reply
  • Cancel

Top Replies

  • e14 Contributor
    e14 Contributor over 13 years ago +1
    I like the Odroid-U2 for it's faster cpu and 2Gb ram, but not for the interesting looking heatsink 'case' and usb ethernet. The UDOO with it's iMX6 SoC is interesting, but I'd like more gpio via the iMX6…
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to morgaine +1
    Morgaine Dinova wrote: It's worth noting that in the time this thread was inactive, the Wandboard Quad was added to the family and features not only a populated SATA connector but also 2 gigs of RAM. And…
  • morgaine
    morgaine over 13 years ago in reply to e14 Contributor +1
    selsinork wrote: With 2GB ram, a couple of these just got added to my list.. just a pity we can't get them from e14 ! I certainly agree with that, and I'll add a couple here! E14, you have at least 4 guaranteed…
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    I like the Odroid-U2 for it's faster cpu and 2Gb ram, but not for the interesting looking heatsink 'case' and usb ethernet.

     

    The UDOO with it's iMX6 SoC is interesting, but I'd like more gpio via the iMX6 rather than the double indirection via the onboard arduino. I see they have a goal to do this if they get funded to $500K.  I struggle with the hybrid approach - a standalone arduino due is going to be cheaper and I can use it with an existing pc.

     

    I'd like to see the CubieBoard as it's reasonably cheap while offering some different options from R-Pi & BeagleBone.

     

    While I can understand that e14 wouldn't want to carry every available board, we already see Olimex, R-Pi, Beagleboard, Sabre-Lite etc. and it's noticeable that the various Alwinner or exynos boards appearing out of china are under represented in e14's lineup.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    what about the Wandboard http://wandboard.org/  ?

     

    or 2Gb Nitrogen 6x http://boundarydevices.com/products/nitrogen6x-board-imx6-arm-cortex-a9-sbc/ ?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • colecago
    0 colecago over 13 years ago in reply to e14 Contributor

    pcDduino

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    Maybe we can come up with a list of which board characteristics we would

    like to see.  For example:

     

    a.  SATA is a plus

    b.  ARMv6 is a minus

    c.  1080p decode is a plus

    d.  trouble-free, mainlined USB driver is a plus

    e.  1.8v UHS SD card support is a plus

    f.  HDMI that can power HDMI to VGA converters is a plus

    g.  ethernet over USB is a minus

    h.  closed source bootloader is a minus

    i.   lack of hot-plug USB thumb drive support is a minus

    j.   plastic SD-card holder is minus

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to e14 Contributor

    coder27 wrote:

     

    e.  1.8v UHS SD card support is a plus

    I've yet to see a board that supports that. Schematics for all the ones I've got so far show the SD card hard wired to 3.3v.

     

    I'll add,

     

    k. full sized SD, especially where the card hangs over the edge of the board is a minus

    l. accelerated X11 drivers are a plus

    m. reasonable number of gpio is a plus

     

    and I'd maybe modify b, to be ARMv6 or earlier

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to colecago

    colecago wrote:

     

    pcDduino

    That looks quite nice... another example of the under represented Allwinner A10.  But I wonder why, like Olimex, they don't bring out the sata port.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to e14 Contributor

    n.  boot from USB/ethernet/SATA is a plus

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to e14 Contributor

    o. battery backed RTC

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to e14 Contributor

    > l. accelerated X11 drivers are a plus

     

    Accelerated X11 drivers are in the land of broken promises.

     

    Liz wrote on Feb 17, 2012:

    "We're going to be offering a bounty for the best accelerated X implementation from the community - more news about that after launch."

    http://www.raspberrypi.org/phpBB3/viewtopic.php?f=2&t=3145&start=20

     

    Liz wrote on Oct 15, 2012::

    "Accelerated X will be a solved problem soon; we've put engineering resource on it, and it's actively being worked on."

    http://www.raspberrypi.org/phpBB3/viewtopic.php?p=194400#p194400

     

    but Simon (working on his own) has apparently given up, writing on May 7, 2013:

    "Nay, I didn't have much time to work on it at the beginning of the year. When I did restart there were some weird bug reports which I could never repro, then I realised that it's just not worth the effort...the demand for an accelerated X is much lower than you might imagine."

    http://www.raspberrypi.org/phpBB3/viewtopic.php?f=63&t=4649&start=396

     

    Earlier he described the problem as essentially fundamentally unsolveable

    due to X applications doing too many single-pixel operations that are

    impossible to accelerate due to the overhead involved in gpu communication.

     

    There is perhaps hope for X applications such as web browsers to

    switch to a different toolkit that can be accelerated, as is done with

    most cell-phone browsers.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to e14 Contributor

    coder27 wrote:

     

    Earlier he described the problem as essentially fundamentally unsolveable

    due to X applications doing too many single-pixel operations that are

    impossible to accelerate due to the overhead involved in gpu communication.

    That's mostly an implementation detail of the Pi's unusual architecture. Other GPU's manage it fine in x86 land even if it is with closed drivers.

    I agree that gpu stuff is currently off in the clouds playing with the flying pigs.. Still, if someone pulls a rabbit out of the hat, or if the lima project gets useful then a group of sbc's using whichever gpu will become much more attractive.  Which puts pressure on competing vendors to do the same.

     

    No, I'm not holding my breath waiting image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
>