Single-Board Computers
  • Products
  • Dev Tools
  • Single-Board Computers
  • More
  • Cancel
Single-Board Computers
Forum Very new to the bbb and have one question
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Single-Board Computers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 4 replies
  • Subscribers 57 subscribers
  • Views 764 views
  • Users 0 members are here
  • beaglebone_black
  • single-board-computers
Related

Very new to the bbb and have one question

e14 Contributor
e14 Contributor over 12 years ago

Can the header rows be used as inputs Im looking to build something that requires 27 inputs....

  • Sign in to reply
  • Cancel

Top Replies

  • e14 Contributor
    e14 Contributor over 12 years ago in reply to e14 Contributor +1
    ty the answer was right on that up to 65 of them can be used as i/o now I'll just have to find me a programmer to make a simple program to read those for when something is present then be able to send…
Parents
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    dosnt matter if digital or analog just as long as i can see if something is present on the inputs.....image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to e14 Contributor

    I think you are in luck.  Here's the header details:

    http://circuitco.com/support/index.php?title=Cape_Expansion_Headers

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to e14 Contributor

    ty the answer was right on that up to 65 of them can be used as i/o now I'll just have to find me a programmer to make a simple program to read those for when something is present then be able to send that wirless to another program on a laptop. basiclly I'm makeing a peice of test equipment to test a large receptical for when voltage or data is present while about 35 feet away at the controls of the equipment. Long term goal is to make it and be able to read data with laptop, tab, or phone image So again ty for that answer.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to e14 Contributor

    ty the answer was right on that up to 65 of them can be used as i/o now I'll just have to find me a programmer to make a simple program to read those for when something is present then be able to send that wirless to another program on a laptop. basiclly I'm makeing a peice of test equipment to test a large receptical for when voltage or data is present while about 35 feet away at the controls of the equipment. Long term goal is to make it and be able to read data with laptop, tab, or phone image So again ty for that answer.