Single-Board Computers
  • Products
  • Dev Tools
  • Single-Board Computers
  • More
  • Cancel
Single-Board Computers
Forum control of 360 degree servos
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Single-Board Computers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 12 replies
  • Subscribers 57 subscribers
  • Views 2869 views
  • Users 0 members are here
  • beaglebone_black
  • single-board-computers
Related

control of 360 degree servos

e14 Contributor
e14 Contributor over 12 years ago

Hi

 

i wonder how i would control a 360 degree servos from a python script?

 

there are lot of guides on 180 degree servos

 

most of them from adafruit... have nothing against them but i like to not be dependent on external libs

 

 

i'm going to use this in a fully automatic tracker.... the tracker will be used to track high altitude baloons (30+ km)

 

 

/bo

  • Sign in to reply
  • Cancel
Parents
  • shabaz
    0 shabaz over 12 years ago

    Hi Bo,

     

    A  servo capable of 360 degrees would be different from those "modified RC servos" that give continuous rotation. Are you planning on using this for a gymbal type mechanism to track?

    If so, perhaps PWM is not the best way to do this, especially if you're going to the mechanical effort at producing a gymbal.

    A better choice would be to use geared-down stepper motors for much higher resolution.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to shabaz

    nope... it will be a simple up/down with one servo and left/right with another.... one limit will be that it can not go from 360/0 to 1... it will be told to go the other way round to not mess up wires

     

    up/down will be limited to 90 degree up and no down...

     

    and i will better stay on servos... cheaper... just need the big hobby servos... then a few bearings to take load off servos

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 12 years ago in reply to e14 Contributor

    Have you got a URL/datasheet to a 360 degree servo that you're planning to use? Modifying a 180 degree servo for continuous rotation is not the same thing as a servo capable of a controlled 360 degrees.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • shabaz
    0 shabaz over 12 years ago in reply to e14 Contributor

    Have you got a URL/datasheet to a 360 degree servo that you're planning to use? Modifying a 180 degree servo for continuous rotation is not the same thing as a servo capable of a controlled 360 degrees.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to shabaz

    http://www.hobbyking.com/hobbyking/store/__18742__Vigor_VSD_11AYMB_MG_HV_Extra_Large_360_Degree_Winch_Servo_0_75sec_50kg_150g.html