Single-Board Computers
  • Products
  • Dev Tools
  • Single-Board Computers
  • More
  • Cancel
Single-Board Computers
Forum A Single Board Computer as a home network server?
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Single-Board Computers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 57 subscribers
  • Views 2258 views
  • Users 0 members are here
Related

A Single Board Computer as a home network server?

spoonsphere
spoonsphere over 12 years ago

Greetings!

 

We have a few computers in our home (the number being used simultaneous varies, but generally does not exceed 6).

 

I would like to set up a single board computer running some linux distribution (I'm most familiar with RHEL/CentOS, but am not opposed to running Ubuntu, etc.) to provide the following services.

* DHCP (isc-dhcp-server)

* DNS (bind)

* Proxy (squid)

* File Sharing (samba)

* Database (mysql)

* Web (apache / php)

* FTP (vsftpd)

* TFTP (tftpd)

* Version Control (subversion)

* Remote syslog (syslog)

 

Most of this will be pretty light weight.  The file sharing and proxy server may be a little i/o and network intensive at times.

 

I don't think the Raspberry Pi will be powerful enough.  I wonder whether the Beaglebone Black running Ubuntu with USB attached storage might be able to handle these requirements.  Or perhaps the InForce IFC6410?

 

Another option is an Intel NUC solution running a Core i3 processor.  Cost aside, this will prove more powerful than the aforementioned solution.  It will also be more turnkey - I know I can slap CentOS on there and it will just work, whereas the Beaglebone Black and the IFC6410 will require more work to get set up.  One concern about the NUC is that it has more parts, which provides more opportunity for something to go wrong.

 

For the file server, I know another option is to implement a solution from QNAP or Synology.  I wouldn't want to do a NUC and one of these file servers - I can't have cost move that far aside.

 

Any suggestions or thoughts you have on this would be kindly appreciated.

 

Please let me know if you have any questions.

 

Thanks!

-s

  • Sign in to reply
  • Cancel
Parents
  • morgaine
    0 morgaine over 12 years ago

    Hi spoon, welcome to the party. image

     

    From the sound of it, you have the issues and tradeoffs well in hand already, so we may not be able to add much.  I can't quite make out the level of performance you're looking for, as you seem to be giving consideration to everything from BeagleBone Black to a Core i3 board --- that's a very large range of performance!  What's more, the range of prices you've mentioned is also very large, to make the choice even more complicated.

     

    What I can recommend stems from the fact that you've identified that "The file sharing and proxy server may be a little i/o and network intensive at times."  That's going to be your main constraining requirement then, because ARM boards are a bit lackluster on I/O.  (PCIe in particular is as rare as hens' teeth on ARM.)  We've done a lot of measurements on "SBC Network Throughput" (the title of our corresponding thread), so you might want to glance at that first.  As that table will show you, not all ARM boards will fully use even a 100Mbps link, so some can be eliminated immediately through poor networking.

     

    Boards with gigabit Ethernet are likely to be important for your purpose, and so is fast storage it seems since you have quite a few applications listed that will require it.  That probably means you need to focus on boards that provide SATA, which eliminates another large raft of boards.  The combination of gigabit Ethernet and SATA is still a bit rare, with only Sabre-Light and Wandboard offering it among previously easily available ARM boards I think (not sure about Gumstix Pepper, but it does at least have gigabit).  You can now also add the InForce IFC6410 that you mentioned to the mix as well -- I hadn't heard of that one, but it seems well spec'd, if a little costly.  If you also add x86 then your options expand dramatically, for example with the Minnowboard, but at considerable cost.  The options are numerous.

     

    I suspect that the best power/performance is likely to come from mini-ITX or downmarket Core i3 boards, but we haven't really been focusing on them here.

     

    We're currently enthusing about the forthcoming A10-OLinuXino-LIME boards from Olimex which hopefully will be available by Xmas,  Although they don't have gigabit Ethernet, they do have SATA, so if I overestimated how much networking throughput you'll be needing, you might want to wait for those to appear --- at just 30 Euros, they'll be selling like hotcakes, and you could afford more than one which will give you more effective network throughput.

     

    You have an awful lot of options! image

     

    Morgaine.

     

     

    PS. Depending where you are located in the world, the Cubietruck [aka. Cubieboard3] might be an option for you as well, providing gigabit Ethernet, SATA, and dual core Cortex-A7 for less money than the InForce, and it's just become available according to the Cubie website.  The ARM price leader for that kind of spec though seem to be the various models of Wandboard.  Once it's out, Olimex's A20-SOM and its EVB baseboard is expected to provide very good competition --- the great combination of gigabit, SATA and Cortext-A7 again.

     

    PPS. We have measurements of "SBC CPU Throughput" as well, in case that might be relevant to you.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • morgaine
    0 morgaine over 12 years ago

    Hi spoon, welcome to the party. image

     

    From the sound of it, you have the issues and tradeoffs well in hand already, so we may not be able to add much.  I can't quite make out the level of performance you're looking for, as you seem to be giving consideration to everything from BeagleBone Black to a Core i3 board --- that's a very large range of performance!  What's more, the range of prices you've mentioned is also very large, to make the choice even more complicated.

     

    What I can recommend stems from the fact that you've identified that "The file sharing and proxy server may be a little i/o and network intensive at times."  That's going to be your main constraining requirement then, because ARM boards are a bit lackluster on I/O.  (PCIe in particular is as rare as hens' teeth on ARM.)  We've done a lot of measurements on "SBC Network Throughput" (the title of our corresponding thread), so you might want to glance at that first.  As that table will show you, not all ARM boards will fully use even a 100Mbps link, so some can be eliminated immediately through poor networking.

     

    Boards with gigabit Ethernet are likely to be important for your purpose, and so is fast storage it seems since you have quite a few applications listed that will require it.  That probably means you need to focus on boards that provide SATA, which eliminates another large raft of boards.  The combination of gigabit Ethernet and SATA is still a bit rare, with only Sabre-Light and Wandboard offering it among previously easily available ARM boards I think (not sure about Gumstix Pepper, but it does at least have gigabit).  You can now also add the InForce IFC6410 that you mentioned to the mix as well -- I hadn't heard of that one, but it seems well spec'd, if a little costly.  If you also add x86 then your options expand dramatically, for example with the Minnowboard, but at considerable cost.  The options are numerous.

     

    I suspect that the best power/performance is likely to come from mini-ITX or downmarket Core i3 boards, but we haven't really been focusing on them here.

     

    We're currently enthusing about the forthcoming A10-OLinuXino-LIME boards from Olimex which hopefully will be available by Xmas,  Although they don't have gigabit Ethernet, they do have SATA, so if I overestimated how much networking throughput you'll be needing, you might want to wait for those to appear --- at just 30 Euros, they'll be selling like hotcakes, and you could afford more than one which will give you more effective network throughput.

     

    You have an awful lot of options! image

     

    Morgaine.

     

     

    PS. Depending where you are located in the world, the Cubietruck [aka. Cubieboard3] might be an option for you as well, providing gigabit Ethernet, SATA, and dual core Cortex-A7 for less money than the InForce, and it's just become available according to the Cubie website.  The ARM price leader for that kind of spec though seem to be the various models of Wandboard.  Once it's out, Olimex's A20-SOM and its EVB baseboard is expected to provide very good competition --- the great combination of gigabit, SATA and Cortext-A7 again.

     

    PPS. We have measurements of "SBC CPU Throughput" as well, in case that might be relevant to you.