Single-Board Computers
  • Products
  • Dev Tools
  • Single-Board Computers
  • More
  • Cancel
Single-Board Computers
Forum Differential Temperature Controller
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Single-Board Computers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 22 replies
  • Subscribers 59 subscribers
  • Views 3172 views
  • Users 0 members are here
  • temperature
  • house
Related

Differential Temperature Controller

e14 Contributor
e14 Contributor over 12 years ago

What is the best way@ to control a whole house fan to run when the temperature outside is less than the temperature inside?

  • Sign in to reply
  • Cancel

Top Replies

  • e14 Contributor
    e14 Contributor over 12 years ago +1
    Folks, does this really have anything to do with Single-Board Computers ? If not, then perhaps move it to a more appropriate area ? element14jamie might be able to help with that if necessary
Parents
  • D_Hersey
    0 D_Hersey over 12 years ago

    I forgot to add that the SS Relay box should be labeled with something like "Warning  -- Turns on Randomly."  If you build this box and can demonstrate that it can turn on, and more uncertainly, turn off the fans, we can control them with either an analog or digital device.  But, if all you want is the simple operation you delineate, say, turn the fans when the outside ambient is 5C or so cooler than the house, back off when the differential falls, say to 2C, simple, cheap and highly reliable op-amps will work.  If you decide you want to data-log later, we can monitor the op amps with a Von-Neumann type computer board, or supplant them completely with one.

     

    There is something elegant about avoiding such a computer in this application.  In 50's Sci-Fi they may have refereed to this overall circuit as an example of a homeostat.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • D_Hersey
    0 D_Hersey over 12 years ago

    I forgot to add that the SS Relay box should be labeled with something like "Warning  -- Turns on Randomly."  If you build this box and can demonstrate that it can turn on, and more uncertainly, turn off the fans, we can control them with either an analog or digital device.  But, if all you want is the simple operation you delineate, say, turn the fans when the outside ambient is 5C or so cooler than the house, back off when the differential falls, say to 2C, simple, cheap and highly reliable op-amps will work.  If you decide you want to data-log later, we can monitor the op amps with a Von-Neumann type computer board, or supplant them completely with one.

     

    There is something elegant about avoiding such a computer in this application.  In 50's Sci-Fi they may have refereed to this overall circuit as an example of a homeostat.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • michaelkellett
    0 michaelkellett over 12 years ago in reply to D_Hersey

    Actually it's kind of hard to justify analogue control systems at all any more. As soon as you need a mixture of logic, thresholds and time delays it's almost always cheaper and more relaible to use a micro. (I'm excluding "junk box" sourcing here). The nice thing about micros is that you can so easily adjust thresholds and have long time constants reliably at low cost. A (32 bit) micro with on chip ADC, timers etc etc will cost less than 50p in decent numbers - you can't get one reliable >5 minute time constant for that in analogue.

    For the experimental one off the micro pays back because it's so easy to connect it to a PC or tablet for monitoring during development - and when you realise that actually you need an extra input or two and some more logic there's no trouble in adding it.

     

    In about 1964 my father installed a central heating system with 100% mechanical "compensator" type controller - measured the outside temperature and adjusted the radiator water temperature accordingly - there was a copper bulb outside with a long flexible copper pipe to the controlelr/valve assembly near the boiler - elegant perhaps, with lot's of lovely machined metal parts, but not the way to do it now.

     

    MK