Single-Board Computers
  • Products
  • Dev Tools
  • Single-Board Computers
  • More
  • Cancel
Single-Board Computers
Forum Sabre Lite Android Boot
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Single-Board Computers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 1 reply
  • Subscribers 56 subscribers
  • Views 334 views
  • Users 0 members are here
Related

Sabre Lite Android Boot

kevinparkes
kevinparkes over 12 years ago

Hi, I would like to boot my Sabre Lite Quad board using an Android image on an SD card. I followed a very simple guide:-http://www.element14.com/community/community/designcenter/single-board-computers/sabrelite/blog/2014/04/01/getting-started-with-sabre-lite-imx6

and I get the following error during bootup:-

 

Board: MX6Q-SABRELITE:[ POR]

Boot Device: I2C

I2C:   ready

DRAM:   1 GB

MMC:   FSL_USDHC: 0,FSL_USDHC: 1

JEDEC ID: 0xbf:0x25:0x41

Reading SPI NOR flash 0xc0000 [0x2000 bytes] -> ram 0x276009b8

SUCCESS

 

*** Warning - bad CRC, using default environment

 

In:    serial

Out:   serial

Err:   serial

Net:   got MAC address from IIM: 00:00:00:00:00:00

FEC0 [PRIME]

Hit any key to stop autoboot:  0

mmc1 is current device

 

MMC read: dev # 1, block # 2048, count 8192 ... 8192 blocks read: OK

Wrong Image Format for bootm command

ERROR: can't get kernel image!

 

I have not tried upgrading U-Boot as the board is new so should contain the most recent version? The current U-Boot version is not displayed during boot, which I thought was strange. What does "Wrong Image Format for bootm command" mean? I've tried many different images, loaded via Linux and Windows. I can see the created partitions on my SD card so the image has been written correctly. I can load the basic Linux slide show demo app.

 

Any ideas?

 

Thanks, Kevin.

  • Sign in to reply
  • Cancel
Parents
  • element14jamie
    0 element14jamie over 12 years ago

    Hello Kevin,

    Welcome to the elemnt14 Community, we hope you enjoy it!

     

    I will move this to the Single-Board Computers area as it is a better fit.

     

    Thank you,

     

    Jamie

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • element14jamie
    0 element14jamie over 12 years ago

    Hello Kevin,

    Welcome to the elemnt14 Community, we hope you enjoy it!

     

    I will move this to the Single-Board Computers area as it is a better fit.

     

    Thank you,

     

    Jamie