Single-Board Computers
  • Products
  • Dev Tools
  • Single-Board Computers
  • More
  • Cancel
Single-Board Computers
Forum RiotBoard problem w SD booting
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Single-Board Computers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 3 replies
  • Subscribers 59 subscribers
  • Views 801 views
  • Users 0 members are here
  • element14
  • riotboard
  • boot
  • sd
Related

RiotBoard problem w SD booting

e14 Contributor
e14 Contributor over 11 years ago

Hi

 

I have a problem with my RiotBoard. I can not boot from SD card inserted into J7 ( microSD slot). Nothing works, even u-boot does not start

When I take the same card and put it into SD adapter and insert it into J6 ( SD card slot) , board starts ( uboot is alive - I can see output from u-boot, kernel etc .)   I checked  DIP settings in both cases and are ok ( "Boot Device: SD ")

 

What is a problem with J7 ? How make it working ?

  • Sign in to reply
  • Cancel
Parents
  • bwelsby
    0 bwelsby over 11 years ago

    Are you using the same switch settings for both?

    The switch settings for booting micro SD are not the same as SD as follows:

     

    Micro SD J7

    D1 D2 D3 D4 D5 D6 D7 D8

    1    0    1    0    0    1    1    0

     

    SD J6

    D1 D2 D3 D4 D5 D6 D7 D8

    1    0    1    0    0    1    0    1

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Reply
  • bwelsby
    0 bwelsby over 11 years ago

    Are you using the same switch settings for both?

    The switch settings for booting micro SD are not the same as SD as follows:

     

    Micro SD J7

    D1 D2 D3 D4 D5 D6 D7 D8

    1    0    1    0    0    1    1    0

     

    SD J6

    D1 D2 D3 D4 D5 D6 D7 D8

    1    0    1    0    0    1    0    1

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to bwelsby

    Thank you