Single-Board Computers
  • Products
  • Dev Tools
  • Single-Board Computers
  • More
  • Cancel
Single-Board Computers
Forum Linux + baremetal
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Single-Board Computers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 11 replies
  • Subscribers 59 subscribers
  • Views 2282 views
  • Users 0 members are here
  • bare-metal
  • sbc
  • dual-core
  • single-board-computers
  • linux
Related

Linux + baremetal

amgalbu
amgalbu over 11 years ago

Hello

I was looking for suggestions about a request a customer made to me

This customer has a system that is made up of two boards: a board with a very simple MCU and an SBC with a dual-core CPU that runs Linux

The first board id actually requested because, in case of system reset, the application starts immediately (MCU has no OS so there is not boot time)

In order to reduce costs, I was asked if it was possible to make the SBC run the application that runs on the MCU

I found this application note but it seems that the bare metal application (running on CPU1) needs to be initialized by Linux, so the boot time is still there

So my question is: is it possible to run a bare metal application before Linux starts?

 

Any advice is welcomed!
Ambrogio

  • Sign in to reply
  • Cancel
Parents
  • clem57
    0 clem57 over 11 years ago

    Do you want to run bare metal instead of Linux? That is possible to do. I assume your Linux is running on ARM of some sort. There is freeRTOS that could run instead of Linux. Another possibility is running Damn Small Linux(DSL) which will come up in a flash. May need to create an ARM binary. Another one is http://archlinuxarm.org/.

     

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • amgalbu
    0 amgalbu over 11 years ago in reply to clem57

    Hi clem

    I want to run a bare metal application on one core and linux on the other cores. And i want the bare metal application to start as soon as the sbc is powered up (i.e. before linux boots)

    I was studying the application note whose link i posted in my original post and trying to understand if i can move the initiinitialization code in uboot

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • clem57
    0 clem57 over 11 years ago in reply to amgalbu

    @amgalbu

    So you want this http://www.wiki.xilinx.com/Multi-OS+Support+%28AMP+%26+Hypervisor%29

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • clem57
    0 clem57 over 11 years ago in reply to clem57

    Or just how to program on bare metal like this https://balau82.wordpress.com/2010/02/14/simplest-bare-metal-program-for-arm/

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • clem57
    0 clem57 over 11 years ago in reply to clem57

    Or just how to program on bare metal like this https://balau82.wordpress.com/2010/02/14/simplest-bare-metal-program-for-arm/

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • amgalbu
    0 amgalbu over 11 years ago in reply to clem57

    No this solution does not include linux