Single-Board Computers
  • Products
  • Dev Tools
  • Single-Board Computers
  • More
  • Cancel
Single-Board Computers
Forum Linux + baremetal
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Single-Board Computers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 11 replies
  • Subscribers 59 subscribers
  • Views 2269 views
  • Users 0 members are here
  • bare-metal
  • sbc
  • dual-core
  • single-board-computers
  • linux
Related

Linux + baremetal

amgalbu
amgalbu over 11 years ago

Hello

I was looking for suggestions about a request a customer made to me

This customer has a system that is made up of two boards: a board with a very simple MCU and an SBC with a dual-core CPU that runs Linux

The first board id actually requested because, in case of system reset, the application starts immediately (MCU has no OS so there is not boot time)

In order to reduce costs, I was asked if it was possible to make the SBC run the application that runs on the MCU

I found this application note but it seems that the bare metal application (running on CPU1) needs to be initialized by Linux, so the boot time is still there

So my question is: is it possible to run a bare metal application before Linux starts?

 

Any advice is welcomed!
Ambrogio

  • Sign in to reply
  • Cancel
  • clem57
    0 clem57 over 11 years ago in reply to amgalbu

    @amgalbu

      I think what you want to do is possible. How much programming in ARM assembler can you handle? The trick is to switch CPU1 with CP0. But then you MUST handle the CPU0 tasks in the bare metal code.Here are some of the trickier pieces:

    Examples of some of the shared resources are:

    • Interrupt control distributor (ICD)

    • DDR memory

      On-chip memory (OCM)

    • Global timer • Snoop control unit (SCU) and L2 cache

    In this example, CPU0 is treated as the master and controls the shared resources. If CPU1 were to require control of a shared resource, it would have to communicate the request to CPU0 and let CPU0 control the resource. To keep the complexity of this reference design to a minimum, the bare-metal application running on CPU1 has been modified to limit access to the shared resources. OCM is used by both processors to communicate to each other. When compared to DDR memory, OCM provides very high performance and low latency access from both processors. Deterministic access is further assured by disabling cache access to the OCM from both processors. Actions taken by this design to prevent problems with the shared resources include: 1. DDR memory: Linux has only been made aware of memory at 0x00000000 to 0x2FFFFFFF. CPU1 uses memory from 0x30000000 to 0x3FFFFFFF for its bare-metal application. 2. L2 Cache: CPU1 does not use L2 cache. 3. ICD: Interrupts from the core in PL are routed to the PPI controller for CPU1. By using the PPI, CPU1 has the freedom to service interrupts without requiring access to the ICD. 4. Timer: CPU1 uses the private timer for the heart beat. 5. OCM: Accesses to OCM are handled very carefully by each CPU to prevent contention. In the case of the heart beat, only CPU1 writes the location and CPU0 reads the location. When data is sent from CPU1 to CPU0, only CPU1 writes the data value, then CPU1 sends a flag by setting a different address location in OCM. CPU0 in turn detects the flag, reads the data, and then clears the flag. Only CPU1 can set the flag, and only CPU0 can clear the flag.

      Basically it boils down to controlling shared resources until Linux can take over... Finally you would kick off linux like this:

     

    CPU0 (running Linux) starts CPU1 (running bare-metal) by writing the value of 0x30000000 to address 0xFFFFFFF0 using the included rwmem application. Normally, CPU0 would need to run a set event (SEV) command to wake up CPU1. Because Linux, running on CPU0, is constantly servicing interrupts (another source of events), an SEV command is not necessary. When CPU1 wakes up, it reads the value 0x30000000 from address 0xFFFFFFF0 (written using the rwmem command) and then jumps to address 0x30000000. Note that the FSBL placed CPU1’s ELF at 0x30000000.

     

    Tricky, but certainly possible,

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
<