Single-Board Computers
  • Products
  • Dev Tools
  • Single-Board Computers
  • More
  • Cancel
Single-Board Computers
Forum Linux + baremetal
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Single-Board Computers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 11 replies
  • Subscribers 59 subscribers
  • Views 2281 views
  • Users 0 members are here
  • bare-metal
  • sbc
  • dual-core
  • single-board-computers
  • linux
Related

Linux + baremetal

amgalbu
amgalbu over 11 years ago

Hello

I was looking for suggestions about a request a customer made to me

This customer has a system that is made up of two boards: a board with a very simple MCU and an SBC with a dual-core CPU that runs Linux

The first board id actually requested because, in case of system reset, the application starts immediately (MCU has no OS so there is not boot time)

In order to reduce costs, I was asked if it was possible to make the SBC run the application that runs on the MCU

I found this application note but it seems that the bare metal application (running on CPU1) needs to be initialized by Linux, so the boot time is still there

So my question is: is it possible to run a bare metal application before Linux starts?

 

Any advice is welcomed!
Ambrogio

  • Sign in to reply
  • Cancel
  • D_Hersey
    0 D_Hersey over 11 years ago

    What bootloader are you using?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • amgalbu
    0 amgalbu over 11 years ago in reply to D_Hersey

    I typical use uboot, but there are no closure in using any other bootloader

     

    thanks!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • clem57
    0 clem57 over 11 years ago

    Do you want to run bare metal instead of Linux? That is possible to do. I assume your Linux is running on ARM of some sort. There is freeRTOS that could run instead of Linux. Another possibility is running Damn Small Linux(DSL) which will come up in a flash. May need to create an ARM binary. Another one is http://archlinuxarm.org/.

     

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • amgalbu
    0 amgalbu over 11 years ago in reply to clem57

    Hi clem

    I want to run a bare metal application on one core and linux on the other cores. And i want the bare metal application to start as soon as the sbc is powered up (i.e. before linux boots)

    I was studying the application note whose link i posted in my original post and trying to understand if i can move the initiinitialization code in uboot

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • clem57
    0 clem57 over 11 years ago in reply to amgalbu

    @amgalbu

    So you want this http://www.wiki.xilinx.com/Multi-OS+Support+%28AMP+%26+Hypervisor%29

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • clem57
    0 clem57 over 11 years ago in reply to clem57

    Or just how to program on bare metal like this https://balau82.wordpress.com/2010/02/14/simplest-bare-metal-program-for-arm/

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • amgalbu
    0 amgalbu over 11 years ago in reply to clem57

    Yes this is the link where i found the application note. The problem is the bare metal applivations starts agter uboot so there is a delay ffrom when the sbc the is powered up to the moment when the bare metal application starts

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • amgalbu
    0 amgalbu over 11 years ago in reply to clem57

    No this solution does not include linux

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • clem57
    0 clem57 over 11 years ago in reply to amgalbu

    No matter how many processors, only one starts in uboot and later the others start when they have been setup for either Linux or bare metal. The delay should be short. If you need logic at immediate start, you may need external digital logic gates for desired output/inputs. One other choice is use PSoC 4 since it has configurable logic on the processor that will be ready at power up. If the hardware already selected, I could conceive of a bare metal approach that "Kick starts" the Linux later on. The Arduino Yun board: Atmel side starts almost instantaneously while the Linux side takes a solid couple of minutes.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • amgalbu
    0 amgalbu over 11 years ago in reply to clem57

    Current solution is based on an external logic, but in order to reduce board size and cost, we are trying to embed everything in a single CPU.

    What is not clear up to now is whether uboot uses MMU or not. If it is not using MMU, I forcefully have to wait until uboot passes control to Linux kernel. Otherwise I can try to launch the bare metal application directly from uboot...

     

    Thanks for your time and for your answers!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
>