Single-Board Computers
  • Products & Partners
  • Dev Tools
  • Single-Board Computers
  • More
  • Cancel
Single-Board Computers
Forum Need help getting started
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Single-Board Computers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 13 replies
  • Subscribers 60 subscribers
  • Views 2313 views
  • Users 0 members are here
Related

Need help getting started

e14 Contributor
e14 Contributor over 11 years ago

I have built a small C# windows service application and need to build a small windows OS computer to run the application. The only requirements I need are Mic input, Audio output, Ethernet and I guess monitor, and usb ports for mouse and keyboard for setting up system. Once complete, no need for monitor, keyboard and mouse. The only other requirement I may need is to host a small web application to modify small configurations of the C# windows application.  This is not absolute. 

 

I am not sure what I really need to use or where to start. I can only assume the bare minimal, cost needs to be as low as possible.  Any help would be appreciated.

 

Thanks,
Shawn

  • Sign in to reply
  • Cancel

Top Replies

  • michaelkellett
    michaelkellett over 11 years ago +1
    You could look at the Brix Ultra Compact Celeron PC, SB0565041 from CPC (One of Farnell's alter egos). £79 but you need to add RAM, hard drive and OS - very neat and small but possibly no cheaper than…
Parents
  • michaelkellett
    0 michaelkellett over 11 years ago

    You could look at the Brix Ultra Compact Celeron PC, SB0565041 from CPC (One of Farnell's alter egos). £79 but you need to add RAM, hard drive and OS - very neat and small but possibly no cheaper than the BP1AD Commercial Pentium SFF PC (SB0563541) from the same place which comes complete at £199.

     

    Another reasonable buy is

    Asus UN42 VivoMini Mini PC Celeron (2957U) 1.4GHz Processor 2GB 32GB SSD
    Read more at http://www.tesco.com/direct/asus-un42-vivomini-mini-pc-celeron-2957u-14ghz-processor-2gb-32gb-ssd/701-5637.prd#0hUCwt15Y5ymSsFT.99

     

    From Tesco at £211

     

    Of course if you need really cheap just get a second hand desktop PC locally - shouldn't cost more than £30.

     

    MK

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • michaelkellett
    0 michaelkellett over 11 years ago

    You could look at the Brix Ultra Compact Celeron PC, SB0565041 from CPC (One of Farnell's alter egos). £79 but you need to add RAM, hard drive and OS - very neat and small but possibly no cheaper than the BP1AD Commercial Pentium SFF PC (SB0563541) from the same place which comes complete at £199.

     

    Another reasonable buy is

    Asus UN42 VivoMini Mini PC Celeron (2957U) 1.4GHz Processor 2GB 32GB SSD
    Read more at http://www.tesco.com/direct/asus-un42-vivomini-mini-pc-celeron-2957u-14ghz-processor-2gb-32gb-ssd/701-5637.prd#0hUCwt15Y5ymSsFT.99

     

    From Tesco at £211

     

    Of course if you need really cheap just get a second hand desktop PC locally - shouldn't cost more than £30.

     

    MK