Single-Board Computers
  • Products
  • Dev Tools
  • Single-Board Computers
  • More
  • Cancel
Single-Board Computers
Forum Explore-NFC, neard, neardal incompatibilities
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Single-Board Computers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 3 replies
  • Subscribers 59 subscribers
  • Views 644 views
  • Users 0 members are here
Related

Explore-NFC, neard, neardal incompatibilities

e14 Contributor
e14 Contributor over 11 years ago

I have purchased two Explore-NFC boards and connected them to Raspberry Pi 2 B boards.  I downloaded SW282713, which contains three .deb files.  These all install nicely and allow explorenfc-basic to work just fine. 

QUESTION #1: However, the download SW282814 contains neard-explorenfc-0.8.  Within this is a file examples/basic.c.  It uses a structure, neardal_tag, which is incompatible with neardal_tag definition in neardal.h (from the only neardal available, neardal-0.14). Where is the version of neardal that you used to compile basic.c?  It is clearly not neardal-0.14!

I have also attempted to follow the README.md instructions.  Many of the apt-get commands do not work, for those versions are no longer available or the command is incomplete.  I was able to work around each of the inconsistencies in this readme.md file, and get to the point of compiling examples/basic.c by getting an older version from your web site. I can now create my own NFC card reading programs, but this leads to the following question:

QUESTION #2: I would like to use the neard and/or neardal libraries to develop an NFC peer-to-peer capability.  I cannot find any documentation on the API for either of these libraries.  (The only thing I can find is to read the actual C code for neard and neardal examples, which may be woefully incomplete.) Please provide me with documentation or links to documentation describing the API calls available for neard and neardal.

I am not a hobbyist. I am a commercial developer attempting to design a product that would incorporate an NXP NFC chip.

  • Sign in to reply
  • Cancel
Parents
  • element14support
    0 element14support over 11 years ago

    Hello eddie24

    Welcome to the element14 Community, I will move this over to the Single-Board Computers area as it is a better fit.

     

    Thank you,

     

    Jamie

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • element14support
    0 element14support over 11 years ago

    Hello eddie24

    Welcome to the element14 Community, I will move this over to the Single-Board Computers area as it is a better fit.

     

    Thank you,

     

    Jamie