Single-Board Computers
  • Products & Partners
  • Dev Tools
  • Single-Board Computers
  • More
  • Cancel
Single-Board Computers
Forum Please recommend a Linux SBC with Industrial stability while it is made in ABC?
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Single-Board Computers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 13 replies
  • Subscribers 57 subscribers
  • Views 3039 views
  • Users 0 members are here
Related

Please recommend a Linux SBC with Industrial stability while it is made in ABC?

HKPhysicist
HKPhysicist over 2 years ago

Hello Engineers,

  • I have even tried the BeaglePlay SBC which is out-sourced to China SeeedStudio`s production line in Vietnam.  It's TI WL card dies after 6 months of purchase and after 70 days of stability test while it did nothing. Rage

  • I personally also like Raspberry Pi4 because it is stable while running under a chip fan.  Also, it is made in Wales, UK!  Quality is the top in the industry!  Heart eyes  However, it is not within the industrial electronic requirement (-40C/-20C to 85C).

  • So could any expert introduce a Linux SBC (working as a border router with LTE dialup) with at least 2GB RAM, 16GB eMMC, average video without graphical acceleration, a wireless lan, an Ethernet, and the last but not the least, not made in China.  The cost of electronic made in China is actually very high!!! Rage
  • Is Snapdrogon 410 board within the industrial stability standard?

Thanks for your opinions.

Nerd

  • Sign in to reply
  • Cancel

Top Replies

  • electronicbiker
    electronicbiker over 2 years ago in reply to shabaz +2
    Raspberry Pi make the 'Compute' module which I believe is used in various industrial-grade PLC's and the like. I don't know much about it as a) I've never had cause to use it, b) the last company I worked…
  • Cquk
    Cquk over 2 years ago +2
    We used the PI CM4 module. It has the best support and you can be sure of ongoing updates. Some of the other systems we used needed "Custom" linux. That was out of date or hard to compile
  • phoenixcomm
    phoenixcomm over 2 years ago +2
    HKPhysicist Ok, here we go! First, the pi will not do it. as it lacks multiple RJ45s, one for incoming the other for outgoing. Personally build a Box and put in it OpenBSD it comes with the best firewall…
Parents
  • phoenixcomm
    0 phoenixcomm over 2 years ago

     HKPhysicist Ok, here we go! First, the pi will not do it. as it lacks multiple RJ45s, one for incoming the other for outgoing. Personally  build a Box and put in it OpenBSD it comes with the best firewall/router in the biz, has never ever been hacked, small learning curve. My box that I pulled together is running 4 network connections, plus one on the mother board which makes 5.

    1.  All inbound, and outbound traffic
    2. Public HTML server VOIP server  (two public addresses Astrix (Rasberry PI) and has a USB to Ethernet for the Phones) 
    3. Second PI for the PIhole
    4. Nat to the internal network 197.168.x.x
    5. back do for special stuff  

    You cant do that on the PI!!  any older box will do. 8Gb of memory (P2) and 1 Gb HDA 

    So where did I get all the ports from?? Simple put in a few adapters.  ~~ Good Luck Cris H. 

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • phoenixcomm
    0 phoenixcomm over 2 years ago

     HKPhysicist Ok, here we go! First, the pi will not do it. as it lacks multiple RJ45s, one for incoming the other for outgoing. Personally  build a Box and put in it OpenBSD it comes with the best firewall/router in the biz, has never ever been hacked, small learning curve. My box that I pulled together is running 4 network connections, plus one on the mother board which makes 5.

    1.  All inbound, and outbound traffic
    2. Public HTML server VOIP server  (two public addresses Astrix (Rasberry PI) and has a USB to Ethernet for the Phones) 
    3. Second PI for the PIhole
    4. Nat to the internal network 197.168.x.x
    5. back do for special stuff  

    You cant do that on the PI!!  any older box will do. 8Gb of memory (P2) and 1 Gb HDA 

    So where did I get all the ports from?? Simple put in a few adapters.  ~~ Good Luck Cris H. 

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • Jan Cumps
    0 Jan Cumps over 2 years ago in reply to phoenixcomm
    phoenixcomm said:
    has never ever been hacked

    The internet says it has been hacked