Single-Board Computers
  • Products & Partners
  • Dev Tools
  • Single-Board Computers
  • More
  • Cancel
Single-Board Computers
Forum Best SBC for Analogic Sensor Reading and Actuation (PWM)
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Single-Board Computers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 0 replies
  • Subscribers 56 subscribers
  • Views 350 views
  • Users 0 members are here
  • sample_rate
  • sbc
  • realtime
  • polling rate
  • adc
Related

Best SBC for Analogic Sensor Reading and Actuation (PWM)

inthevoid
inthevoid over 10 years ago

Hello!

 

I'm looking for suggestions on which SBC to choose or maybe some other platform.

 

The requirements are:

- ADC with minimum 12bit resolution (best for the wider input range it's capable e.g. 0-5V)

- The software and hardware must be capable of at least 500Hz polling rate of that ADC

- Must have horsepower for heavy computations, e.g. Fast single thread process time of math.

- At least 4 PWMs with at least 10bit resolution with adjustable modulation frequency (e.g. 14Hz)

 

I used Arduino mega 2560 before, but it couldn't handle the computation and the ADC was poor. I looked at Arduino Due but the 3.3V ADC is a deal breaker. That's why I'm looking at SBC now, however any suggestions are welcome.

 

I'm aware that linux have limited polling rate (at least for USB). I'm hoping I can get faster access to the ADC on these boards.

Also I know that there are ADC modules that are capable of lots of samples per second, however I need to access that data *on the SBC* at 500Hz.

 

Thanks in advance! image