GIZMO 2
  • Products & Partners
  • Dev Tools
  • Single-Board Computers
  • GIZMO 2
  • More
  • Cancel
GIZMO 2
Blog Gizmo 2 - Out of the box
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join GIZMO 2 to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: xever
  • Date Created: 16 Apr 2015 8:43 AM Date Created
  • Views 3123 views
  • Likes 1 like
  • Comments 9 comments
  • gizmo2
  • gizmo
Related
Recommended

Gizmo 2 - Out of the box

xever
xever
16 Apr 2015

I have received my Gizmo 2 just before the Easter weekend.  Its arrival was perfect timing for me to see try out its capabilities out of the box and share that experience in this post.  There are already a few great reviews in this community who had earlier access to this wonderful single board machine, and I strongly recommend them as they are well worth the read.

 

What's inside the box?

image

Upon opening the box, one will find:

- The Gizmo 2 Single Board Computer inside the anti-static bag

- A Kensington 4GB microSD card preloaded with Timesys Embedded Linux Demo

- 12V DC travel adapter

- and a Quick Start Guide

 

Form Factor and Peripherals

The Gizmo 2 board measures 10cmx10cm (or approximately 4inx4in), almost twice the size of Raspberry Pi and about a quarter of Advantech mini-ITX x86-based board I have lying around.

imageimage

Comparing the Gizmo 2 board with another x86 SBC, Vortex Tiny SBC Module VDX-6318, the Gizmo 2 board is relatively larger as can be seen in the picture below.

image

For the peripherals, the Gizmo 2 is packed with modern connectivity ports:

 

image.php?id=0x2014&image=amd_gizmo2_linux

 

Physical PCIe 36-pin and x4 edge connectors standout between the boards presented above.  These edge connectors provide direct access to the embedded peripherals of the board, i.e. GPIO, ADC/DAC, PWM, SPI, (more) USB, I2C, display port, PCIe, and SATA.  By designing a daughter board, the Gizmo's functionality can be extended to meet other application requirements.  Some of the examples that I can think of is by the creation of a daughter board with SATA connector, the Gizmo board can be used to build a NAS server.  Another would be to directly interface with sensors and read sensor values via ADC, or connect to other RF modules such as ZigBee through the SPI lines, etc.  With this capability, it actually makes it possible to create a product application utilising low-level peripherals without the need for an extra MCU.

 

Embedded Linux OS

The 4GB microSD card that came with the board is preloaded with an embedded Linux OS and Timesys embedded demo (launcher) application.  Booting from the included microSD card will automatically run Timesys Launcher application and starts off with a quick tutorial on how to use the launcher application.  There are five round buttons on top of the screen, (1) Video Player Demo (2) About GizmoSphere (3) Exit to Desktop (4) XBMC launcher (5) About Timesys.  So I started to see how video playback would be and launched the Video Player Demo.

 

Side note.  The navigation of this UI is horrendous, the button on the top are NOT clickable, you have to click one side and drag the pointer to either left or right simulating a "swipe" action to highlight a button.  This UI and its experience is really bad when using a mouse and non-touch monitor (or TV in most cases).

 

The demo video player plays the Big Buck Bunny clip smoothly on 1080p, keen to test the video on 4K UHD-TV (will update soon).

 

Testing out XBMC

XBMC is... well XBMC and it can only be experienced fully if the system is connected to the Internet (at least initially) so it can be configured and can be used to stream online channels.  All being good and being used to XBMC, I added more videos to test and so I stuck one movie in a USB flash drive and added that to the play list.  The movie did play just fine except when it requires to refresh fast, triangles used in rendering the video can be noticed.

 

image

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

Since I wanted to connect the Gizmo 2 board to my monitor in the room where there is no LAN cable running, I decided to attach a USB WiFi dongle to connect to the network.  However the default OS does not provide any default drivers.

 

Desktop Applications

The Desktop is XFCE and has a few standard pre-installed apps, such as Firefox, LeafPad, and Screen Grabber Util among others.  I was able to run Firefox once to experience web browsing on the Gizmo board and relate that experience with rPi (for example).  However, running Firefox seemed to have slowed down the whole system, and typing on the address bar was really clunky to a point that the system felt frozen and unresponsive.  This happened a few times to a point where I now can no longer run the Firefox.

 

Since I wanted to capture the Timesys Launcher screen, I attempted to use the screen grabbing tool and set a delay to capture the whole screen after 10 seconds.  This did not seemed to work, starting the countdown and switching the app to show the Timesys launcher halted the whole system and had to restart.  I stopped after a few moments and decided not to spend more time with the default OS.

  • Sign in to reply

Top Comments

  • e14 Contributor
    e14 Contributor over 11 years ago in reply to DAB +2
    Hey :-) I was just coming online to post a quick blog about the Gizmo 2 performance and a little gem of information that might help you out with your issues. I was amazed by the initial performance if…
  • xever
    xever over 11 years ago in reply to shabaz +1
    Thanks for the info Shabaz. It really just happens during fast scenes that seemed to do a lot of rendering. Am about to test it on an UHDTV and visibly check if it is any worse. If so, then as a work around…
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to xever

    Hi, I've attached prebuilt packages to the Gizmo on Fire blog post.

     

    Let me know how you get on with them image

     

    Lucie

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • xever
    xever over 11 years ago in reply to e14 Contributor

    I get what you mean now, thanks.  Oh yeah, if you can share the .deb packages that would be great as well, and I will re-run my perf tests.  I have installed Ubuntu and so far so good, the Timesys one caused some griefs. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to e14 Contributor

    For the package builder go to

     

    http://support.amd.com/en-us/download

     

    Then scroll down and choose the following options from the lists

     

    Embedded graphics》radeon embedded》g-series》linuxx86 /x86-64

     

    Linux x86 is for the 32bit 386 distros and the x86/64 is for the 64 bit 686 distros. Those options should take you to the catalyst display driver for gseries soc devices.

     

    Good luck

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to xever

    Hi,

     

    The cores only run at 100% while the packages are being compiled. After that, you just install them. I'll see if i can work out the process for getting back to them.

     

    If you like, i'll upload the .deb packages that i already compiled. They  are compiled to run specifically on ubuntu so wont work for any other distro's.

     

    Ubuntu should auto allocate some swap space, other versions of linux require it to be manually configured so it was probably overlooked with the included software.

     

     

    Lucie

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • xever
    xever over 11 years ago in reply to e14 Contributor

    Thanks for the info.  The link you provided seemed to be broken, or at least redirects to me to "Download Incomplete" page.

    You will probably have to install a few other dependancies to be able to build packages and the whole thing runs both cores at 100% for about 10minutes but the end result is fully worth it.

    So what happens after 10 minutes? Will it stop running at 100%?

     

    Firefox happens to work fine in Ubuntu, but not on the Timesys Embedded Linux.

     

    Regards,

     

    Christever

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
>