GIZMO 2
  • Products & Partners
  • Dev Tools
  • Single-Board Computers
  • GIZMO 2
  • More
  • Cancel
GIZMO 2
Blog Gizmo 2 - Out of the box
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join GIZMO 2 to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: xever
  • Date Created: 16 Apr 2015 8:43 AM Date Created
  • Views 3123 views
  • Likes 1 like
  • Comments 9 comments
  • gizmo2
  • gizmo
Related
Recommended

Gizmo 2 - Out of the box

xever
xever
16 Apr 2015

I have received my Gizmo 2 just before the Easter weekend.  Its arrival was perfect timing for me to see try out its capabilities out of the box and share that experience in this post.  There are already a few great reviews in this community who had earlier access to this wonderful single board machine, and I strongly recommend them as they are well worth the read.

 

What's inside the box?

image

Upon opening the box, one will find:

- The Gizmo 2 Single Board Computer inside the anti-static bag

- A Kensington 4GB microSD card preloaded with Timesys Embedded Linux Demo

- 12V DC travel adapter

- and a Quick Start Guide

 

Form Factor and Peripherals

The Gizmo 2 board measures 10cmx10cm (or approximately 4inx4in), almost twice the size of Raspberry Pi and about a quarter of Advantech mini-ITX x86-based board I have lying around.

imageimage

Comparing the Gizmo 2 board with another x86 SBC, Vortex Tiny SBC Module VDX-6318, the Gizmo 2 board is relatively larger as can be seen in the picture below.

image

For the peripherals, the Gizmo 2 is packed with modern connectivity ports:

 

image.php?id=0x2014&image=amd_gizmo2_linux

 

Physical PCIe 36-pin and x4 edge connectors standout between the boards presented above.  These edge connectors provide direct access to the embedded peripherals of the board, i.e. GPIO, ADC/DAC, PWM, SPI, (more) USB, I2C, display port, PCIe, and SATA.  By designing a daughter board, the Gizmo's functionality can be extended to meet other application requirements.  Some of the examples that I can think of is by the creation of a daughter board with SATA connector, the Gizmo board can be used to build a NAS server.  Another would be to directly interface with sensors and read sensor values via ADC, or connect to other RF modules such as ZigBee through the SPI lines, etc.  With this capability, it actually makes it possible to create a product application utilising low-level peripherals without the need for an extra MCU.

 

Embedded Linux OS

The 4GB microSD card that came with the board is preloaded with an embedded Linux OS and Timesys embedded demo (launcher) application.  Booting from the included microSD card will automatically run Timesys Launcher application and starts off with a quick tutorial on how to use the launcher application.  There are five round buttons on top of the screen, (1) Video Player Demo (2) About GizmoSphere (3) Exit to Desktop (4) XBMC launcher (5) About Timesys.  So I started to see how video playback would be and launched the Video Player Demo.

 

Side note.  The navigation of this UI is horrendous, the button on the top are NOT clickable, you have to click one side and drag the pointer to either left or right simulating a "swipe" action to highlight a button.  This UI and its experience is really bad when using a mouse and non-touch monitor (or TV in most cases).

 

The demo video player plays the Big Buck Bunny clip smoothly on 1080p, keen to test the video on 4K UHD-TV (will update soon).

 

Testing out XBMC

XBMC is... well XBMC and it can only be experienced fully if the system is connected to the Internet (at least initially) so it can be configured and can be used to stream online channels.  All being good and being used to XBMC, I added more videos to test and so I stuck one movie in a USB flash drive and added that to the play list.  The movie did play just fine except when it requires to refresh fast, triangles used in rendering the video can be noticed.

 

image

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

Since I wanted to connect the Gizmo 2 board to my monitor in the room where there is no LAN cable running, I decided to attach a USB WiFi dongle to connect to the network.  However the default OS does not provide any default drivers.

 

Desktop Applications

The Desktop is XFCE and has a few standard pre-installed apps, such as Firefox, LeafPad, and Screen Grabber Util among others.  I was able to run Firefox once to experience web browsing on the Gizmo board and relate that experience with rPi (for example).  However, running Firefox seemed to have slowed down the whole system, and typing on the address bar was really clunky to a point that the system felt frozen and unresponsive.  This happened a few times to a point where I now can no longer run the Firefox.

 

Since I wanted to capture the Timesys Launcher screen, I attempted to use the screen grabbing tool and set a delay to capture the whole screen after 10 seconds.  This did not seemed to work, starting the countdown and switching the app to show the Timesys launcher halted the whole system and had to restart.  I stopped after a few moments and decided not to spend more time with the default OS.

  • Sign in to reply

Top Comments

  • e14 Contributor
    e14 Contributor over 11 years ago in reply to DAB +2
    Hey :-) I was just coming online to post a quick blog about the Gizmo 2 performance and a little gem of information that might help you out with your issues. I was amazed by the initial performance if…
  • xever
    xever over 11 years ago in reply to shabaz +1
    Thanks for the info Shabaz. It really just happens during fast scenes that seemed to do a lot of rendering. Am about to test it on an UHDTV and visibly check if it is any worse. If so, then as a work around…
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to DAB

    Hey :-)

     

    I was just coming online to post a quick blog about the Gizmo 2 performance and a little gem of information that might help you out with your issues.

     

    I was amazed by the initial performance if Gizmo 2 but had also noticed some occasional system hanging for a second or two for really no reason. I did a bit of searching about and came across the drivers for the actual SOC device. The download is here http://www2.ati.com/drivers/embedded/14.502.1015-150305a-181697e-aes.zip unzip it and run the .run file as an administrator or super user. There is a prebuilt package option or a choice to build your own which I chose. You will probably have to install a few other dependancies to be able to build packages and the whole thing runs both cores at 100% for about 10minutes but the end result is fully worth it. The performance increase is astonishing once you have installed the packages. Plus you get a nice GUI app for configuring graphics adapter settings.

     

    Another thing that might be causing your slowdown with firefox is memory issues. If you haven't already, make a swap partition, I set mine to 2GB  and modify your fstab file. You can try it out before modifying the file by making the partition, then right clicking it in gparted and selecting swap on. The swap partition is there for the system to move resources out of ram that arent currently being used so applications that are being used can utilise that space. It's similar to the page file or virtual memory in windows.

     

    I turned mine off to shift it along the drive and my system became pretty much unusable till I closed firefox down (webpages are huge these days...)

     

      Lucie

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DAB
    DAB over 11 years ago

    Nice post.

     

    The board looks capable enough, but if the software is not up to snuff, then people will just not use it.

     

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • xever
    xever over 11 years ago in reply to shabaz

    Thanks for the info Shabaz.  It really just happens during fast scenes that seemed to do a lot of rendering.  Am about to test it on an UHDTV and visibly check if it is any worse.  If so, then as a work around will have to disable acceleration as you have done.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 11 years ago

    Hi Christever!

     

    I too had issues with graphics acceleration too so when I installed a new OS, I changed the video output mode to not use the acceleration in the application I was using at the time (probably mplayer) and then the output quality was good for HD resolution video.

    I tested a couple of months ago, so I don't know if the driver has been fixed since then.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
<