BeagleBoard
  • Products & Partners
  • Dev Tools
  • Single-Board Computers
  • BeagleBoard
  • More
  • Cancel
BeagleBoard
Blog BBB - Building a DAC
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join BeagleBoard to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: shabaz
  • Date Created: 6 Jul 2013 7:19 PM Date Created
  • Views 17197 views
  • Likes 8 likes
  • Comments 126 comments
  • onsemi
  • audio
  • dac
  • bbb
  • texas_instruments
  • bb_black
  • beagle_bone_black
  • ti
Related
Recommended

BBB - Building a DAC

shabaz
shabaz
6 Jul 2013

Introduction

This project was about getting audio out of the BeagleBone Black. The aim was to have stereo audio, at least as good as an iPod. See further below for the circuit, and also a video showing it working.

Later, this project was used to build a PCB design (see below for the link to this part 2, and then the PCB was used to make a home Sonos-type hi-fi audio player (see the link to part 3 below).

 

The BBB has an on-board I2S interface, which makes interfacing an external DAC easy. The I2S interface is connected from the AM3359 processor to the HDMI chip (TDA19988) but it is not required for HDMI to be used in order to make use of the I2S interface. The I2S interface is brought out to some pins on port P9 (see here for details). It was encouraging that Technoshaman and Donald Miller had some success with the interface, so I wanted to try it out and I got some time today.

 

Part 2 to this post, which implements the prototype, can be found by clicking here.

image

Part 3 implements a complete design in an enclosure for a Sonos-like solution.

image

See Creating an Internet Radio for a complete project by the EAGLE team including board layouts

image

 

Parts Selection

Since the interface is capable of 24-bit/192kHz audio, it was worthwhile picking a nice DAC. A good but not over-the-top device seemed to be the Texas Instrument's PCM5101 which is nice because it has reasonable specs and also provides a built-in charge pump so that it can function from a single supply. A headphone amp was connected, and this was ON Semi's NCP2811A. The combination of PCM5101 (actually my prototype used PCM5101A which can also function from 1.8V, but this was not needed)  and NCP2811A was chosen so that the entire circuit could operate from the BBB supply if desired, even if it was from a Li-Ion battery that was powering the BBB, and for low noise and distortion. The only problem is that the PCM5101 has quite a high output (clearly a good thing!) but the audio amp minimum recommended gain is 1 and it cannot meet the required output voltage, and it means that it will distort at high volume. So, at a lower volume (and lower SNR) it will be fine, and I prefer this particular amp because of the very low distortion. The ON semi datasheet was sparse though.

 

Building It

This is the DAC prototype:

image

This is the whole thing connected up:

image

This is the rear of the board - a bit messier! It was built on a SMD to DIP adapter board with some copper tape for supply rails:

image

This is the audio amp - not a lot to it, since it is so integrated.

image

 

Testing It

I made a recording, but excuse the quality. The audio is from a small 64 ohm speaker picked up by a simple camera in-built microphone so it sounds bad, but connecting to headphones is a different story - it sounds as good as an ipod (although this is subjective - I don't have a way to measure). Another thing I still need to check is that originally I thought the data was read on the falling edge of the bitclock on the BBB, but I2S specifies the opposite. Maybe I made a mistake in my initial observations (I have not had a chance to re-check), or maybe it changed in a build. But the circuit as shown here works for me.

 

This is running on an not-recent Angstrom downloaded build (maybe a few weeks old image), and I still hear some very slight audio issues - it sounds like perhaps a break for a few tens of milliseconds occasionally, only if you're listening closely. I really hope it is resolved in a build soon (or maybe it is due to ffmpeg - perhaps avconv gives better results).

EDIT: I've since been using mplayer (command line is mplayer -ao alsa -volume 4 AmyWinehouse-BackToBlack.mp3  and either I'm not noticing any audio issues or they have disappeared). I've concluded it sounds at least as capable as my old ipod touch, maybe better).

 

I played audio using the command line:

ffmpeg -i AmyWinehouse-YouKnowImNoGood.mp3 -f alsa "default:CARD=Black" -re -vol 150

and it reported the stream as:

Stream #0.0: Audio: pcm_s16le, 44100 Hz, stereo, s16, 1411 kb/s

 

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

Circuit Diagram

This is the circuit. All the 3.3V supplies were connected together for the prototype (I wouldn't do that for real, although it sounded very good in my limited tests). The amplifier V+ can be connected to 3.3V or the 5V supply (or the Li-Ion battery directly).

Note 16th Jan 2014: See the comments section below for more detail; the SCK pin on the PCM5101A was disconnected from 0V and instead connected to the BBB P9 pin 25. This will provide the lowest jitter by disabling the DAC's internal PLL. A sample capture of the audio quality (captured from the headphone output of the NCP2811A, just to give an approximate idea of what it sounds like from headphones) is attached to the post below, in the zip file dac-output.zip. More info on it in the comments section below.

Note 2: Please add a logic inverter to the bitclock connection. For more detail, see the comments below (search for the word 'bitclock' to make it easier to find). See the part 2 blog post, and the attached file there called dac-documentation.zip for the circuit diagram, showing the bitclock inversion. More recent BBB images may not need it, but it was certainly needed for the images I tested with.

image

 

Experiments with FLAC

I've also tried a FLAC file, but I'm hitting some limitation with ffmpeg it seems, and it picks a 16-bit format when it ought to be 24-bit. Meanwhile, avconv I couldn't get to work for MP3 or FLAC (it reported 'av_interleaved_write_frame(): Resource temporarily unavailable'). If anyone knows, any tips on how to play FLAC at 24-bit would be gratefully appreciated.

 

root@beaglebone:~# ffmpeg -i Taxman_2009_Digital_Remaster.flac -f alsa "default:CARD=Black" -re -vol 5
ffmpeg version v0.8.4, Copyright (c) 2000-2012 the Libav developers
  built on May 20 2013 13:00:42 with gcc 4.7.3 20130205 (prerelease)
This program is not developed anymore and is only provided for compatibility. Use avconv instead (see Changelog for the list of incompatible changes).
[flac @ 0x2da80] max_analyze_duration reached
Input #0, flac, from 'Taxman_2009_Digital_Remaster.flac':
  Metadata:
    ORIGREFERENCE   : 6C05C9F79EE74052A7991B9669B98533
    ORIGDATE        : 2009:09:14
    ORIGTIME        : 11:57:01
    TIMEREFERENCE   : 5292000
    CODINGHISTORY   : A=PCM,F=44100,W=24,M=stereo,T=SADiE5
    ORGANIZATION    : EMI
    TITLE           : Taxman
    track           : 1
    ARTIST          : The Beatles
    ALBUM           : Revolver (24 BIT Remastered)
    DATE            : 2009
  Duration: 00:02:37.85, bitrate: 1892 kb/s
    Stream #0.0: Audio: flac, 44100 Hz, 2 channels, s32
Incompatible sample format 's32' for codec 'pcm_s16le', auto-selecting format 's16'
Output #0, alsa, to 'default:CARD=Black':
  Metadata:
    ORIGREFERENCE   : 6C05C9F79EE74052A7991B9669B98533
    ORIGDATE        : 2009:09:14
    ORIGTIME        : 11:57:01
    TIMEREFERENCE   : 5292000
    CODINGHISTORY   : A=PCM,F=44100,W=24,M=stereo,T=SADiE5
    ORGANIZATION    : EMI
    TITLE           : Taxman
    track           : 1
    ARTIST          : The Beatles
    ALBUM           : Revolver (24 BIT Remastered)
    DATE            : 2009
    encoder         : Lavf53.21.0
    Stream #0.0: Audio: pcm_s16le, 44100 Hz, 2 channels, s16, 1411 kb/s
Stream mapping:
  Stream #0.0 -> #0.0

Attachments:
dac-output.zip
  • Sign in to reply

Top Comments

  • e14 Contributor
    e14 Contributor over 12 years ago in reply to e14 Contributor +2
    Current test rig. BBB ($45), cs4271 on breadboard (about $15 parts and dozens of hours of labor), Cary Audio SE-1 amp (about $1K), pair of B&W DM302 speakers (about $200). I assembled this system that…
  • shabaz
    shabaz over 8 years ago in reply to shabaz +2
    Also, unrelated, but for after you have resolved the device tree issue, I just wanted to confirm, if you're following the circuit, make sure you include the 'bitclock inversion' functionality. The BBB…
  • shabaz
    shabaz over 8 years ago in reply to jithu_element14 +2
    Hi Jithu, Just to follow up on this, I re-tried on another image too, but still no luck. I've posted a request for help on the Beagleboard.org BBB-Wireless forum, in case anyone else has had success. Reproducing…
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to e14 Contributor

    Hi John, i've following this thread closely, by the way: excellent work!

    I'm trying to build a ADC for the BBB, the hardware part is done, but i'm stuck with the software... Do you think that your implementation could be modified for reading I2S data? are you using the tda998x driver??

    Regards

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago

    Success at long last! I now have my cs4271 acting as a clock master and able to interface with the alsa sound system at 48, 96, and 192 kHz. The sound quality is nearly flawless, even with my breadboard layout. The only flaw I hear is a very low level of digital grunginess, so low level that you have to put your ear right against the speaker with the volume fully turned up to hear it. From normal listening distances, it is inaudible. I cannot hear any distortion at all (need to make some measurements). 192 kHz and 96 kHz sound exactly the same to me, but that's not surprising. The input stage of the hifi system to which the analog output of the beaglebone-cs4271 is connected first converts analog to 96 kHz digital. So I have not ever actually heard anything rendered at 192 kHz. There is a slight but obvious, once you train your ears, step up in sound quality going from 48 kHz to 96 kHz. Oddly this can be heard even playing 44.1 kHz tracks ripped from CDs, though it is more obvious on material that was recorded at higher bit rates (I have several 176 kHz tracks obtained from HDTracks.)

     

    Next is to figure out what I actually did in the guts of the sound driver that made it work and why, remove gobs of debug prints, and make a clean patch with just the necessary parts. There are a couple of oddities I don't understand yet. With the mcasp in slave mode, it sends the audio serial bit stream to the DAC on a different pin than when it is in master mode, in fact it sends the serial data on P9.25, which is normally the 24.576 MHz master clock output! I saw nothing in the documentation about this and I never would have guessed it, but I accidentally noticed it on my scope while trying to figure out why nothing was working. Another other oddity is that I'm not sending the master clock frequency from the sound chip to the beagleboard at all. I couldn't figure out where to connect it, given that P9.25 is not an input pin. I suppose mcasp is syncing to the serial clock, which I'm sending on P9.31.

     

    I'm going to make a printed circuit board for the DAC, which hopefully will get rid of the digital grunge. I'll use a different DAC chip, since the cs4271 is quite old and requires more external circuitry than more modern DACs. I started with the cs4271 since there was already a driver for it on the beaglebone. Also I need at least four channels of output and the cs4271 has only two. There are more modern DACs that have up to 8 channels out.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to shabaz

    Hi Everyone image

     

    I'm so glad to see incoming answers. Thanks everyone. Allow me to congratulate you John. I'm following your way and digging into kernel source in that file you have specified. I'm a barely newbie on kernel sources and understanding how the source files works it's quite difficult for me. But i will not give up.

     

    The most important thing , for me, it's to have new tips to find out the solution.

     

    I hope to give you some good news soon .

     

    I have bought this EVM PCM5102EVM-U Texas Instruments | 296-29268-ND | DigiKey

    to avoid manual soldering and tests the quality of the audio output. I hope it will be helpful

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 12 years ago in reply to e14 Contributor

    Hi John,

     

    Thanks for the information. It was a bit of a long shot, I hoped that the I2C may not matter :-( It's great you have 96k functioning. As you say, it is likely just some tweak/I2C register content change like alignment, word size, etc. before the sound comes out perfect.

    If you're getting sound but it sounds bad, it may be just layout related - not sure if the breadboard may be a step too far at these frequencies.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to shabaz

    The HDMI audio does use a different audio device than the audio cape. KERNEL/sound/soc/davinci has the source codes, which I'm currently trying to understand. It appears that an audio device using davinci is actually a composite of mcasp, a codec chip, a dma engine, with davinci gluing everything together. I managed to put together an audio device using davinci and an external cs4271 chip. It does work in that the audio device is created and it will play a .wav file using aplay, but the sound quality is horrible. Also the only clock rate I can generate is 96kHz. The control interface to the cs4271 is I2C and it is vital that it actually works. If the davinci part of the audio device cannot read/write the I2C port correctly, it will report a failure. It took me a while to get the I2C interface to the external audio chip working; it was initially not responding to I2C read/write commands. Looking at the waveforms on a scope, I noticed that the rise time spec of the cs4271 of the I2C SDA signal was being violated. I put some 6.8k ohm resistor pullups from the I2C pins to the 3.3v rail to speed up the rise time and changed the power supply arrangement around, and then the I2C communication started working.

     

    I did notice that some of the SPI drivers do not require davinci to be able to read from the external audio chip (they instead keep a local cache of values sent). Maybe you could use SPI instead of I2C in which case davinci would never notice that its control commands are being ignored. This is just a guess, but try changing the audio cape to make the chip use SPI. For example, in BB-BONE-AUDI-01-00A0.dts, change

     

    ----

    fragment @3 {

      target = <&i2c2>;

      __overlay__

      ...

    ----

    to

    ----

    fragment @3 {

      target = <&spi0>;

      __overlay__

      ...

    ----

     

    I have not tried this, so good luck.

     

    I expect that the reason my test setup sounds horrible is that there is a difference of opinion between mcasp and cs4271 about whether clocks are inverted, or MSB delay from frame sync, or some such incompatibility. I'm studying davinci-evm.c and davinci-mcasp.c now to figure out what they are actually doing to set up mcasp. Hopefully that's all that needs fixing.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>