BeagleBoard
  • Products & Partners
  • Dev Tools
  • Single-Board Computers
  • BeagleBoard
  • More
  • Cancel
BeagleBoard
Blog BBB - Building a DAC
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join BeagleBoard to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: shabaz
  • Date Created: 6 Jul 2013 7:19 PM Date Created
  • Views 17203 views
  • Likes 8 likes
  • Comments 126 comments
  • onsemi
  • audio
  • dac
  • bbb
  • texas_instruments
  • bb_black
  • beagle_bone_black
  • ti
Related
Recommended

BBB - Building a DAC

shabaz
shabaz
6 Jul 2013

Introduction

This project was about getting audio out of the BeagleBone Black. The aim was to have stereo audio, at least as good as an iPod. See further below for the circuit, and also a video showing it working.

Later, this project was used to build a PCB design (see below for the link to this part 2, and then the PCB was used to make a home Sonos-type hi-fi audio player (see the link to part 3 below).

 

The BBB has an on-board I2S interface, which makes interfacing an external DAC easy. The I2S interface is connected from the AM3359 processor to the HDMI chip (TDA19988) but it is not required for HDMI to be used in order to make use of the I2S interface. The I2S interface is brought out to some pins on port P9 (see here for details). It was encouraging that Technoshaman and Donald Miller had some success with the interface, so I wanted to try it out and I got some time today.

 

Part 2 to this post, which implements the prototype, can be found by clicking here.

image

Part 3 implements a complete design in an enclosure for a Sonos-like solution.

image

See Creating an Internet Radio for a complete project by the EAGLE team including board layouts

image

 

Parts Selection

Since the interface is capable of 24-bit/192kHz audio, it was worthwhile picking a nice DAC. A good but not over-the-top device seemed to be the Texas Instrument's PCM5101 which is nice because it has reasonable specs and also provides a built-in charge pump so that it can function from a single supply. A headphone amp was connected, and this was ON Semi's NCP2811A. The combination of PCM5101 (actually my prototype used PCM5101A which can also function from 1.8V, but this was not needed)  and NCP2811A was chosen so that the entire circuit could operate from the BBB supply if desired, even if it was from a Li-Ion battery that was powering the BBB, and for low noise and distortion. The only problem is that the PCM5101 has quite a high output (clearly a good thing!) but the audio amp minimum recommended gain is 1 and it cannot meet the required output voltage, and it means that it will distort at high volume. So, at a lower volume (and lower SNR) it will be fine, and I prefer this particular amp because of the very low distortion. The ON semi datasheet was sparse though.

 

Building It

This is the DAC prototype:

image

This is the whole thing connected up:

image

This is the rear of the board - a bit messier! It was built on a SMD to DIP adapter board with some copper tape for supply rails:

image

This is the audio amp - not a lot to it, since it is so integrated.

image

 

Testing It

I made a recording, but excuse the quality. The audio is from a small 64 ohm speaker picked up by a simple camera in-built microphone so it sounds bad, but connecting to headphones is a different story - it sounds as good as an ipod (although this is subjective - I don't have a way to measure). Another thing I still need to check is that originally I thought the data was read on the falling edge of the bitclock on the BBB, but I2S specifies the opposite. Maybe I made a mistake in my initial observations (I have not had a chance to re-check), or maybe it changed in a build. But the circuit as shown here works for me.

 

This is running on an not-recent Angstrom downloaded build (maybe a few weeks old image), and I still hear some very slight audio issues - it sounds like perhaps a break for a few tens of milliseconds occasionally, only if you're listening closely. I really hope it is resolved in a build soon (or maybe it is due to ffmpeg - perhaps avconv gives better results).

EDIT: I've since been using mplayer (command line is mplayer -ao alsa -volume 4 AmyWinehouse-BackToBlack.mp3  and either I'm not noticing any audio issues or they have disappeared). I've concluded it sounds at least as capable as my old ipod touch, maybe better).

 

I played audio using the command line:

ffmpeg -i AmyWinehouse-YouKnowImNoGood.mp3 -f alsa "default:CARD=Black" -re -vol 150

and it reported the stream as:

Stream #0.0: Audio: pcm_s16le, 44100 Hz, stereo, s16, 1411 kb/s

 

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

Circuit Diagram

This is the circuit. All the 3.3V supplies were connected together for the prototype (I wouldn't do that for real, although it sounded very good in my limited tests). The amplifier V+ can be connected to 3.3V or the 5V supply (or the Li-Ion battery directly).

Note 16th Jan 2014: See the comments section below for more detail; the SCK pin on the PCM5101A was disconnected from 0V and instead connected to the BBB P9 pin 25. This will provide the lowest jitter by disabling the DAC's internal PLL. A sample capture of the audio quality (captured from the headphone output of the NCP2811A, just to give an approximate idea of what it sounds like from headphones) is attached to the post below, in the zip file dac-output.zip. More info on it in the comments section below.

Note 2: Please add a logic inverter to the bitclock connection. For more detail, see the comments below (search for the word 'bitclock' to make it easier to find). See the part 2 blog post, and the attached file there called dac-documentation.zip for the circuit diagram, showing the bitclock inversion. More recent BBB images may not need it, but it was certainly needed for the images I tested with.

image

 

Experiments with FLAC

I've also tried a FLAC file, but I'm hitting some limitation with ffmpeg it seems, and it picks a 16-bit format when it ought to be 24-bit. Meanwhile, avconv I couldn't get to work for MP3 or FLAC (it reported 'av_interleaved_write_frame(): Resource temporarily unavailable'). If anyone knows, any tips on how to play FLAC at 24-bit would be gratefully appreciated.

 

root@beaglebone:~# ffmpeg -i Taxman_2009_Digital_Remaster.flac -f alsa "default:CARD=Black" -re -vol 5
ffmpeg version v0.8.4, Copyright (c) 2000-2012 the Libav developers
  built on May 20 2013 13:00:42 with gcc 4.7.3 20130205 (prerelease)
This program is not developed anymore and is only provided for compatibility. Use avconv instead (see Changelog for the list of incompatible changes).
[flac @ 0x2da80] max_analyze_duration reached
Input #0, flac, from 'Taxman_2009_Digital_Remaster.flac':
  Metadata:
    ORIGREFERENCE   : 6C05C9F79EE74052A7991B9669B98533
    ORIGDATE        : 2009:09:14
    ORIGTIME        : 11:57:01
    TIMEREFERENCE   : 5292000
    CODINGHISTORY   : A=PCM,F=44100,W=24,M=stereo,T=SADiE5
    ORGANIZATION    : EMI
    TITLE           : Taxman
    track           : 1
    ARTIST          : The Beatles
    ALBUM           : Revolver (24 BIT Remastered)
    DATE            : 2009
  Duration: 00:02:37.85, bitrate: 1892 kb/s
    Stream #0.0: Audio: flac, 44100 Hz, 2 channels, s32
Incompatible sample format 's32' for codec 'pcm_s16le', auto-selecting format 's16'
Output #0, alsa, to 'default:CARD=Black':
  Metadata:
    ORIGREFERENCE   : 6C05C9F79EE74052A7991B9669B98533
    ORIGDATE        : 2009:09:14
    ORIGTIME        : 11:57:01
    TIMEREFERENCE   : 5292000
    CODINGHISTORY   : A=PCM,F=44100,W=24,M=stereo,T=SADiE5
    ORGANIZATION    : EMI
    TITLE           : Taxman
    track           : 1
    ARTIST          : The Beatles
    ALBUM           : Revolver (24 BIT Remastered)
    DATE            : 2009
    encoder         : Lavf53.21.0
    Stream #0.0: Audio: pcm_s16le, 44100 Hz, 2 channels, s16, 1411 kb/s
Stream mapping:
  Stream #0.0 -> #0.0

Attachments:
dac-output.zip
  • Sign in to reply

Top Comments

  • e14 Contributor
    e14 Contributor over 12 years ago in reply to e14 Contributor +2
    Current test rig. BBB ($45), cs4271 on breadboard (about $15 parts and dozens of hours of labor), Cary Audio SE-1 amp (about $1K), pair of B&W DM302 speakers (about $200). I assembled this system that…
  • shabaz
    shabaz over 8 years ago in reply to shabaz +2
    Also, unrelated, but for after you have resolved the device tree issue, I just wanted to confirm, if you're following the circuit, make sure you include the 'bitclock inversion' functionality. The BBB…
  • shabaz
    shabaz over 8 years ago in reply to jithu_element14 +2
    Hi Jithu, Just to follow up on this, I re-tried on another image too, but still no luck. I've posted a request for help on the Beagleboard.org BBB-Wireless forum, in case anyone else has had success. Reproducing…
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to shabaz

    You are right, the McASP can be slaved to an external master clock. I've just started reading up on McASP. I was originally planning to use a PRU to interface to the DAC, I still might have to. I need 3 output channels for my home-made 3-way speakers (tweeter, midrange, bass). I'm running each driver via a separate amplifier; there are no analog crossover networks in the speakers, it is all done in the digital domain. For stereo I need 6 channels, 3 per speaker, and my plan for that is to use a Beaglebone/DAC per speaker. This will eliminate long cable runs, and to open the possibility of making the DAC/amplifier/speaker combos wireless. Good quality audio speaker cables are expensive! Much cheaper to put the DAC right next to the amp and the amp right next to the speaker, that'll let me get away with very short runs for the wiring.

     

    How do you post pictures on this forum? I'd like to post a pic of the current hifi system.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • morgaine
    morgaine over 12 years ago in reply to shabaz

    shabaz wrote:

     

    I'm no audio expert, but I can imagine it could make a difference to audio to have a clean clock.

     

    I'm no expert either, but in the music industry "the difference" is regarded as very severe indeed and warrants using special quality wordclock generators to maintain samplerate accuracy and minimize jitter.  Apparently we are extraordinarily sensitive to the jitter of wordclocks in particular --- it's an anomaly that has no counterpart in sound generated and perceived wholly in the physical world.  The word "unmusical" is often used to describe the effect.  Many kinds of distortion are highly musical and even deliberate, but this one is not.  (Allegedly.)

     

    The S/PDIF stream is self-clocking and the receiver extracts the wordclock signal from the incoming stream and locks to it, so poor quality clocking at source can propagate all the way up the digital audio chain, clearly something to avoid.  In the DAC at the end of the chain, wordclock jitter contributes the perceived unmusical effect as well as harmonic distortion and noise, and inaccurate clock frequency or drift can give phase locked loops a headache and produce a variety of artifacts.  Clicks and pops are common when either clock frequency or jitter are significantly out of AES spec, and a slow or fast clock will also (obviously) make your music play at the wrong speed, and lose sync with video in a composite system.

     

    It's also worth mentioning that if the physical medium is so poor that the edges just aren't getting across the 1-3MHz 75-ohm transmission line coax cleanly then of course the eye pattern closes up and intersymbol interference raises its ugly head, and you can imagine the effect that has on clock extraction!  (Shudder ...)  There's probably an optical counterpart to such issues in S/PDIF over optical fibre / Toslink too.

     

    It's a fun topic, and a lot more complicated than a simple digital data link might at first suggest.

     

    Here's a well-detailed 5-part article that will leave you wishing you knew less about it: image   TNT-Audio on jitter.

     

    Morgaine.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 12 years ago in reply to e14 Contributor

    Hi John,

     

    I'm no audio expert, but I can imagine it could make a difference to audio to have a clean clock. The AM3359 TRM mentions that a certain pin's mode (AHCLKX) can be used for an external clock source. I only briefly looked and I'm not sure if that is brought out to the headers or not. It may be worth checking. That way you can feed a nice clock from a dedicated oscillator.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 12 years ago in reply to morgaine

    I wish to try creating an optical output for the BBB soon. I've finally got a soundcard with optical input capability, so I can capture the audio and inspect it. That will allow me to transmit the test audio files that were mentioned a while back, and examine them.

    By the way, John, for the post below, you may wish to take a look at NEON in a later iteration of your design, it may help with algorithm acceleration (although it sounds like you've already exceeded your design goals). Looking forward to seeing your design, do post more details as you develop it! :-)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • morgaine
    morgaine over 12 years ago in reply to e14 Contributor

    John Rhoades wrote:

     

    Yes the PRU can do audio. I wrote a PRU program that accepts audio samples from a .wav file via the host CPU and generates a PCM bitstream on one of the header pins. Just run that bitstream through an RC filter to remove the ultrasonics then to an amp

     

    That sounds like an interesting project, John, and at least the digital side of it is likely to be compatible with what I had in mind.  I want no analogue anywhere near my computer equipment --- it's the job of a proper home A/V amp or a quality audio DAC to convert from digital to analogue as I see it, and these days even the cheapest of those have quality circuitry to do the conversion which we couldn't possibly match in a simple project.  Also, by converting to analogue ourselves, we would introduce wires and hence noise and pickup between the BBB and our audio power amp --- not an optimum approach.

     

    So, my recommendation is to stay in the digital domain on the BBB.  The PRUs only need to emulate an audio device as far as audio time sync, samplerate conversion, software mixing, buffer management and output formatting is concerned, and then push the result out the back door either on S/PDIF or onto the network as an audio stream.  All digital.

     

    Of course the AM3359 does some of the above already, although it generates I2S not S/PDIF.  I guess it might be possible to snatch the raw digital audio from the SoC's audio device and send it to the PRU to complete the task, which might be a good approach because shabaz ascertained that the AM3359 is capable of outputting 24-bit 192kHz audio on I2S.  This would be expanding the existing audio device, an alternative to creating a new virtual audio device with the PRUs.

     

    Morgaine.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>