BeagleBoard
  • Products & Partners
  • Dev Tools
  • Single-Board Computers
  • BeagleBoard
  • More
  • Cancel
BeagleBoard
Blog BBB - Building a thermal imaging camera
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join BeagleBoard to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: shabaz
  • Date Created: 7 Jun 2013 8:36 PM Date Created
  • Views 3374 views
  • Likes 3 likes
  • Comments 10 comments
  • beaglebone_black
  • bb_black
  • beagle_bone_black
Related
Recommended

BBB - Building a thermal imaging camera

shabaz
shabaz
7 Jun 2013

Introduction

This was a quick, fun exercise, to build a complete thermal camera using the Beaglebone Black, a small LCD and a thermal array sensor.

It was really more of a consolidation, combining some earlier experiements.

 

The setup

The image here shows the entire assembly, capturing an image of my hand (taken from about 1 foot away. It was hard to take a photo at the same time!).

 

image

The final code is attached. The information on each sub-section is at these links:

Thermal array circuit

I2C interface code (either compile it, or just copy the libi2cfunc.a file to /usr/lib, and the i2cfunc.h file to /usr/include )

1.8inch LCD display

Image scaling (or use NEON functionality)

PRU information (you will need to install the PRU assembler if you want to make changes - if you don't, you can use the pre-assembled .bin file in the zip file).

 

The attached code is not tidy, but it works. It could be optimised a lot, I made no effort to do this. Currently the image updates at about 1Hz, but this could be improved many times. Many conversions are done that could be simplified.

Edit: It looks like actually the whole process is occurring at many tens of Hz, but the LCD updates at about once per second; this looks like a limitation of the LCD display (the update over the serial interface is occurring rapidly, but internally it presumably only updates once per sec. An alternative display is required!).

Edit 2: It turned out that the LCD was fine; the thermal sensor was set to internally update at 1Hz, regardless of the readout speed. The version 2 code attached has it now set to 16Hz in ir.c, but possibly 4Hz or 8Hz would be sufficient and give higher accuracy.

Compiling and running the code

Here is how to use the code:

 

First, make sure the I2C library is installed as mentioned above.

 

Then, copy the attached code into any folder, unzip and then follow one of these two steps:

 

1. If you have not installed the PRU assembler:

make partclean;make ir_app; make dtfrag

 

 

2. If you have installed the PRU assembler:

make clean;make

 

 

Copy the generated .dtbo file to the /lib/firmware folder.

 

Then, type the following (it could be placed in a startup script when the board has booted):

export SLOTS=/sys/devices/bone_capemgr.9/slots

echo cape-bone-lcd18 > $SLOTS

cat $SLOTS

 

 

The code can now be run by typing:

./ir_app

 

To generate video the code was modified (v3 code) to accept a file prefix.

./ir_app img

 

This will generate files beginning with img, i.e.

img00000.png, img00001.png, etc.

 

Then, they can be converted into a video using:

avconv -i img%05d.png -b:v 1000k test.mp4

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

Another video (the temperature to color conversion had a bug in the earlier video, fixed in the v3 code):

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

Here is another photo, this time of a tub of icecream.

image

This is holding an ice lolly on a stick:

image

Other ideas

It would be nice to be able to retrieve the images via a PC, either stream the images, or to have a web server to access them, or just dump files in a folder for now. I didn't get a chance to try any of these.

If I get time I might build this into an enclosure, as a permanent project (powering the the entire thing from a Li-Ion battery that connects on the board (Olimex BATTERY-LIPO1400mAh fits, if you buy the right connector).

Attachments:
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
ir_code_v3.zip
  • Sign in to reply

Top Comments

  • shabaz
    shabaz over 10 years ago +1
    Just noticed that the awesome Grid-EYE sensors from Panasonic are now in stock! Finally cheap thermal vision : ) Anyone planning to try them out?
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to shabaz

    Agree about the grid-eye. I purchased one with the idea of making a simple camera out of it. Will post link here when I can get around to actually doing it!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 12 years ago in reply to e14 Contributor

    Hi Bruce,

    Glad you found it useful! The Melexis sensor is sadly a little expensive (I've been waiting for Farnell to stock the Panasonic Grid-Eye which should be a similar sensor) but works very well, and has an I2C interface, making this a straightforward project.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago

    Really awesome and useful project! I would like to build one of these... thanks for posting.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 13 years ago in reply to morgaine

    It's definitely an interesting thing to play with. It does pick up chip heat, and it also warmth from the LCD display which I couldn't tell was warm by touch. I finally got the speed higher, so it would be cool to be able to save video clips (maybe just dump png files using cairo, and then try ffmpeg. I'm curious how fast it would encode, since it should be hardware accelerated on the BBB. (Edit: some quick videos now attached).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • morgaine
    morgaine over 13 years ago

    That's pretty cool!

     

    We could have used one of those back in the days before RPF fixed the Pi's 1.8V board fault and the LAN9512 chips had the secondary use of frying your breakfast. image

     

    Re the LiPo battery charging, that's one of the really nice features of several Olimex boards.  I use their Olimexino-STM32 with a 2000mAh LiPo battery, a perfect fit because board and battery are almost identical in size.

     

    I know the BBB has some battery charging potential via unpopulated pads, but I haven't delved into it yet.  It wouldn't be particularly useful though, as the board is not as power-frugal as a Cortex-M3.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
<