BeagleBoard
  • Products & Partners
  • Dev Tools
  • Single-Board Computers
  • BeagleBoard
  • More
  • Cancel
BeagleBoard
Blog BBB - High speed data acquisition and web-based UI
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join BeagleBoard to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: shabaz
  • Date Created: 4 Aug 2013 1:17 AM Date Created
  • Views 14156 views
  • Likes 7 likes
  • Comments 93 comments
  • test
  • beaglebone_black
  • bbb
  • texas_intruments
  • measurement
  • bb_black
  • beagle_bone_black
Related
Recommended

BBB - High speed data acquisition and web-based UI

shabaz
shabaz
4 Aug 2013

Introduction

This was a fun yet initially challenging experiment, to find a convenient way to read in data at a reasonably high speed on a BeagleBone Black. This photo shows the results from a mobile, showing a couple of sampled waveforms (100kHz and 1MHz sinewaves in this case).

image

This was another capture of the same signals on a PC (this is an older picture with a x10 probe so the amplitude is a little low in the photo - it should fill the screen).

image

 

What does it do?

In its current state, it grabs analog data from an ADC, and dumps it into memory on the BBB, ready to be displayed or further processed. It could be used for gathering analog information from sensors, CCDs or other data acquisition use-cases. To be reasonably useful, the desire was for it to support 20Mbytes/sec of data or more. It does achieve this, but it is for further study to find higher speed methods.

 

How does it work?

A few different ways were considered. The initial approach was using an FTDI device (USB interface). However the method described here just feeds data directly into the on-chip 200MHz PRU that is part of the Beaglebone’s AM3359 chip. Other methods are possible too.

It was also desired to have an external clock, so that the data could be sampled at a determinable jitter, so that it could be useful for frequency analysis, or maybe Software Defined Radio (SDR).                                                           

The overall approach that was taken is outlined here.                                                                                                                                                                                  

image

The analog signal was amplified and fed into a high-speed ADC (A parallel bus ADC is needed in order to achieve high throughput).

A pre-built amp+ADC board was used from KNJN (note: in my opinion it is not a good choice, because it is closed source; there are no circuit diagrams for it so it is hard to modify it, the datasheet is sparse and also it is expensive; better to construct one up manually).

A linux application (called adc_app in the diagram) was used to kick off the PRU code which reads in data and dumps to shared memory. Once complete, the adc_app stores it in a .csv format file.

I wanted to try out Node.js ever since a recent blog post, so some very basic code is used to create a HTTP server.  The real-time comms between the browser and web server is achieved using Socket.IO which is a way of passing arbitrary data.

A photo of the overall system:

image

A bit more detail:

image

The underside was more untidy!

image

 

ADC Detail

As mentioned, a ready-built amplifier and ADC board was used. The on-board oscillator was disabled, so that an external one could be fed in. I needed a clock of 20MHz or less, but I only had a 32MHz oscillator at hand and didn't want to wait (and the local Maplin store doesn’t sell any 3.3V-compatible logic to divide by two!) and I’m not entirely sure how long the shared memory write takes, and I did experience lost samples with the 32MHz oscillator. I plan on trying frequencies in the range 14MHz-20MHz to find the upper limit for missing no samples; for further study!

Note that some ADCs will have specific requirements related to the clock and duty cycle.

The ADC on this particular board was ADC08200 but an ADC08100 or ADC08060 could have been used at lower cost).

 

Buffers

These were extremely important for two reasons. One reason is that the pins to the BBB that I wished to use need to be isolated during power-up, because they are used for selecting the boot method. If there was any unusual level on the pins upon power-up then the BBB will not boot from the eMMC. So, a tri-state buffer is needed.

The other reason is that there is a fair bit of capacitance and it is highly likely that the ADC may not be able to directly drive the pins at high speed. I actually came across this problem while trying to connect a camera to the BBB. I struggled for days without realising that the camera could not support the load. So, the buffers are likely to be essential for most designs using the pins that were selected. I used a 74LVC244A device as a buffer.

Note that the clock also needs a buffer, unless significant jitter is acceptable. No tri-state is required here, so I used a MC74VHC1GT50.

 

PRU code

The PRU code uses shared memory for communication. I designated a single byte of shared memory to be used for commands. When run, the PRU sits in a loop waiting for the command to instruct it to begin the data capture.  PRU GPI mode is used which allows inputs to be read at the processor speed of 200MHz with no varying latency. Just a few instructions are needed to populate the data into shared memory. No attempt was made to pack the data, and 32-bits are used to store the 8-bit sample. This is not such a bad idea, because in future the ADC could be swapped out to a (say) 10-bit ADC with no code change on the PRU.

There are two PRUs in the AM3359. There are a total of 12 PRU GPI capable pins available that are connected to PRU 1 which are brought out to port 8 on the BBB. So, this means that realistically 10 or 11-bit is about the limit for high-speed parallel ADCs connected in this manner. Still, at (say) 16MHz clock, this would equate to 20Mbytes/sec of data for a 10-bit ADC.

EDIT: See comments section - on PRU0, all 16 pins are in theory available).

The pins used are shared with the HDMI interface; it proved necessary to disable the HDMI interface by recompiling the device tree file in the /boot folder (EDIT: See Brian's comment below for a better method to disable HDMI). Since I wished to display the data using a web browser, I have no issue with losing the HDMI.

Once the data has been captured (2000 samples in this example), the command byte is acknowledged, so that the Linux hosted application can know that the PRU has completed. The PRU now sits and waits for a new instruction from the Linux hosted application.

These were the pins used. They were used as D[0..7], CLK and a *EN signal for controlling the octal tri-state buffer.

image

 

Linux hosted application

The adc_app program is very simple (C code); it downloads the assembled code into PRU1 and executes it. The resultant data in shared memory is dumped to a text file and then the program exits.

 

Node.js application

The Node.js application creates a HTTP server (no need for apache!) and a Socket.IO connection. This sits and waits for a connection from any web browser. Once it receives a connection, it will send a handshake and then wait for a ‘capture’ command from the web browser. It then calls the adc_app program. Once complete, it opens the file of captured data and transmits it over the Socket.IO connection line-by-line. This is very inefficient, but it is proof-of-concept code that could really be optimised.

 

Web Page

The web page served up contains some small bits of code to handle the Socket.IO connection and send a ‘capture’ request when a button is clicked and to display the received data with a canvas element and pixel manipulation.

 

Summary

In conclusion, it is possible to read analog data with low jitter at fairly high speeds without any external FIFO or logic (beyond a simple buffer IC), while continuing to run Linux applications such as a web server. It is also nice that a web-based UI can be rapidly created using Node.js.

 

Note: It is still for further study how long captures can be sustained and read off by the Linux application without any data loss. If it can be sustained, then it could be useful for SDR applications just about, although a higher speed (and better ADC) would be preferable.

 

Note2: The waveforms used to test out the system were generated by the same BBB using a low-cost ‘direct digital synthesis’ (DDS) board. That’s a subject for a later date.

 

Using the code

Disable the HDMI as mentioned in the comments.

You may need to install Socket.IO. Type this to install it:

npm install socket.io

 

Create a development folder and then the attached code can be unzipped to (say) /home/root/development/adc.

 

make clean
make
cp BB-BONE-HSADC-00A0.dtbo /lib/firmware/
source install_hsadc_cape.sh
node index.js

Then, navigate to http://xx.xx.xx.xx:8081/index.html

 

If you want to make subsequent changes, there is a bug in the makefile, and you will need to issue 'make clean' before typing 'make' whenever any change is made in the C code.

If you just want to reassemble the PRU code, type 'make pru' (no need for 'make clean').

Attachments:
adc_v1.zip
  • Sign in to reply

Top Comments

  • e14 Contributor
    e14 Contributor over 13 years ago in reply to bwelsby +2
    Brian Welsby wrote: again are all the pins available? I'm beginning to wonder how long it's going to take for somebody here to decide they want a BBB with a few differences, take the available designs…
  • stanto
    stanto over 12 years ago in reply to morgaine +2
    These values sound very small. Perhaps I have misread but is this relevant ? https://groups.google.com/forum/m/#!topic/beagleboard/Gb6xL7V7Z00
  • morgaine
    morgaine over 13 years ago +1
    After your I2S audio DAC article, I was wondering when the ADC one would appear. In addition to SDR, I'm interested in ADC functionality for the multifunction instrument idea. Since you pointed out that…
  • morgaine
    morgaine over 12 years ago in reply to e14 Contributor

    selsinork wrote:

     

    I've spent a few days recently getting u-boot to behave in the same way across Sabre-Lite, OLinuXino, Cubieboards, Wandboard.

     

    Ironic, don't you think, that the most common vehicle for boot-time synergy between OSHW ARM boards is provided by a medium with a proprietary specification and usually formatted to a patented Microsoft standard. image

     

    Morgaine.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to morgaine

    Morgaine Dinova wrote:

     

    We cope with the situation of course (largely because it's the current norm), but we should be bothered by it because it forces us to treat each board brand as a separate entity --- there is no synergy between them.

    I've spent a few days recently getting u-boot to behave in the same way across Sabre-Lite, OLinuXino, Cubieboards, Wandboard. I'm most of the way to having kernels in the 3.12/3.13 range running on all of them, albiet some rather experimental kernels for now. Then I have my LFS built userspace that will run on them all.

    So don't think I'm oblivious to the problem. Trying to get some synergy in the bits I have some direct ability to change for myself is about all I can do at this point though.

     

    Physical pinouts are hard to change, although I'm quietly hoping that Olimex are open to listening to us, they seem to have made changes to some boards due to popular demand previously. Having someone like Tsvetan on side would probably bring your ideal future a step closer.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • morgaine
    morgaine over 12 years ago in reply to e14 Contributor

    selsinork wrote:

     

    Well, ever the pragmatist, I'll take the choices we have over no choice at all.

     

    Agreed.  But I'm upbeat about having choices in this area.  I'm quite defeatist on some things (eg. lawyers and politicians), but not on this one.  "We have the technology", as they say.  What's missing is the will to move out of our current comfort zone, which is a bit like the comfort zone allegedly held by some happy slaves --- unfortunately not entirely a metaphor, because we are indeed slaves to commercial manufacturers.

     

    But... it's not me you need to convince. I'm more than open to changing my mind should a viable alternative present itself. If I wasn't I'd still be advocating that the sun shines from the RPi's

     

    Agreed.  Sometimes one has to work towards a particular future though, or it won't present itself at all.  This is especially true when there are vested commercial interests about, as in our case.

     

    The EOMA-68 thing is the poster child for the problem. So long in the making that it may be too late by the time it's a reality, and no commercial interest because it's taking so long.

    The Pi changed the game, got people interested and that caught the commercial interest, but was really a small step. What you're talking about here is a much bigger step and so is very much harder to accomplish.  IBM once tried a change of mindset with MCA (for selfish reasons of course) and look how well that worked out.

     

    Agreed on all 5 points.  I'll just point out though that "success" in the open source communities is determined differently than commercially, and it is not conditional on product life cycles nor slice of the market pie.  It just needs a few people to be making steady progress and that whatever they're doing actually works as they intend.  It's comparatively easy to claim "success", although it's undeniable that this still entails a huge amount of work and dedication.

     

    Yes, it's quite clear we're treated as consumers here. Doesn't take too much reading through the RPF & BBB forums to realise that a high percentage of people owning those boards literally are nothing more. How do you change their mindset ?

     

    Heh, no idea.  But that's not actually what I had in mind (my educational cap isn't on currently).  To get something along the lines that I was describing started I would have to convince many deeply dyed in the wool techies that OSHW should work more like RepRap than like iTunes.  As the last few posts here showed, that already seems doomed because many techies consider OSHW to be just fine exactly where it is today, thank you very much --- ie. much more like iTunes than like RepRap.

     

    So, the likelihood of any improvement in the situation is, I think, very close to nil.

     

    Morgaine.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to johnbeetem

    John Beetem wrote:

     

    The idea that one can simply produce a piece of OSHW and "the community" will magically step up to the plate and support an OS is IMO naïve.

    Agreed. With one slight reservation. Anything that's Cortex-A* class onwards already has some very good OS support from a range of distros.  The bigger issue tends to be driver support for the random IP blocks the vendor bought in and stuck in the SoC without much real understanding of what they were doing.  The remainder of the OS is almost irrelevant if you don't have a display or input device or network connection. As you rightly point out that takes a kernel developer who wants to scratch that particular itch, and they tend to be less interested in user experience. The GPU elephant in the room always being the most difficult obstacle. Never mind commercial considerations, even a community full of expert kernel/GPU developers may not care if you only ever sell a couple of thousand boards - they're all in your situation, too many other interesting things to do...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to morgaine

    Morgaine Dinova wrote:

     

    Hah!  You agree on the symptoms, yet you want to continue with the problem that causes them!

    Well, ever the pragmatist, I'll take the choices we have over no choice at all.

     

    But... it's not me you need to convince. I'm more than open to changing my mind should a viable alternative present itself. If I wasn't I'd still be advocating that the sun shines from the RPi's .........

     

    The EOMA-68 thing is the poster child for the problem. So long in the making that it may be too late by the time it's a reality, and no commercial interest because it's taking so long.

    The Pi changed the game, got people interested and that caught the commercial interest, but was really a small step. What you're talking about here is a much bigger step and so is very much harder to accomplish.  IBM once tried a change of mindset with MCA (for selfish reasons of course) and look how well that worked out.

     

    Yes, it's quite clear we're treated as consumers here. Doesn't take too much reading through the RPF & BBB forums to realise that a high percentage of people owning those boards literally are nothing more. How do you change their mindset ?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>