BeagleBoard
  • Products & Partners
  • Dev Tools
  • Single-Board Computers
  • BeagleBoard
  • More
  • Cancel
BeagleBoard
Blog BBB - Logic Supply BB100 Case
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join BeagleBoard to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: shabaz
  • Date Created: 19 Feb 2014 2:49 PM Date Created
  • Views 1739 views
  • Likes 2 likes
  • Comments 8 comments
  • beagbone_black
  • bbb
  • enclosures
  • beagle_bone_black
  • case
Related
Recommended

BBB - Logic Supply BB100 Case

shabaz
shabaz
19 Feb 2014

The Logic Supply BB100 case has be available for a while (also in black), I purchased one recently while buying other gear, these were my thoughts on it

(pictures were from a cameraphone so apologies for the quality - better images at the Logic Supply website of course).

image

 

If you need your BeagleBone Black boxed up, there are worse ways. I thought it was very well made and quite flexible. The cover can be mounted at three heights, to accomodate capes (the gaps can then be used for wires and ribbon cables for example. I will probably fit the Olimex 1400mAH LiPo inside it too as shown here.

 

The case is steel (not aluminium) and in my opinion is extremely accurately cut and shaped. The case has sub-millimeter accuracy. The base and shell are less than a millimeter thick, yet extremely tough because of the choice of material.

 

All connectors are spot-on centered into their holes and the tiny narrow microSD card slot doesn't scrape or touch the card at all.

 

The board is held in place with four screws on permanently fitted metal stand-offs. The finished result is about the size of a pack of playing cards.

Fullscreen contentimage_29915.html Download
<html><head><title>Jive SBS</title></head>
<body><font face="arial,helvetica,sans-serif">
<b>Error</b><br><font size="-1">
An general error occurred while processing your request.
</font></font></body></html>

 

The exterior finish is a matt type, slightly roughened surface so not gloss shiny/smooth. I think the finish is great.

Initially I wasn't a fan of the D-Sub connector punch-out (I don't like using this connector for serial connections although it is a standard) but I now think it is a great idea, since it can serve as the I/O for 8 pins or more if a serial port is not desired. On the other side there is a circular punch-out ideal for coax shaped connectors or for a switch for example (approx 6.5mm dia hole measured with a ruler). These punch-outs mean that for many use-cases one may not need to ever drill any holes in the case.

Very narrow slots allow for all LEDs on the board to be visible.

image

 

Lots of spare screws are supplied in two sizes; the flush ultra-tiny ones shown in the photo earlier, or slightly larger pan-head. By only fitting two screws, the lid can become hinged.

The rear has punch-outs for providing screwed attachment to another surface, or thin vertical slots can be used for fitting to a metal chassis. Really nice engineering everywhere on this case.

Four thin rubber feet are supplied for optional fitting.

The case is not cheap but metal cases usually do cost more, and so this case is fairly good value for money especially if you want a case you can use as part of a demonstration for example.

Postal cost is quite low in Europe for this case shipped from Netherlands, so that helps too.

 

As a summary, the case is very nice and practical, and I think it is worth the cost.

  • Sign in to reply

Top Comments

  • DAB
    DAB over 12 years ago +1
    Hi Shabaz, The case does look like it has been built for a number of different types of applications. I like the user selectable configuration for IO connectors and agree with you about the nice matt finish…
  • bwelsby
    bwelsby over 12 years ago +1
    Nice, I shall put one on my shopping list for when I can get a BBB to put in it.
  • shabaz
    shabaz over 12 years ago in reply to e14 Contributor

    Hi Chris,

     

    That's true. I was wondering if there are higher-density D-sub connectors but same size as DB9 (like VGA type connectors) for the scenarios where more I/O is needed. It could be wired to single header jumper pins so they could be swapped around at will.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago

    Nice case but it's a shame there is not breakout option for the headers.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to shabaz

    I'm based in another EU country, Cyprus.

     

    I looked at UK postage price - 3.95 euro (no track & trace), the cheapest to Cyprus was 25 euro for 4 day delivery - there wasn't a 'no track' option.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 12 years ago in reply to e14 Contributor

    Oh. It was 3.95 euro postage from Netherlands to UK. I notice they also have a separate US site, but I don't know if that makes a difference. Where are you based?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago

    I agree that 11 euros isn't too bad for a solid, metal case.

     

    Can't agree with the 25 euro postage being low. image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
>