BeagleBoard
  • Products
  • Dev Tools
  • Single-Board Computers
  • BeagleBoard
  • More
  • Cancel
BeagleBoard
Blog BBB - Rechargeable on-board battery system
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join BeagleBoard to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: shabaz
  • Date Created: 9 Aug 2013 11:53 PM Date Created
  • Views 21024 views
  • Likes 18 likes
  • Comments 129 comments
  • beaglebone_black
  • bbb
  • bb_black
  • beagle_bone_black
  • ti
Related
Recommended

BBB - Rechargeable on-board battery system

shabaz
shabaz
9 Aug 2013

Note April 2017: There are different revisions of the BeagleBone Black since this post was written in 2013, and without testing them all, it is the user's decision whether to try this solution or not. The revision changes are listed here and a possible option for at least some revision boards is shown in the photo here but I've not investigated this. The newer BeagleBone Blue already has a battery connection, so that is another option.

 

This posting is about implementing a rechargeable battery system for the BeagleBone Black. It is simple, safe and very low cost (less than 6 Euro).

 

image

 

First, some brief information about the power circuitry on the BBB.

 

The BBB has a built-in power management IC (PMIC) based on the TI TPS65217C device. This device contains multiple switch-mode regulators and LDO regulators to provide all voltage levels needed for the entire board. It handles wake-up using a push-button fitted on the BBB. Automatic power-down via the button requires some software to be implemented (to do the equivalent of 'shutdown now' from the command line). When the button is pressed, an interrupt is generated and the microprocessor is supposed to query the PMIC (via I2C) to learn that the button was pressed, and kick off the shutdown sequence. In the event of a failure here, the power can be switched off by holding the button down for 8 seconds.

The IC also contains built-in battery charging capability.

Apart from the USB requirement of 5V, there is no need to run the BBB from 5V; it can happily run from a lower supply. This means that a single 3.7V cell could be used to power the entire board. No need to step-up to 5V or to run dual cells and step-down to 5V, both of which could have been inefficient.

Why is this useful?

It makes it an excellent platform for outdoor/portable use.

For indoor use a battery is useful because it serves as a backup supply in case the main power (from a mains powered supply or from USB) gets disconnected. It could prevent filesystem corruption. If the main supply gets disconnected, the battery immediately takes over. In fact, I permanently leave the battery connected even when I'm running from the mains supply, in case I forget to safely shutdown the board.

What battery can be used?

Any small Lithium Ion (Li-Ion) or Lithium Polymer (Li-Po) single cell can be used, preferably as long as it has a built-in protection circuit. If it doesn't have an in-built circuit, it is highly advisable that one with a built-in thermistor is used. A cell in the range 700mAH to around 2AH is advisable. The one that I used in the photo above is from Olimex part code BATTERY-LIPO1400mAh. It should last around 3.5 hours (EDIT: Now been measured, it lasts 2 hours 50 minutes - see notes below, and comments below) on a full charge (not measured) and should fully charge in around 2 hours. This particular battery is just the right size to fit in between the two rows of headers and is flush so that a cape can still be plugged on top. So, the entire thing can fit inside any enclosure.

You will also need a connector (see next section) and one resistor.

Construction detail

The BBB has four holes that are suitable for connecting up the battery. They are detailed in the BBB system reference manual (SRM):

image

This is what they look like:

image

The Olimex Li-Po has a built-in protection circuit, so I soldered a 10k resistor to TS and GND to simulate the thermistor. (EDIT: You may or may not wish to do this, please study Li-Po and use your own judgement - see comments below) It is desirable to use a connector for the Li-Po.

The LiPo connector was convenient to solder to pins TP6 and TP8, and then  a zero-ohm link between TP5 and TP6 on the underside.

Here is how it was done step-by-step (there are just two steps):

1. Solder the 10k resistor, and a zero-ohm link (both are achieved on the underside of the board) as shown here in the yellow box. These are simple 0603 resistors; I used a 1% tolerance resistor, but 5% should be fine.

image

2. Solder in the connector.

This is straightforward, but complicated slightly by the fact that the connector has 2mm pin spacing, but the board has 0.1" spacing. It means that the pins on the connector need to be splayed or bent into the correct spacing. The connectors are available in vertical mount or right-angle (RA) mount. If you use a vertical mount connector, there may not be enough space to splay the pins. Instead, I used a right-angle connector and bent the pins into a vertical orientation, and then I had space to bend the pins and still have the connector flush with the board as shown here. You can see another view of the connector from the first photo.

image

I'm fairly sure that the desired connector is JST 'PH' series.

 

That's it; plugging in the battery, the board worked instantly. Note that the Li-Po charge method is usually to have a constant current supplied to the battery until it reaches a certain, very precise voltage. After that the charger switches to a constant-voltage mode. For the Li-Po battery that I used, the charger needs to be set to 4.2V, but the BBB by default sets it to 4.1V (It can be set to 4.2V via I2C control but today it doesn't). I'm not sure what the impact of this is (beyond storing less charge), but I believe it is safe. I have been using it daily for three months and the battery is always cool to touch.

Controlling the PMIC

The TPS65217C PMIC is very programmable; it has dozens of configuration settings specifically for charging and it has safety timer capability. The PMIC is configured upon startup via I2C. There are three I2C busses on the BBB, and one is dedicated to on-board peripherals. Control of the PMIC is not normally possibly by the user; it requires driver code or possibly there is access by the device tree infrastructure. Checking the .dts file in /boot did not reveal how to control the battery charger functionality. There are two current Google Summer of Code (GSoC) projects that touch on PMIC:

1. IIO, ADC, PMIC, LCD debug/patchwork (summary page, blog page) - Zubair Lutfullah

2. MINIX I2C drivers (summary page, blog page) - Thomas Cort

Hopefully the guys working on the projects (Zubair and Thomas) can offer some advice on how to set the level to 4.2V. Zubair's project also includes how to use the in-built ADC inside the AM3359 to monitor voltages.

Notes

There really should be some more detail including measurements to show how long the battery lasts and to observe the charging status (via I2C reads). Unfortunately I didn't have time to collect this information. But I've been using it for three months regularly and it functions well.

EDIT: The following simple test was conducted using the Olimex battery referred to above.

1. Power up the BBB using the DC power supply and let it charge the battery while powering the BBB

2. After about 4-5 hours, the DC supply was disconnected, and a script was run on the BBB to log the current date/time to a file, every minute. The script would sleep in-between. The Ethernet connection was left up, and the BBB was left alone until the battery died, and then the log file was examined.

 

#!/bin/bash
while true; do
date >> log.txt
sleep 60
done

 

The result was that the log file showed that the BBB ran for 2 hours 30 minutes before it died. After this, the test was repeated. The second time, it ran for 2 hours 50 minutes. The discrepancy may be because this battery has never been fully charged followed by such a long discharge, and so perhaps it is related to that. No test has been run with the Ethernet disconnected, but the BBB should run for longer in that case of course.

In a third test, the battery again ran for  2 hours 50 minutes (to within 1 minute). Again, this was with the Ethernet interface up.

  • Sign in to reply

Top Comments

  • shabaz
    shabaz over 13 years ago in reply to morgaine +2
    Hi Morgaine, Thanks! That's a good link and tip. I too had found the connector tight. Hi John, (Replying here so that we can retain the battery comments in a single location): John Alexander wrote: How…
  • shabaz
    shabaz over 13 years ago in reply to fustini +2
    Hi Drew, I'm not sure where the 500mV number could be from. The charge voltage will go up to 4.2V, or at least it should, but today is 4.1V until the PMIC is programmed for a 4.2V threshold). Apparently…
  • mcb1
    mcb1 over 13 years ago in reply to shabaz +2
    Nice project. There are LDO regulators that can be lower than 500mV. We had a very interesting talk about LiPo/LiOn batteries by the battery expert at a local large firm that has them in their radios.…
  • shabaz
    shabaz over 11 years ago in reply to mtnman

    Hi Terry,

     

    No problem at all! I hope it helps. I too would have preferred a supercap solution for the scenario where just a shutdown is needed and no need to keep the BBB powered for a long time, but couldn't think of a suitable way. There are some very small supercaps but their internal resistance is high and designed for RTC type scenarios, whereas the larger ones with low internal resistance start getting bulky and pricey : (

     

    Good luck with your project : )

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mtnman
    mtnman over 11 years ago in reply to shabaz

    Shabaz – thank you so much for your quick response and your insight.  I’ve been reading more since I posted this topic earlier and was getting more and more discouraged about using a Supercap.  While according to my calculations, I might get 20 seconds out of it, it would drop below the usable voltage level too quickly and I’d be lucky to get half that amount of time of powering the circuitry.  And, I’ve read on a couple of other posts that shutdown can easily take longer than 10 seconds.  So, perhaps a battery is the best way.  I was trying to avoid a battery, but I’m not sure I see a better option at this point. 


    We use a supercap in another product to keep an RTC running when the remainder of the board is shutdown and just love that solution.  I was hoping to find a way to use one here as well, rather than going with a battery.   But, it looks like using a supercap is going to require much more effort than I had hoped for.

     

    I'll go through your posting in much more detail so I understand how the battery gets connected and I’ll start looking at smaller LiPo batteries.

     

    Again, I greatly appreciate you taking the time to help me out.  You’re very kind.

     

    Terry

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 11 years ago in reply to mtnman

    Hi Terry,

     

    Unfortunately I don't think a supercap will work, without additional circuitry. On its own, it will confuse the PMIC most likely, which is not expecting such a device connected. It may work, if you can find a way to charge up to 4.2V (but no more than the supercap rating) e.g. if you had some diodes from the 5V supply and a series resistor. This is assuming the PMIC doesn't complain, which it might.The method of supercap on the 3.3V power line not work, because quite a lot of current needs to be supplied when the supercap is discharged, and it will look like too heavy a load for the voltage regulator in the BBB.

     

    So in summary some experimentation and probably some additional circuitry is needed for supercap.

     

    As you say, the supercaps will be pricey too, so perhaps the LiPo is the cheaper and simpler option. I know a supercap is preferable but maybe for the intended life-cycle of your project, the LiPo could work reliably? Although I used a 1200mAH LiPo, you could probably just use a far smaller cell.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mtnman
    mtnman over 11 years ago in reply to shabaz

    Hi, Shabaz.  Thank you so much for the detailed information and your responses - you're very generous to share your knowledge like this.

     

    I have a question related to this topic and wonder if you could provide some additional insight.  I am trying to do what has been described here as well - provide a means to gracefully shut down a Beaglebone Black (BBB) unit running a Debian distribution on loss of power.  And, I'm trying to figure out an inexpensive and simple means of accomplishing this.  As has been described, I only need for the unit to remain powered long enough to shut down - hopefully only a matter of several seconds.  I've not tried to determine how long that will be, but it appears to be fairly quick (I'm trying to figure out how to measure this now).  So, I really like your idea of running the main +5V line to a GPIO line on the processor through a voltage divider and use that to trigger the shutdown. However, I've got to keep the processor running long enough to do this.  Rather than using a battery, I'm wondering if I could use a supercapacitor?  Have you ever looked into using a Supercapacitor rather than a battery to provide the necessary power to keep it going long enough to shut down?

     

    Calculations would suggest that a 2F supercap could provide 500 mA of current for 20 seconds.  I've seen data on the BBB current draw indicating approximately 450 mA, as a worst case scenario, and it's probably significantly less in a steady state environment.  One issue - the voltage will drop below usable at some point, so I wouldn't get the full time as calculated.  So, the thought process would be to monitor the voltage on the GPIO pin and if the voltage goes away for 3 seconds, or some amount of time, then run a script that causes a shutdown of the BBB.  Perhaps the supercap could just be attached to the 3.3V power line.  I did find supercaps at Digikey that could do this (even though they're not as cheap as I'd hoped).

     

    You did make this comment in an earlier post - "For the scenario that a backup supply is needed momentarily for when main power is removed (for a graceful shutdown),  I've noticed the recent debian images will initiate a shutdown automatically, assuming that a LiPo is directly connected. Power-up occurs when the main supply is reconnected, or via the switch on the BBB (for battery-only power, or if the BBB was shutdown using the switch rather than accidental main power disconnect)."  I'm guessing that putting the supercap in place of the LiPo would not work as well?

     

    Does this have any possibility of working - using a supercap rather than a battery, or am I totally off-base?

     

    Thanks.

    Terry

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 11 years ago in reply to e14 Contributor

    Hi Joseph,

     

    Only a LiPo cell can be wired to the connector described in the post above, any other rechargeable or non-rechargeable battery type would not work.

    If you want to use regular AA or C batteries, then a DC-DC converter is needed. For info on that, refer to this article, it concerns converting the BBB into a handheld games machine powered from AA batteries.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>