BeagleBoard
  • Products & Partners
  • Dev Tools
  • Single-Board Computers
  • BeagleBoard
  • More
  • Cancel
BeagleBoard
Blog BBB - Sonos-like Sound System
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join BeagleBoard to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: shabaz
  • Date Created: 5 Mar 2014 3:27 PM Date Created
  • Views 4961 views
  • Likes 4 likes
  • Comments 22 comments
  • hifi_mixed_signal
  • beaglebone_black
  • beaglebone_project
  • bbproject
  • burr_brown
  • hifi
  • bbb
  • texas_instruments
  • hifi_mixed_signal_dac
  • ti
Related
Recommended

BBB - Sonos-like Sound System

shabaz
shabaz
5 Mar 2014

Introduction

This post briefly documents a BeagleBone Black (BBB) based music box. If you’ve ever wanted a Sonos system but (like me) felt they were a little expensive, then it is worth considering using a compact Linux platform like the BBB for creating something slightly similar. I feel the sound quality is not leagues different (better nor worse) than some more expensive commercial offerings.

image

It was a quick, fun project and costs about £100 including the cases and the BBB.

The idea for this project was simple - a compact box that connects to the home network and allows the ability to send it music to play (or it can play music stored on-board or on a server). The documentation provides just an overview because the circuits are already documented, and every implementation could be slightly different depending on end user needs, speaker enclosure, etc.

Here is the rear view:

image

 

Shown below is a video of it in action. The sound was recorded from the camera in-built mic so is not representative of actual sound quality. For actual sound quality, refer to the MP3 recording here, which was captured by connecting the headphone output (not line output) directly to an ADC and captured by the PC.

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

Components

The main bits and pieces are the speaker box, the BBB and a DAC/amplifier.

Although a BBB and home-built DAC/amplifier was used, a Raspberry-Pi and Wolfson audio card could be used too, for a similar price.

The home-built DAC and amplifier is easy to assemble; it uses medium-sized SMD components that are hand-solderable, and gives results similar to a Meridian DAC which uses the same chip (a Texas Instruments ic). Full circuits and information are at these two locations: part 2 has the schematic, and part 1 has some more technical detail.

There are plenty of other DACs available including pre-built ones. A search for “I2S DAC” will reveal ones that should be suitable (I have not tried them) – this ebay example is just over £10. (Note that you may require a logic inverter, see the comments sections in the links earlier).

 

The speaker is a Tivoli Audio speaker. It is possible to get these in new condition for about £15-20 frequently on ebay, in various color options. Any speaker enclosure would have been fine. The official Tivoli webshop sells new speakers (slightly different model) from £39 upwards.

 

Design and Implementation

The DAC board was mounted inside the speaker, and the BBB was mounted outside. This allows access to all the BBB ports while making the minimal amount of holes in the Tivoli speaker (Speakers are sealed for good audio reasons).

It won't replace main home music systems but that was not the intention, nor is it stereo (that capability is easy to achieve by adding a second speaker connector, but I didn't require it). This is more a bedroom or home study one-box sound system.

 

Step 1: Fit BBB inside a case

The first step was to get the BBB into its own case. I connected a push-switch to safely power on/off the platform. I also wired up a DB9 connector to interface to the DAC.

image

I used L-shaped single-in-line header pins to solder up the connections and heatshrink at the DB9 connector end. The switch and LED were wired up to the power switch pin on the BBB and to the 3.3V supply (via a 100 ohm resistor) respectively. The push-switch is wired to the P9 header, pin P9_9 and to ground (pin P9_1). The LED 3.3V supply can be taken from P9_3.

 

The photo below shows the LiPo battery fitted. I used a paper sticker on the underside of it, to insulate it further. The BBB doesn’t run hot, but the battery could have a spacer between the PCB and itself if desired.

image

Here is the finished result, powered up. It can be safely powered down by pressing the button again (this feature is by default in the current Debian image).

image

The other side of the case provides access to the USB port, and a small USB WiFi adapter was fitted. I have not got round to finding a software driver for it yet, so for now I just used Ethernet.

 

Step 2: Speaker modifications

The next step was to put the BBB aside and work on the speaker and DAC. The speaker was opened up, and the wadding was removed and stored in a plastic bag to prevent dust and drilled fragments of plastic getting on it. The speaker cable was chopped and discarded, and the grommet removed.

image

The DAC board was fitted with L-brackets http://uk.farnell.com/jsp/search/productdetail.jsp?CMP=i-ddd7-00001003&sku=1466881 and the speaker rear cover was marked up for drilling the holes to secure it, and for the headphone and line jack outputs (3mm holes for the screws, and 6mm holes for the jacks).

image

The photo below shows the finished result.  The jacks are rather recessed. This is actually no problem for some headphones (e.g. a pair of low-end AKG I own) but others will have problems. I plan to drill to a recess with a larger drill bit to 7mm and it will cover both of my sets of headphones. Note that you want to make the holes as small as practical.

image

After wiring up the DAC to the speaker, the wadding was placed back in position and the cover was closed up again as shown below. Then the DB9 matching connector was soldered (wires protected with heatshrink). I didn’t bother with a cover for it.

image

After testing, the hole needs to be sealed (perhaps with epoxy resin glue).

Finally, the BBB was attached to the speaker (rubber feet and adhesive foam pads can be used).

 

Step 3: Try it out!

This step was the easiest.

Plug in the power supply, power up and install the audio player software:

sudo apt-get install mplayer

Then, try to play a music file (either from local storage or from network storage):

/usr/bin/mplayer -ao alsa -volume 10 “songname.mp3"

 

Summary/Next Steps

A quick and simple sound system was created. With a pre-built DAC and amplifier, the hardware implementation can be extremely easy.

There are plenty of software options for creating a library of songs and providing an interface for the user to select something to play. I have not tried them. For now I will just use SSH to select music. Eventually the hope is to create a simple browser based app that will allow one to upload MP3 songs from a PC or mobile phone for instant playback. A wake-up alert in the morning with a random song, or the news, will be a good option too (enabled via browser on mobile phone).

  • Sign in to reply

Top Comments

  • shabaz
    shabaz over 12 years ago in reply to fustini +2
    Hi Drew, Thanks! Yes, it was nice to draw the line on something with a final application. Although I think I should build one for the office now too, to see what audio files people send it during the day…
  • mcb1
    mcb1 over 12 years ago in reply to shabaz +1
    Nice post, well done. I think I should build one for the office now too That's almost worse than having to listen to someone else music in the next area ... I guess you can always turn it down. It…
  • Problemchild
    Problemchild over 12 years ago in reply to shabaz +1
    Here's the page about it on the OpenWRT site it also has links to various projects using it http://wiki.openwrt.org/toh/tp-link/tl-wr703n
  • shabaz
    shabaz over 11 years ago in reply to Problemchild

    Unfortunately I couldn't see that from the schematics, looks like that capability is not present. BBB still seems to be the most audio-suited board I'm aware of.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Problemchild
    Problemchild over 11 years ago in reply to shabaz

    The C seems to have a CVBS output which has some pads but no connector ...wonder if they have Audio as well hidden away ?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 11 years ago in reply to Problemchild

    Ah, that could be easier. The U3 has a built-in speaker amplifier (pdf), >3W per channel. I've not tried it, but the pads are next to the eMMC connector on the underside : )

    There is also I2S, but that could be very hard to tap, there are no pads for that as far as I'm aware.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Problemchild
    Problemchild over 11 years ago in reply to shabaz

    Sounds like keeping it simple paid dividends.

    I feel the need to bury an ODROID into a set of speakers image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 11 years ago in reply to Problemchild

    Hi John,

     

    No attempt was made to sync audio - in fact for the above project I combined the stereo after the DAC into mono for a one-box solution more for bedroom or study room type use.

     

    There are some standards for low-latency audio over Ethernet as you probably know, but I've not had a chance to investigate them.

     

    I was at the time just happy the sound seemed reasonable, I want to do more with this project at some stage. I made a recording of the stereo analog output from the circuit using the best sound card I had, and I can't tell the difference between that and the original source. Nor could I tell the difference when comparing with a friend's $300 DAC. All subjective of course! The recording from the circuit is here http://www.element14.com/community/servlet/JiveServlet/download/38-126336/dac-output.zip and the source file was an Amazon purchased MP3 file.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
>