BeagleBoard
  • Products & Partners
  • Dev Tools
  • Single-Board Computers
  • BeagleBoard
  • More
  • Cancel
BeagleBoard
Blog BeagleBone Web Server - LED Blinking
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join BeagleBoard to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: oneleggedredcow
  • Date Created: 22 Nov 2013 1:21 AM Date Created
  • Views 7268 views
  • Likes 2 likes
  • Comments 42 comments
Related
Recommended

BeagleBone Web Server - LED Blinking

oneleggedredcow
oneleggedredcow
22 Nov 2013

Table of Contents

Setup

LED Blinking

MySQL Installation

Temperature Sensor

Introduction

In the previous article, we set up the BeagleBone to be a webserver running Lighttpd and PHP.

 

In this article, we are going to build upon that foundation.  We are going to create a web site that lets the user turn on and off an LED on the BeagleBone.  This is a good example of how to create a simple web page that interacts with the BeagleBone and is a step towards our final goal of creating a website to show historical temperature information.

 

Turning a LED On/Off

BeagleBone LEDs can be turned on/off through command line, but in order to do this, we need to figure out what they are named.  The names can be found like this:

 

ls -1 /sys/class/leds

image

So, turning the usr2 LED on/off would look something like this:

image

1 will turn the LED on, and 0 will turn the LED off.

 

By default, some of the LEDs are used to display information to us about what is going on.  So, if you change the state of one of those LEDs, it will be quickly overwritten.  We can see this by looking at the trigger:

 

cat /sys/class/leds/beaglebone::usr0/trigger

image

To modify this so that the LED only changes when we tell it to, we can change the trigger to none:

 

echo none > /sys/class/leds/beaglebone::usr0/trigger

image

 

C Program

Now that we know how to turn on/off the LEDs, we can write a small C program to make it easier for us. The program will take in the number of the LED to change (0-4) and the state to change it to (off = 0, on = 1). Here’s the code:

 

#include <stdio.h>

#include <stdlib.h>

#include <fcntl.h>

#include <unistd.h>

 

int main(int argc, const char *argv[])

{

if (argc != 3)

{

printf("Usage:\n");

printf("\tledCtl <led> <on/off>\n");

printf("\n");

printf("<led>  : Number between 0-3\n");

printf("<on/off>: 1 = on, 0 = off\n");

 

return 1;

}

 

int ledNum = atoi(argv[1]);

if (ledNum < 0 || ledNum > 3)

{

printf("<led>  : Number between 0-3\n");

 

return 1;

}

 

char ledPath[1024];

sprintf(ledPath, "/sys/class/leds/beaglebone::usr%d/brightness", ledNum);

int fid = open(ledPath, O_WRONLY);

 

int onOff = atoi(argv[2]);

switch (onOff)

{

case 0:

write(fid, "0", 1);

break;

case 1:

write(fid, "1", 1);

break;

default:

printf("<on/off>: 1 = on, 0 = off\n");

return 1;

}

 

close(fid);

 

return 0;

}

 

Remember to change the path of the LED to the path that we found earlier.

 

For a simple task like this, we could have just used the command line to turn the LEDs on/off. However, I wanted to put it into a C program so that we set ourselves up better for the future.  When we take temperature measurements and put them into a MySQL database, it will require more logic that is better suited for a small program rather than the command line.

 

The code should be fairly clear.  It is mostly just checking the inputs that the user gave us to make sure that they are reasonable.

 

Before we compile it, we need to create a directory to store the scripts that we are going to be running on our web site:

 

mkdir /www/cgi-bin

 

To compile the code, type:

 

g++ ledctl.cpp -o /www/cgi-bin/ledctl

image

 

Then we can run some examples and make sure that it works:

 

/www/cgi-bin/ledCtl

/www/cgi-bin/ledCtl 2 1

/www/cgi-bin/ledCtl 2 0

image

 

Creating a Web Page

Awesome, now that we have a program to control the LEDs on the BeagleBone, let’s create a web page so that we can control the LEDs over the Internet.  Let’s call the web page ledCtl.php and place the following code in it:

 

<html>

<head>

<title>BeagleBone LED Changer</title>

<style type="text/css">

p { display: table-cell; }

button { width: 75px; margin: 2px auto; }

</style>

<?php

if (isset($_GET['led']) && isset($_GET['onOff']))

{

$led = $_GET['led'];

$onOff = $_GET['onOff'];

 

exec( "/www/cgi-bin/ledctl $led $onOff" );

}

?>

</head>

<body>

<div style="width: 200px; margin: 0px auto;">

<div style="width: 100px; float: left;">

<p>LED #2:</p>

<button type="button" onclick="location.href='ledCtl.php?led=2&onOff=1'">ON</button>

<button type="button" onclick="location.href='ledCtl.php?led=2&onOff=0'">OFF</button>

</div>

<div sytle="width: 100px; margin-left: 100px;">

<p>LED #3:</p>

<button type="button" onclick="location.href='ledCtl.php?led=3&onOff=1'">ON</button>

<button type="button" onclick="location.href='ledCtl.php?led=3&onOff=0'">OFF</button>

</div>

</div>

</body>

</html>

 

Note: We used LEDs #2 and #3 because LED #0 and #1 occasionally blink and override our on/off settings.

 

Then we can test our web page by going to a browser and using our new web page:

image

Pressing the buttons on the page should change the state of the LEDs on the BeagleBone!

 

Next Article

In the next article, we are going to get MySQL up and running on the BeagleBone.  We will use MySQL as a convenient place to store the temperature measurements that we take.  This will also make it easy to retrieve the data when the user requests historical temperature information through our web page.

Attachments:
ledctl.zip
  • Sign in to reply
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to e14 Contributor

    Mario Rodriguez wrote:

    I create a .cpp with only a printf("HelloWorld); when the code .php run that HelloWorl (with exec(...)) nothing happens and in the Beagle´s console I don´t see the "Hello World".

     

    I'll suggest reading what the php manual has to say about what exec() does with command output: http://www.php.net/manual/en/function.exec.php

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • oneleggedredcow
    oneleggedredcow over 12 years ago in reply to e14 Contributor

    So, this time I did mean to have 4 digits in the chmod command (4755).  The first 4 means that when the program is run, the user ID is changed to be the owner of the file, in this case root.  So, the program is run as though root ran it.  (Which is why there are large security implications to doing it.)

     

    Doing a printf won't put any output in the console window.  This is because the program is run in some other context and so the output will go there.  In order to do a test like that, what you can do is write a text file.  So, change up the code so that it writes "Hello World!" to /www/cgi-bin/hello.txt (or some other file).  Just make sure that you have permission to write to that directory (chmod 777 /www/cgi-bin).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to oneleggedredcow

    but I think that it is not the problem, because even if I change "ledctl" and I create a .cpp with only a printf("HelloWorld); when the code .php run that HelloWorl (with exec(...)) nothing happens and in the Beagle´s console I don´t see the "Hello World".

     

    I have also tried doing

         chmod 475 /www/cgi-bin/HelloWorld

    and

         chmod 777 /www/cgi-bin/HelloWorld

        

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • oneleggedredcow
    oneleggedredcow over 12 years ago in reply to oneleggedredcow

    I'll be honest, I wasn't thinking about setuid.  However, that's a good thing to try.  Try doing "chmod 4755 /www/cgi-bin/ledctl" and see if that works.

     

    Now as selsinork points out, this isn't really a great idea from a security standpoint.  This is especially true since it is being run from a web page.  So, his suggestion of changing the permissions on /sys/class/leds is a much better idea.  So, if setuid works, then I would quickly change it back to "chmod 755 /www/cgi-bin/ledctl" and change the permissions on /sys/class/leds.  I would try something like "chmod 666 /sys/class/leds/beaglebone::usr*/brightness".

     

    Or you can just set the permission on /sys/class/leds first and not play around with fire (setuid).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • oneleggedredcow
    oneleggedredcow over 12 years ago in reply to e14 Contributor

    Opps, one too many 5's.  That's what I get for not proof-reading!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>