BeagleBoard
  • Products & Partners
  • Dev Tools
  • Single-Board Computers
  • BeagleBoard
  • More
  • Cancel
BeagleBoard
Blog BeagleBone Web Server - Setup
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join BeagleBoard to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: oneleggedredcow
  • Date Created: 20 Nov 2013 6:39 PM Date Created
  • Views 12221 views
  • Likes 2 likes
  • Comments 16 comments
Related
Recommended

BeagleBone Web Server - Setup

oneleggedredcow
oneleggedredcow
20 Nov 2013

Table of Contents

Setup

LED Blinking

MySQL Installation

Temperature Sensor

Introduction

In this series, we are going to turn our BeagleBone into a web server.  Then we are going to use that web server to monitor the temperature in a room.  To do this, we are going to leverage a couple of common open source programs.  We are going to use lighttpd as our web server.  Then we are going to integrate in PHP to handle the required server side logic.  We will also use a MySQL database to store the temperature measurements so that we can display historical information.  To gather the temperature measurements, we will use C to read a BeagleBone GPIO port.  Finally, we will use Javascript to give the user a nice interface to work with.

 

The technologies that we are going to us in this tutorial are very powerful and this is just meant as a starting point to demonstrate how the technologies can be used together on a BeagleBone.  Trust me, this is just the tip of the iceberg.

 

Install Lighttpd

Now before we install any new software, it is a good idea to update opkg:

 

opkg update

 

To install Lighttpd, type:

 

opkg install lighttpd lighttpd-module-fastcgi

 

Note, this will display a message about the job failing.  This is because port 80 is already in use.

 

Disable Preloaded Services

The BeagleBone comes with a bunch of preloaded services.  This this makes it really easy to get started, but the preloaded services use port 80, and that is exactly the one that we want to use.  So, we need to disable them, so that we can run on that port. Also, we disable a few extras in order to free up some memory on the BeagleBone.  Here’s how to disable the services (and a link to what the services that you are disabling do, in case you are interested):

 

For BeagleBone:

systemctl disable cloud9.service

systemctl disable gateone.service

systemctl disable bone101.service

systemctl disable avahi-daemon.service

systemctl disable gdm.service

 

For BeagleBone Black:

systemctl disable cloud9.service

systemctl disable gateone.service

systemctl disable bonescript.service

systemctl disable bonescript.socket

systemctl disable bonescript-autorun.service

systemctl disable avahi-daemon.service

systemctl disable gdm.service

systemctl disable mpd.service

 

image

Excellent, now that the services are disabled, we need to reboot and the services will be no longer started:

 

shutdown -r now

 

Warning

It may seem more logical to disable the services first, and then install Lighttpd.  However, this didn’t seem to work for me.  It would hang on the “configuring lighttpd…” step. Doing the installation first seemed to work much better.

 

Now, let’s test to make sure that Lighttpd installed correctly.  To do this we need to figure out the IP Address of the BeagleBone:

 

ifconfig -a

image

Now on another computer on your network (anything but the BeagleBone), point a web browser to that IP Address, and you should see a very reassuring message:

image

 

Install PHP

Next, we need to install PHP.  To do that type:

 

opkg install php php-cgi php-cli

 

Now we need to configure Lighttpd to use PHP.  To do this, we need to edit the lighttpd.conf config file.  However, before we do this, we need to gather a little bit of information. We need to find out where php-cgi was installed:

 

which php-cgi

 

Then we need to edit the Lighttpd config file:

 

vi /etc/lighttpd.conf

 

And we need to do two things.  First, we need to uncomment “mod_fastcgi”, which was at line 24 for me:

image

Then we need to uncomment the fastcgi configuration.  Here we will also need to configure the “bin-path” to point to the location of php-cgi that we found earlier.

image

To complete the configuration, we need to restart Lighttpd, so that the configuration file will be read in:

 

/etc/init.d/lighttpd restart

image

Finally, to test that the web server is working correctly, we are going to create a simple web page:

 

vi /www/pages/test.php

 

And type in the following code:

 

<html>

<head>

<title>Test</title>

</head>

<body>

<?php print(“PHP is working on the BeagleBone!”); ?>

</body>

</html>

 

To view the web page, go back to the web browser that you used earlier and type in:

 

<IP Address>/test.php

image

 

Video

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

Next Article

In the next article, we are going to use the web server to display a web page that lets you turn the LEDs on the BeagleBone on and off.  Once we have accomplished that, then we will move on to incorporating a MySQL database and a temperature sensor.

  • Sign in to reply
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to oneleggedredcow

    Ok, thanks again!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • oneleggedredcow
    oneleggedredcow over 11 years ago in reply to e14 Contributor

    Pretty sure that I overwrote the SD card with a new image and started with a clean slate.  There might be a better way, but I never discovered it.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago

    I appreciate your work with this tutorial! You mentioned that you got hung up on "Configuring lighttpd" what did you undo that allowed everything to work again? I followed the tutorial closely, but made a noob mistake in the PHP section and ended up starting over. Since I had already disabled those basic add-ons, I automatically installed lighttpd after, and ran into this problem. If I forcibly end the "configuring lighttpd", when I try and open /etc/lighttpd.conf, only about 10 lines of it are there. Thanks in advance for your time!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • oneleggedredcow
    oneleggedredcow over 11 years ago in reply to e14 Contributor

    Awesome, thanks for posting those links.

     

    If I ever get a chance, I'd like to try this on Debian.  Too many projects, too little time...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago

    For those having trouble getting this to work on Debian cross reference this with the below articles.  Also wherever someone uses vi you may want to swap it with nano (seems much easier edit with for me)

     

    General command differences between Armstrong & Debian

    Inspire | BeagleBone Black Tutorials, Resources and Workshops

     

    Lighttpd & PHP install on Debian

    https://www.howtoforge.com/installing-lighttpd-with-php5-and-mysql-support-on-debian-squeeze

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
>