BeagleBoard
  • Products & Partners
  • Dev Tools
  • Single-Board Computers
  • BeagleBoard
  • More
  • Cancel
BeagleBoard
Blog Installing & Running BOINC on a BBBlack
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join BeagleBoard to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: mp2100
  • Date Created: 14 Apr 2020 9:14 PM Date Created
  • Views 2461 views
  • Likes 2 likes
  • Comments 1 comment
  • boinc
  • bbb
  • BeagleBone
  • einstein@home
Related
Recommended

Installing & Running BOINC on a BBBlack

mp2100
mp2100
14 Apr 2020

Intro

As a follow-up to my previous post:

Finding Pulsars on Raspberry Pi (BOINC & einstein@home)

I also wanted to run BOINC and einstein@home on my Beaglebone Black (BBB).  BOINC is, of course, the Berkeley Open Infrastructure for Network Computing, a crowdsourcing computer clustering system to solve scientific problems.  I have a few BBB setting in a drawer (more than I like to admit), so why not put them to use?  Beaglebone is running a fairly modern debian image, so it should be similar to but different from a raspberry Pi.

 

The debian operating system that my BBB reports when I run the command uname -a is  4.14.49-ti-r54 #1 SMP PREEMPT Fri Jun 15 22:14:13 UTC 2018 armv7l GNU/Linux,

That's not the latest kernel, but fairly recent. I did try it with an older version of BBB debian, but boinc could not resolve the dependencies.

 

On the raspberry Pi, BOINC was easy to install and configure because I could use the simple synaptics software manager to install boinc-client, and boinc-manager.  With the BBB, one issue to consider is beaglebone.org seems to be moving toward headless only images.  As a matter of fact, for performance reasons, I set up several of my BBB with the "IoT" version flashed onto them.  So I figured command line boinc configuration would be a good thing to learn.  I did get it working, but as it turned out, (so far) I have only been able to get it working by setting it up with what I'll call a hybrid command line and GUI system.  Let me explain below.

 

Installation

Googling around (actually https://duckduckgo.com -ing around), I found a few instructions such as:

https://boinc.berkeley.edu/wiki/Installing_BOINC_on_Debian

and

https://boinc.berkeley.edu/wiki/Client_configuration

and

https://boinc.berkeley.edu/wiki/Stop_or_start_BOINC_daemon_after_boot

 

These confirmed that I do the typical commands.

$ sudo apt-get update

$ sudo apt-get install boinc-client

and then needed to edit one or two xml files,  The configuration files are located at two places:

/etc/boinc-client

/var/lib/boinc-client

 

Config

The file listing at /etc/boinc-client is:

debian@beagle0:/etc/boinc-client$  ls -l

 

-rw-rw-r-- 1 boinc boinc  356 May  8  2017  cc_config.xml

-rw-rw-r-- 1 root  boinc 1498 Apr 12 22:40  global_prefs_override.xml

-rw-r----- 1 root  boinc    1 May  5  2017  gui_rpc_auth.cfg

-rw-r--r-- 1 root  boinc  312 Apr  9 18:36  remote_hosts.cfg

See below, I did end up editing the file remote_hosts.cfg, because I decided to control it remotely.  Looking through /var/lib/boinc-client, it wasn't obvious to me what to enter in the xml files to get my project running.  Maybe it's just me, but I need a few examples to be able to get the xml entries put in the right place.  The boinc.berkeley.edu wiki provided information, but with the long list of options it was not clear to me how I would get the client running, and get it to use my einstein@home account.

 

Most helpful was this posting from pimylifeup.  Yes it's a raspberry Pi tutorial, but it often happens that Pi answers help guide me when I'm learning to use my beaglebone.

https://pimylifeup.com/raspberry-pi-boinc/

This was quite useful because of the examples using "boinccmd" to configure the client.  I also used the following two commands.  I had previously set up my username and password when I first configured my raspberry Pi. For my project, I'm not running setiathome, I'm running einsteinathome,  so in the following commands I substituted the web site     http://einstein.phys.uwm.edu

$ boinccmd --lookup_account http://setiathome.berkeley.edu <your_email> <your_password>

$ boinccmd --project_attach http://setiathome.berkeley.edu <your_account_key>

This got me attached to my einstein@home account, great.  And I could see (with "top" command) that the client was running.  But, alas, it still didn't start processing data.  The " boinccmd --get_tasks  " returned  a blank result, no processing was going on.  Probably if I'd spent more time, the options with boinccmd would have gotten me going.  At this point, I thought I'd backtrack and install boinc-manager, and set up the BBB with a keyboard and monitor.  So I ran the typical command to do that.

     $ sudo apt-get install boinc-manager

 

 

But then, in my searching, I decided to try the "hybrid" approach.  My raspberry Pi 4 was busy running BOINC and einstein@home.   I had the both beaglebone and my raspberry Pi on the same network, and the Pi already had the GUI boinc manager running.  I had seen on the boinc wiki that remote control was possible, so I figured I would try to control the beaglebone remotely using the boinc-manager running on my Pi.  I knew my BBB IP address.  I went into /etc/boinc-client and edited the remote_hosts.cfg as follows, typing in the last line, the IP address of my Pi 4 that I want to use.

# This file contains a list of hostnames or IP addresses (one per line)

# of remote hosts, that are allowed to connect and to control the local BOINC core client via GUI RPCs.

# Lines beginning with a # or a ; are treated like comments and will be ignored.

# allen's Pi4 is at IP address .15

#host.example.com

192.168.0.15

 

https://boinc.berkeley.edu/wiki/Controlling_BOINC_remotely

This web page has some information, but as above, the instructions were lacking details.   The goal was to get the beaglebone processing data and link it to my account.  I knew that setting up user name and starting an einstein project was easy using the GUI boinc-manager.  What worked was going into the Pi boinc manager, with the Advanced View, and open another window:

image

 

From that window, I chose the BBB client rather than the local (Pi) client.  For Host name entering the IP address.  I typed in 192.168.0.41 (my BBB), and for a Password,  no password, leave it blank, and I was in.   (originally I thought I had to type the BBB password, but my Pi 4 crashed today, and when I redid the connection, only the IP address was needed.)  If I do enter a password at this step, no connection is established, leaving the password blank is what makes it connect properly.

 

image

 

Now I'm connected remotely, and I can easily enter my username and add the einstein@home project to my BBB.

 

image

 

OK. that's all working well now.  It's been running a few days.  If you look carefully at the above image, with the speed of the BBB, it takes more than 2 days to process one task from einstein@home.  I'm not going to win any awards for best contributor, but the journey was interesting.  After using the remote host to configure the BBB,  in directory /var/lib/boinc-client, it now has a lot of configuration files that were created.  The command line boinccmd --get_tasks now gives me the status of my boinc client, so I can monitor it that way using the command line.

 

debian@beagle0:/var/lib/boinc-client$ boinccmd --get_tasks

======== Tasks ========

1) -----------

   name: p2030.20170503.G39.54+01.50.S.b2s0g_240_0

   WU name: p2030.20170503.G39.54+01.50.S.b2s0g0._240

   project URL: http://einstein.phys.uwm.edu/

   report deadline: Mon Apr 27 12:11:46 2020

   ready to report: no

   got server ack: no

   final CPU time: 0.000000

   state: downloaded

   scheduler state: scheduled

   exit_status: 0

   signal: 0

   suspended via GUI: no

   active_task_state: EXECUTING

   app version num: 147

   checkpoint CPU time: 60733.660000

   current CPU time: 60752.690000

   fraction done: 0.298859

   swap size: 134 MB

   working set size: 134 MB

   estimated CPU time remaining: 157904.272082

 

Next

Next step, learn a fully command line configuration of boinc.  Using the auto-generated xml files as my guide, I may be able to figure it out.

  • Sign in to reply
  • Dirk_P_Broer
    Dirk_P_Broer over 4 years ago

    You can use the manager for easy configuration and management. Click on 'View', and choose 'Advanced'. This saves hours if not days. Don't forget to click on 'Options' too.