BeagleBoard
  • Products & Partners
  • Dev Tools
  • Single-Board Computers
  • BeagleBoard
  • More
  • Cancel
BeagleBoard
Blog NASA Space Rover Under Alaskan Ice
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join BeagleBoard to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: fustini
  • Date Created: 16 Jun 2015 10:35 PM Date Created
  • Views 1794 views
  • Likes 6 likes
  • Comments 11 comments
  • beaglebone_black
  • bbb
  • BeagleBone
Related
Recommended

NASA Space Rover Under Alaskan Ice

fustini
fustini
16 Jun 2015

NASA Jet Propulsion Laboratory prototyped a new rover design with the BeagleBone Black!

 

"Testing a Space Rover Under Alaskan Ice"

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

Here's a screenshot of the BeagleBone:

image

  • Sign in to reply

Top Comments

  • mcb1
    mcb1 over 11 years ago in reply to kas.lewis +3
    Ice is an insulator.... Down in the Antartic they simply string the HF communications antenna just above the ground (it melts into the ice otherwise) for their comms. I suspect the antenna on the rover…
  • jw0752
    jw0752 over 11 years ago +1
    Hi Drew, That was really interesting. Thanks for posting the video. John
  • bwelsby
    bwelsby over 11 years ago +1
    Thanks Drew, nice one. The BBB is still my favourite.
  • balearicdynamics
    balearicdynamics over 11 years ago in reply to mcb1

    mcb1 I have not considered the water at +0 C, while seeing the video but it is more than correct; it is around 3-5 C... Then I am almost sure that there is a ground (over the ice surface) repeater. Thank you for the linked document.

     

    Enrico

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mcb1
    mcb1 over 11 years ago in reply to kas.lewis

    Ice is an insulator....

    Down in the Antartic they simply string the HF communications antenna just above the ground (it melts into the ice otherwise) for their comms.

     

    I suspect the antenna on the rover linked to a base station in the shelter ....

    But the water would act as an attenuator, so maybe there is something more planned, or it needs a mothership to act as the go between.

    This paper back in 1987 uses 1.8Mhz and suggests a depth of 20m underwater is possible.

    http://users.tpg.com.au/users/ldbutler/Underwater_Communication.pdf

     

    The temperatures are not that low at 0degC or -32F, otherwise the water would freeze.

    I read somewhere that because of sunlight being trapped the water under the ice was above that, so I suspect the BeagleBone is toasty rather than frozen.

     

     

    Mark

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 11 years ago

    Hi Drew,

     

    That was an incredible video to watch (good old National Geographic : ). I can see that features like the on-board eMMC, very secure mounting capability and open source hardware were probably critical features for selection for this scenario.

    I wonder if any parts were modified, or if it was a totally unmodified BBB that was run through temperature tests to confirm operation, since it was controlling what was probably very expensive hardware.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • balearicdynamics
    balearicdynamics over 11 years ago in reply to kas.lewis

    You are true. The most reliable option is that the rover has the antenna (maybe this white long stuff that seems doing nothing?) and on the surface not far away (some meters) there is a receiver / satellite repeater. In this video it is sure that the show was only a demo (or less than a demo): you see the rover underwater and this means that there was also an equipe that does not appear in the video - not part of the scientific expedition - filming all the event.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • kas.lewis
    kas.lewis over 11 years ago in reply to balearicdynamics

    The video It says the rover can and sometimes is controlled from JPL. The issue I have is the attenuation of water/ice how do you get a signal strong enough to reach a satellite from a small battery operated rover that is under the water/ice.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
>